English

FS Upgraded FHD Fiber Enclosure—Ultra-High-Density Solution for Rack Cabling

Updated on Aug 4, 2020 by
1.6k

Nov 23rd, FS News – As data center continues to expand, rack cabling becomes an increasingly important topic in data center. A qualified rack cabling may reduce network downtime and dramatically improve network efficiency. To meet customers’ need for ultra high density and easy-to-manage rack cabling, FS has upgraded the 1U Rack Mount FHD fiber enclosure. The followings are the new features of the upgraded FHD fiber enclosure

1. More Durable Door

Unlike the former FHD enclosure, the front door of this upgraded enclosure is made of thicker acrylic materials, which provides top-level protection for the inner fiber cables.

More Durable Door

2. Symmetrical Spring Door Latches

Furthermore, the front door is also equipped with two symmetrical door latches which will make the door uniformly stressed when the drawer is pulled out. In addition, the two spring latches can also fix the drawer automatically, and also help you to pull and push it effortlessly.

Symmetrical Spring Door Latches

3. Parallel Sliding Drawer with Smooth Slide Rail

The biggest change is this upgraded FHD fiber enclosure adopts parallel sliding drawer with smooth slide rail. This design allows the drawer to be pulled or pushed steady and fast in a straight line, also makes it easier for cable assembly/disassembly.

Parallel Sliding Drawer with Smooth Slide Rail

In the End

Accommodating 4pcs FHD adapter panels or cassettes, this upgraded FHD fiber enclosure can provide 96 fiber connections. And the upgraded designs make it faster and simpler for cable employment and management in the enclosure.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k