FS Wide Brand Compatible 40GBASE-SR4 QSFP+ Transceiver Test Assured Program
Jan. 12th, Shenzhen, FS News – FS offers a wide range options of brand-compatible 40GBASE-SR4 QSFP+ transceivers. In order to ensure each transceiver with high-compatibility, we have a comprehensive and reliable test assured program for each optics.
Specializing in the explore of fiber optic transceivers, FS always keeps offering high-quality, 100%-compatible and superior-performance transceivers. Since last year, we keep improving optical transceivers solution to meet the accelerating 40/100G data center optics market. The whole series of 40G QSFP+ transceivers are available with ready stock in FS. As the advanced OEM transceiver supplier, we achieved perfection on the compatibility of the transceivers via a rigorous and professional test assured program. At present, we have finished to build up the test beds of Cisco, HP, IBM, Arista, Brocade, Dell and Juniper etc., these original-brand switches will be used to perform the test for each optics which greatly guarantees the high compatibility.
40GBASE-SR4 QSFP+ transceivers support with a link length up to 100 meters on OM3 and 150m on OM4. It primarily enables high-bandwidth 40G optical links over 12-fiber parallel fiber terminated with MPO/MTP multifiber female connectors. As the wide deployment of 40GbE, 40GBASE-SR4 QSFP+ transceivers are widely used in multimode transmission network system. The following shows our brand-compatible test assured program of our 40GBASE-SR4 QSFP+ transceivers. Several major brands such as Cisco, HP, IBM, Brocade, Arista, Dell and Juniper etc., will be included.
Brand | Platform | Transceiver | Test Show |
Cisco | Cisco Nexus 9396PX | QSFP-40G-SR4 CO*, 850 nm, 150 m | |
HP | HP 5900 JG510A | QSFP-40G-SR4 HP*, 850 nm, 150 m | |
HP 5900 JC772A | QSFP-40G-SR4 HP*, 850 nm, 150 m | ||
IBM | IBM G8264 | QSFP-40G-SR4 IB*, 850 nm, 150 m | |
Arista | Arista 7050S-64 | QSFP-40G-SR4 AI*, 850 nm, 150 m | |
Brocade | Brocade ICX 7750-260Q | QSFP-40G-SR4 BR*, 850 nm, 150 m | |
Dell-Mellanox | Dell Mellanonx IS5030 | QSFP-40G-SR4 ME*, 850 nm, 150 m | |
DELL-Mellanox M3601Q | QSFP-40G-SR4 ME*, 850 nm, 150 m | ||
Juniper | Juniper QFX3500 | QSFP-40G-SR4 JU*, 850 nm, 150 m | |
For more information about our Test Assured Program or 40G QSFP+ Optics, please visit here or contact us over sales@fs.com.
FS is a leading manufacturer and supplier of fiber optic subsystems, components and solutions. With last four years growing, we have built our strong and professional teams in optical communication product R&D, systematic solution and supply chain management. Nowadays, we are doing business with more and more worldwide well-known corporations like CloudFlare, EXFO, Apple, MRV, JDSU, ADTRAN, Avago, EMC, etc., who have put large volume of our products into production for their Data Center or Cloud Computing application and speak highly of our service and products. We will be working together with our customers, partners and co-workers to benefit them more and contribute more to the global popularity of optical communication.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023