English

An RJ-45 to 10G SFP+ Transceiver Module: 10GBASE-T SFP+

Updated on Mar 23, 2023 by
36.4k

10GBASE-T has been available in switches and servers as an add-in card since 2008, two years after the new IEEE standard is released. Maturing 10GBASE-T products adopted by a wide ecosystem of adapter/switches vendors in 2012 with the new innovation of the 40nm 10GBASE-T PHY. So far, 10GBASE-T RJ-45-based 10Gbps connectivity has become the most flexible, economical, backward-compatible, and user-friendly 10G Ethernet connectivity option available.

Most of 10GbE switches are with SFP+ ports, when to connect server or switch with 10GBASE-T Rj45 port, the 10GBASE-T SFP+ module will enable 10G SFP+ switches and routers to connect to 10GBASE-T RJ-45 endpoints using Cat 6a cables.

10GBASE-T SFP+ module is a smaller form factor RJ-45 to 10G SFP+ transceiver. It is mainly used over Cat 6a or Cat 7 copper cabling system for 10G transmission with a maximum distance up to 100 m. It conforms to the SFF-8431 and SFF-8432 MSA standards. Read Module Guide: 10G SFP+ Types Classification for more information about 10G SFP+.

Benefits of 10GBASE-T SFP+ Module

  • Enables connectivity to end points where 10GBASE-T RJ45 connectivity has become more popular—these include rack servers, storage servers, and compute appliances.

  • Based on the existing expertise of the previous generation of BASE-T knowledge and training.

  • Connectivity over Cat 6a cables

  • Supports Top of Rack, Middle of Row or End of Row architectures

Frequently Asked Questions About 10GBASE-T SFP+ Module

Q: What cables are supported with 10GBASE-T SFP+ modules?

A: The module is compatible with 10GBASE-T, 1000BASE-T, and 100BASE-T. The Supported cables as below:

Speed Cable Type Max. Cable Distance
10GBASE-T Cat 6a 30m-50m
Cat6a shielded/Cat 7 80m-100 m
1000BASE-T / 100BASE-T Cat 6/Cat 6a /Cat5e 100m

Q: Can the 10GBASE-T be used at low temperatures?

A: The 10GBASE-T is available in commercial and industrial versions. Standard products are suitable for operating temperature range of 0~70 °C. For a wider temperature range, it is recommended to purchase industrial modules (-40 to 85°C) .

Q: What are their differences of 10GBASE-T SFP+ vs SFP+ DAC vs Fiber SFP+?

A:10GBASE-T SFP+, SFP+ DAC, and SFP+ Transceiver are the most commonly used types in the 10G network. The main differences between these products are: 10GBASE-T vs SFP+ vs DAC: Which to Choose for 10GbE Data Center Cabling?

Comparsion SFP+ DAC 10GBASE-T SFP+ SFP+ Fiber
Media Integrated copper/fiber Category 6a or 7 Fiber Cable (SM/MM)
Connector SFP+ RJ45 LC
Distance 15m 30m-100m Max 100km
Cabling System No Copper cabling Fiber cabling
Data rate 10 Gbps 10 Gbps 10 Gbps
Power Consumption 1~1.5w 2~5w ~0.7w

Q: Is the heat generated when the 10GBASE-T is working?

A: The calorific value is very high. The designed power consumption of the 10GBASE-T is 2.5w. Its heat generation is very high, and the high temperature can be obviously felt during use. The switches with multiple SFP+ interfaces cannot be fully equipped with 10GBASE-T. As for the maximum number of 10GBASE-T that can be equipped with, it depends on the switch availability.

Q: Where can 10GBASE-T be used?

A: If using 10GBASE-T, the places are required to be in the Data Center or horizontal areas (in building, including wiring closet). But it is not suited for vertical (riser links) applications within building, or campus & metro applications.

10Base-t modules are used in Data Center TOR areas

The 10GBASE-T modules are used in Data Center TOR areas.

Cases for 10GBASE-T Ethernet Connections

Case 1: Connecting a switch with only SFP+ ports to a switch with only 10GBASE-T ports.

FS 5850 switches with Cisco switches

Case 2: Connecting two switches with only 10GBASE-T ports.

FS 5860 switches with Cisco switches

Case 3: Connecting two switches with only SFP+ ports.

FS 5860 48SC switches with Cisco switches

Case 4: Connecting switches with both SFP+ and 10GBASE-T ports.

Netgear switches

When the two switches both have SFP+ and 10GBASE-T ports, it is recommended to use the 10GBASE-T copper ports first, and save the SFP+ ports for possible future connections to an optical network for longer transmission distance.

Tags

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
384.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
366.8k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
333.8k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
419.5k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
293.1k