English

Guideline for Fixed Fiber Attenuator

Updated on May 13, 2018 by
14.0k

As a beginner in fiber optic network, I used to think that the optical power should be as strong as possible. Even sometimes we use optical amplifiers to improve the optical signal. So what is the fiber attenuator used for? As we know, the source of the single mode fiber is laser, the power of which is extremely strong. Therefore we can use single mode fiber to achieve long distance transmission. But, if the transmission distance over single mode fiber is too short, too much light may overload a fiber optic receiver, which may cause serious high bit error rates. How to solve this? Fiber attenuator should be inserted at the receiver end to reduce the power to the proper level. There are fixed and variable two types fiber attenuators in the market. The knowledge of fixed fiber optic attenuator will be introduced in this article.

What Is Fixed Fiber Attenuator?

Fixed fiber optic attenuator, also called fixed plug type or fixed build-out fiber attenuator, is used in fiber optic communications to reduce the optical fiber power by a certain level. Typical attenuation values are between 1 and 30 dB. Usually, it has a male plug connector at one side to allow fiber attenuator to be plugged directly into receiver equipment or adapters in patch panel, and has female type fiber optic adapter at the other side to allow the patch cords to plug in. Fixed fiber optic attenuator name is based on the connector type and the attenuation level. LC attenuator 5dB means this attenuator uses LC fiber optic connector, and it can reduce the optical fiber power level by 5dB.

Fixed Fiber Attenuator

Fixed Fiber Attenuator

Fixed Fiber Optic Attenuator Types

Fixed fiber optic attenuators are available in LC, SC, ST, FC and MU style with APC and UPC polish. Generally, multimode systems do not need attenuators as the multimode sources, VCSELs, rarely have enough power output to saturate receivers. Instead, single-mode systems, especially short links, often have too much power and need attenuators. Therefore, fixed fiber optic attenuators are usually single-mode types. The most commonly used type is LC single mode female to male and female to female fixed fiber optic attenuator. Unlike the common female to male type mentioned above, the female to female fixed fiber optic attenuators have female type fiber optic adapter at the both ends, which are also therefore called fiber optic adapter type attenuators. They can be used as adapters and attenuators at the same time.

Fixed Fiber Attenuator Types

Fixed Fiber Attenuator Types

How to Use Fixed Fiber Attenuator?

As shown in the figure below, fixed fiber optic attenuators should be always installed at the receiver end of the link (X in the drawing). This is because it's more convenient to test the receiver power before and after attenuation or while adjusting it with your power meter at the receiver, plus any reflectance will be attenuated on its path back to the source.

How to Use Fixed Fiber Attenuator

How to Use Fixed Fiber Attenuator

For female to male fixed fiber optic attenuators, we can plug the patch cord to the female fiber optic adapter of the attenuator. And then plug the male plug connector of the attenuator to the equipment directly. For female to female fixed fiber optic attenuators, we should plug the two patch cords to the two female fiber optic adapter of the attenuator (shown in the figure below).

female to male fixed fiber attenuators

Female to Male Fixed Fiber Optic Attenuators

FS.com Fixed Fiber Attenuator Solution

FS.com provides a wide range of fixed plug type single-mode fiber optical attenuator with optional attenuation value from 1dB to 30dB. They are used directly on the fiber optic connectors and provide a fixed level of optical attenuation. Our fixed fiber optical attenuator has low return loss and works at both 1310nm and 1550nm wavelength range. LC and SC fiber connector types with UPC or APC polish are available, as well as ST and FC types of attenuators.

Category Description
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 1dB
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 3dB
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 5dB
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 6dB
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 7dB
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 10dB
LC Attenuator LC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 12dB
SC Attenuator SC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 3dB
SC Attenuator SC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 5dB
SC Attenuator SC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 7dB
SC Attenuator SC/UPC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 10dB
SC Attenuator SC/APC Singlemode Fixed Fiber Optic Attenuator, Male-Female, 2dB

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
382.9k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
366.2k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
332.5k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
418.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
291.9k