English

Useful Tips for Selecting PoE Cables

Updated on Dec 16, 2021 by
113.5k

FS PoE Cable Selection

PoE has gained popularity in a number of applications, including IP cameras, IP phones, and wireless access points, by running power and data transfer over a single Ethernet cable. However, without proper PoE cables, PoE may have cable heating and connectivity problems, which would negatively impact the transmission performance from the PoE switch to these devices. This article will give you some guidance for your Ethernet cable selections in PoE deployment.

PoE Standards

Power over Ethernet (PoE) stands for a proven method of delivering DC power over the same twisted pair cabling used for LAN data transmission. The IEEE (Institute of Electrical and Electronics Engineers) standards for Power over Ethernet are 802.3af, 802.3at, and 802.3bt presented as follows:

Power Over Ethernet Standards

PoE technology allows a single PoE network cable to provide the required communication and electrical power to a variety of devices. Therefore, choosing the right PoE cable is essential for network communication.

Applications Using PoE Ethernet Cables

PoE technology with explosive growth rates has been widely adopted in various applications—PoE IP surveillance cameras, PoE-enabled Voice over IP (VoIP) phones, Wireless Access Points (WAPs), IP PoE-based lighting, Point-of-Sale (PoS), etc. You can determine the PoE power supply standard and choose the appropriate Ethernet cable based on the power consumption of the devices.

PoE power supply standard

FS provides comprehensive structured cabling solutions. For example, see how FS PoE Cat6a cables function in a network scenario by connecting FS S3150-8T2FP PoE switch to powered devices (PDs).

PoE Application

Factors to Select PoE Cables

Choosing the right cable is the key to network quality and reliability. What should be taken into consideration when choosing PoE network cables? There are several factors that need to be considered when selecting the cable type used for PoE applications.

Data Transmission Requirements

The first factor to consider is the data transmission requirement (e.g., 1000BASE-T, 10GBASE-T) of the device(s) being utilized. Cat5 cable can be sufficient for PoE protocol short-distance transmission. However, more advanced transmission-grade cables, like 1000Base-T, can be needed for digital devices like high-megapixel IP cameras. Cat6 cable and Cat6a cable are typically utilized for applications that require modest efficiency. To accommodate high-wattage PoE requests, 2.5GB to 5 GB Ethernet data speeds are needed, hence HDBase-T cable is recommended. Cat7 and Cat8 cables are preferred for the most sophisticated, effective applications. The newest and most advanced copper cable type, category 8, offers strong performance and top transfer rates of up to 25 GB across a steady channel.

Network Cable coverage distance

The extent of coverage required for the Ethernet cable is a critical consideration. The main distinction between Cat6 and Cat6a lies in how data speed varies with distance. Cat6 cables may, at times, achieve speeds surpassing 1 Gbps, but their maximum distance is limited to 165 feet. If the data ports in your network topology are over 55 meters away from the server, opting for Cat6a can enhance overall performance.

For distances shorter than 55 meters, Cat6 remains a reliable choice, delivering excellent data speeds when correctly installed and used with suitable hardware to maximize its performance.

Conductor Size

Conductor resistance (DCR) in PoE applications results in heat generation in the cable. Typically, Cat6 and Cat7 have larger conductor sizes than Cat5e patch cables. Cables with a larger conductor size can reduce more conductor resistances. Generally speaking, the heat generated in the cable will be reduced with the same ratio of the conductor resistance reduction. Cat6 cables tend to have about 80% of the DCR of Cat5e, thus only about 80% of the heat generation. The larger the conductor size of the cable, the better.

Ethernet Cable Structure

Cable construction is also a factor causing the temperature rise of a cable. Copper cable can be divided into UTP (unshielded twisted pair cable) and STP (shielded twisted pair cable) two types based on cable structure. Usually, cables with metallic or foil shields are proven to dissipate more heat than UTP cables. Higher heat dissipation leads to cooler cable. When using Cat6 F/UTP cable, more than 40% of the heat can be dissipated compared to Cat6 UTP. If allowed, picking Cat7 S/FTP cable with a foil shield around each pair can dissipate more heat than Cat6 and Cat6 F/UTP.

Further Learning: Shielded vs Unshielded Cat6a: How to Choose?

Ethernet Cable Temperature

The previous two factors will affect the cable temperature to some degree. Cables with high-temperature ratings allow for a higher amount of power to be dissipated. Typical temperature ratings for cables are 60°C, 75°C, and 90°C. If the temperature of a cable rises, the electrical performance will be degraded. And it's not good for the cable's physical performance and longevity. Normally speaking, STP cables are less likely to be affected by temperature than UTP cables.

Ethernet Cable Materials

When selecting PoE network cables, make sure that you are comparing apples to apples. Copper-clad aluminum vs. pure copper cables, the former uses aluminum instead of copper wire. Some people may choose the copper-clad aluminum cable (CCA cable) on account of the tight budget, which may lead to network issues from using inferior materials to transmit the signal. The CCA cables have much higher DC resistance than copper cables. If the resistance is not compensated, the voltage drop will be greater for any channel length. Longer lengths will exceed TIA's channel DCR requirements, limiting the voltage available to the device. Higher resistance causes radiant heat to build up faster, and this may cause damage to the device. 100% copper network cabling is a safer and more reliable choice for PoE applications.

Power Consumption

The amount of power that the PoE device requires for operation can't be ignored when selecting PoE cables. The power requirement will dictate which IEEE standard to follow and what the minimum category cabling to be used. Although each standard regulates a minimum category of cabling, other factors are important to be considered including voltage drop and heat dissipation. Voltage drop determines how much of the supplied power reaches the receiving device. The energy that is lost over the length of the cable transforms to heat and is referred to as heat dissipation. Excessive heat build-up can cause an increase in attenuation as well as premature aging of the cabling jacket.

Installation Configuration

The last factor is the cable installation configuration which has a large effect on the heat dissipation ability. Heat will be kept within the cable as high thermal resistance and high conductor temperature occur with large cable bundles or other installation factors. The larger the cable bundle size, the higher the temperature, no matter what cable category and construction structure. Therefore, to avoid elevated temperatures, avoid environments that may confine heat to the cable, such as large cable bundles, cable bundles close together, and constructions or installations that don't adhere to approved standards. It is important to have a proper ventilation system in the environment.

Here provides several specific installing tips for PoE cabling:

  • Get well-prepared before deploying, and never just wing it.

  • Check your network devices to verify that they are PoE compliant.

  • Make use of different media in the whole cabling design.

  • Do not run cable near devices that generate electrostatics.

  • The PoE cable installation is not a one-and-done, please prepare for future upgrades.

  • Think about your budget for the whole cabling installation, and find a cost-effective solution from a reliable supplier.

FS: A Trustworthy PoE Cable Supplier

After considering the abovementioned factors, finally, there comes the selection of the network cable provider. High-quality and high-reliability PoE cables are what a qualified supplier should offer. FS encompasses a wide range of high-quality Cat5e, Cat6, Cat6a, Cat7, and Cat8 PoE cables with shielded or unshielded type options. All of the Ethernet patch cables have passed strict Fluke tests, including the Fluke patch cord test, Fluke channel test, and Fluke permanent link test to guarantee high performance. FS Assured Program for Ethernet Cables offers more detailed information on FS's PoE Ethernet cables.

You might be interested in

Knowledge
See profile for Howard.
Howard
How to Avoid Overheating in PoE Cabling?
Jul 2, 2020
11.4k
Knowledge
Knowledge
See profile for Irving.
Irving
How to Choose an Ethernet Cable?
Nov 1, 2021
43.7k
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
384.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
366.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
333.8k
Knowledge
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
419.5k