English

MLAG vs. vPC: What's the Difference?

Updated on May 19, 2022 by
45.9k

fs data center switch

 

The wider adoption of data center virtualization to streamline data flows keeps driving the demand for higher bandwidth and faster speeds. To cater to this trend, network engineers are seeking ways to connect as many networking devices as possible. One of them is the link aggregation group (LAG) which can combine multiple Ethernet links into a single logical link and improve data transmission efficiency. Both MLAG and vPC can be used to create LAG. But when talking about MLAG vs vPC: what is MLAG? What is vPC?And how do they differ from each other? These problems will be discussed in detail below.

What Is MLAG?

 

MLAG (Multi-chassis Link Aggregation) is a non-standard protocol that enables Layer 2 multipathing from the host to gain either additional bandwidth or link resiliency. It’s a public protocol so that every vendor can support MLAG by using their own custom-rolled implementation of it. MLAG can make two or more enterprise network switches act like a single switch when forming link bundles.

The Working Principle of MLAG

In MLAG links, Link Aggregation Control Protocol (LACP, 802.3ad) is typically used to negotiate north and south between the host and an MLAG virtual switch or between two virtual MLAG switches. East and west proprietary protocols are used between MLAG enterprise network switches that are members of the same virtual MLAG switch. Figure 1 shows the example of using multiple gigabit MLAG switches - FS S5850-48T4Q to form an MLAG Pair. With four leaf switches in an MLAG pair, you can build redundant connections from the server to the MLAG enterprise network switches. The LAG groups can be formed using static link aggregation or LACP-based negotiation methods.Form an MLAG Pair
Figure 1: Using FS S5850-48T4Q Switches to Form an MLAG Pair

Benefits of MLAG

  • Traffic is evenly distributed to each of the switches through the use of LAG hashing.

  • Simply bundle more links into the LAG to increase bandwidth for North & South as well as East & West

  • Offers stability with dual management and control planes

  • Able to upgrade one switch at a time without affecting other devices

  • Expands port capacity freely and simply adds another switch East or West by creating another MLAG to another switch

Interested in how to configure it, you can watch the following video, taking the FS S5800-8TF12S hyper-converged infrastructure switch as an example. 

What Is vPC?

 

vPC (Virtual Port Channel) is a Cisco Nexus technology where a Port Channel is a regular LAG. A Port Channel is a technology that provides a way to aggregate (bond) multiple interfaces together. Traffic is then load-balanced across each of the connections. It is a Cisco Nexus-specific protocol that is hard to configure on any other type of switch.

The Working Principle of vPC

vPC allows links physically connected with two different Cisco MLAG switches to appear as a single Port Channel to a third device. The third device can be an ethernet switch, a server, or any other networking device supporting IEEE 802.3ad Port Channels. vPC also allows the creation of Layer 2 Port Channels that span two switches.
As illustrated below, vPC is utilized to create inter-switch links spanning two MLAG switches while keeping two control planes of these MLAG switches separate. After you enable the vPC function, you create a peer keep-alive link, which sends heartbeat messages between the two vPC peer devices. The vPC domain includes vPC peer devices, the vPC peer keep-alive link, the vPC peer link, and all the Port Channels in the vPC domain connected to the downstream device. You can have only one vPC domain ID on each device.

Figure 2: Form a vPC Pair by Creating Inter-switch Links
 

Benefits of vPC

  • Allows a single device to use a Port Channel across two upstream devices

  • Eliminates Spanning Tree Protocol blocked ports

  • Provides a loop-free topology

  • Uses all available uplink bandwidth

  • Provides fast convergence if either the link or a device fails

  • Provides link-level resiliency

  • Helps ensure high availability

MLAG vs. vPC: 4 Key Differences

 

Both MLAG and vPC can create a port group between two switches and enable Layer 2 multipathing. In MLAG or vPC domain, each MLAG enterprise network switch is managed and configured independently and is able to forward/route traffic without passing to a master switch. Despite their similarities, they still differ in some ways.

Difficulty of implementation

 

Obviously, the biggest difference between them is the difficulty of implementation. MLAG is a public protocol that is supported by almost every vendor using their own custom rolled implementation, while vPC is a Cisco Nexus-specific protocol, not all the vendors have this technology. Thus, MLAG setup is a bit easier than vPC.

Compatibility issues

Another issue is compatibility. For vPC pairing, the same type of Cisco Nexus switches must be used. For example, it is not possible to configure vPC on a pair of switches including a Nexus 7000 series and a Nexus 5000 series switch. And the vPC peers must run the same NX-OS version except during the non-disruptive upgrade, that is, the In-Service Software Upgrade (ISSU).

Layer multipathing

 

Besides, the vPC peer link must consist of at least two 10G Ethernet ports in dedicated mode. vPC is more advanced than MLAG. It supports both Layer 2 and Layer 3 multipathing, which allows you to create redundancy by enabling multiple parallel paths between nodes and load-balancing traffic where alternative paths exist. If you want to enable Layer 3 multipathing, you could also use the Multi-Active Gateway Protocol (MAGP).

Application scenarios

Normally, vPC can only be used on Cisco Nexus data center switches, while MLAG can be applied to a wide range of scenarios. Whether in a traditional 3-tier data center architecture or a 2-tier spine-leaf architecture, switches that support MLAG can form an MLAG pair at different layers. All FS data center switches support MLAG. By using MLAG in data center network design, FS data center switches help deliver system level redundancy and improve network reliability.

 

Item MLAG vPC
Simplifies Network Design Yes Yes
Eliminates Spanning Tree Protocol (STP) Yes Yes
Multipathing Layer 2 Layer 2 & Layer 3
Difficulty of Implementation Easier Relatively Difficult
Switch Type for Pairing No requirement Strict Requirements
Using Scenarios Common seen in distribution or data center switches Usually in Cisco Nexus data center switches

Conclusion

 

Both MLAG and vPC are desirable implementations for data centers and cloud computing networks that require the highest level of network bandwidth and reliability. Before you decide on MLAG or vPC, the foremost thing is to make clear whether your networking devices can support MLAG or vPC. Then take account of your fabric architecture and your own specific needs to make an informed decision.

You might be interested in

Knowledge
See profile for Howard.
Howard
EVPN-VXLAN: How to Use It in Data Center
May 20, 2023
10.4k
Knowledge
See profile for Howard.
Howard
VXLAN: the Future for Data Center Networks
May 20, 2023
8.1k
Knowledge
See profile for Howard.
Howard
Using MLAG in Data Center Network Design
May 27, 2019
5.9k
Knowledge
See profile for Moris.
Moris
VPN vs MPLS: What’s the Difference?
Jul 8, 2022
58.3k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
390.7k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
369.4k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
339.3k
Knowledge