English

MTP/MPO Conversion Cable Wiki and Applications

Updated on Nov 25, 2021 by
5.0k

12-fiber MTP/MPO cables are widely used for 40G/100G high-density backbone cabling in data centers, streamlining network deployment and offering more flexibility. Meanwhile, the base-12 solution also brings about fiber wasting for utilizing only eight of the twelve fibers, which leads to a transition to a more cost-effective 8-fiber MTP/MPO system preferred in 40G/100G backbone networks. To solve this problem, MTP/MPO conversion cables become effective solutions for converting the previously designed base-12 backbone to the currently popular base-8 and base-24 backbones.

MTP/MPO Conversion Cable Overview

MTP/MPO conversion cables, also known as conversion harness cables, are designed with the same fanout form as MTP/MPO breakout cables but differ in fiber counts and types. They are terminated with only MTP/MPO connectors on both ends, making it especially fit for high-density cabling. Specifically, they can be used for 10G-40G, 40G-40G, 40G-100G, 40G-120G direct connections, which avoid fiber wasting and largely increase the capacity and flexibility of the existing base-12 and base-24 MTP/MPO cabling systems.

fig1.jpg

Figure 1: MTP/MPO Conversion Cable Types.

MTP/MPO Conversion Cable Applications

1×2 MTP/MPO conversion cables, 1×3 MTP/MPO conversion cables, 2×3 MTP/MPO conversion cables are designed with different structures fit for diverse connections.

1×2 MTP/MPO Conversion Cable

This MTP/MPO conversion cable is terminated with a 24-fiber MTP/MPO connector on one end and two 12-fiber MTP/MPO connectors on the other end, which enables a base-24 MTP cable to be integrated into the existing base-12 backbone MTP links to carry the signals. The transmitted data are split equally across two 12-fiber previously installed within the MTP/MPO system. As shown in Figure 1, the base-24 100G connection is converted into the 12-fiber MTP/MPO backbone trunks via 24-fiber to 2×12-fiber MTP/MPO conversion cables, so as to extend further value of the legacy infrastructures.

fig2.png

Figure 2: 100G Connection with 1×2 MTP/MPO Conversion Cable.

1×3 MTP/MPO Conversion Cable

This MTP/MPO conversion cable is terminated with a 24-fiber MTP/MPO connector on one end and three 8-fiber MTP/MPO connectors on the other end, which allows a base-24 backbone link to be converted into three base-8 cables so as to achieve 40G to 120G deployment. When connected to 40G, this conversion cable can create three 40G interfaces for QSFP+ modules, fully utilizing all the 24 fibers. Thus, three 40G dual-way transmissions are achieved in the existing 24-fiber MTP/MPO cable. In addition, 24-fiber to 3×8-fiber MTP/MPO conversion cables can be also used to break the 120G CXP module signals into three 40G QSFP+ links to realize the migration from 40G to 120G networking.

fig3.png

Figure 3: 40G-120G Connection with 1×3 MTP/MPO Conversion Cable.

2×3 MTP/MPO Conversion Cable

This MTP/MPO conversion cable is terminated with two 12-fiber MTP/MPO connectors on one end and three 8-fiber MTP/MPO connectors on the other end, which allows converting the signals from three four-channel modules to two 12-fiber trunks and achieves full utilization of the 12-fiber system. 2x12-fiber to 3×8-fiber MTP/MPO conversion cables can be used for 10G-40G and 40G-40G connections. In 10G-40G connection, the three 8-fiber MTP/MPO connectors can be plugged into three 40G QSFP+ transceivers on the switch. And the two 12-fiber ends are terminated with a 2x12-MTP to 12x duplex LC cassette, converting the three 40G signals to 12 x10G signals.

fig4.jpg

Figure 4: 10G-40G Connection with 2×3 MTP/MPO Conversion Cable.

As for the 40G-40G connection, the three 8-fiber MTP/MPO connectors of the 2×3 MTP conversion cable are linked to the three 40G QSFP+ transceivers on the switch. And the two 12-fiber MTP connectors of both two MTP conversion cables are plugged into MTP 12-fiber adapters. In this way, the Base-8 MTP links are able to transmit on the existing Base-12 cabling system to fully leverage the fiber resource.

fig5.jpg

Figure 5: 40G-40G Connection with 2×3 MTP/MPO Conversion Cable.

Conclusion

MTP/MPO conversion cables are designed to provide a more flexible high-density cabling system. It can largely increase the capacity of the existing 12-fiber and 24-fiber MTP/MPO networks and is also a cost-effective solution for 40G/100G/120G connections. Three existing MTP/MPO conversion cable types are fit for different networking environments. You can choose suitable ones according to your current demands and future network migration planning.

Related Resource:

MTP® High-Density Data Center Cabling Solution

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
390.8k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
369.4k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
339.4k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
423.1k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
298.6k