Network Security
What is Network Security?
Network security protects the underlying network infrastructure from unauthorized access, misuse, or theft. It involves the creation of a secure infrastructure so that devices, applications, users, and applications can operate in a secure manner.
Businesses use network security to:
-
Protect business information
-
Manage and ensure network accessibility
-
Prevent intrusions
-
Address and rectify incidents
-
Secure physical devices (such as routers, switches, firewalls), software, and proprietary knowledge
-
Protect data centers and cloud computing
Network Security and Data
These data elements are the foundation of network security:
-
Data access - The access to data is managed by a mechanism that enforces the Triple-A (AAA) protocol – authenticating, authorizing, and auditing users. This involves verifying user identity (typically via a login or personal identification number), assigning access and privileges according to users' roles, and documenting modifications to data as well as tracking user interactions within the network.
-
Data availability - Data is accessible to users as required (on-demand availability); only users with proper authorization have the capability to access and utilize the data.
-
Data confidentiality-Unauthorized individuals are prevented from obtaining or utilizing data; through the use of data encryption, the transfer of information is secured, thus thwarting any illicit access attempts by external entities.
-
Data integrity–Alterations to data are prohibited without proper authorization; this principle ensures that only appropriately authorized users have the privilege to access and amend the information.
Network Security and Protection
The traditional approach to network security, which focused on fortifying the network's edge through the use of firewalls, has become insufficient. The majority of cyber threats and incursions stem from the web, emphasizing the importance of solidifying internet-facing interfaces. Other prevalent sources include devices compromised by users and devices used by mobile peers. The intricate nature of network structures and their communications often compromises the security of internal and external interactions. Networks face a risk from various types of assaults, including both proactive and passive strategies, as well as threats originating from within or targeting the core from the outside. Proactive forms of attacks, like denial-of-service (DoS) onslaughts, falsifying IP addresses also known as masquerade attacks, and viruses aimed at disrupting both tangible servers and virtual machines (VMs), pose especially challenging security issues. These target the control plane, which is the section of the network infrastructure responsible for signaling and routing decisions.
A change in mindset is required for the future of network security:
Security must be embedded everywhere-in the protocols, systems, elements, provisioning, and business that surround the network. To better combat and contain network security threats, service providers are moving to a more distributed architecture. This enables detection and enforcement everywhere. You can have automated and centralized security policies with decentralized enforcement at switches and routers driven by dynamic and real-time security updates as the threat environment changes and accelerates. With software-defined controls, you can detect threats and enforce security policies with high levels of automated security, unified threat detection, and real-time protection.
Currently, network security overseers must adopt a stance of zero trust towards all components within the network, while service providers are aiming to manage their networks as a unified enforcement zone. In this environment, every single element—beyond just the boundary points—serves as a checkpoint for policy implementation.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023