Optimize Data Center Cabling with FS HD LC Uniboot Push-Pull Patch Cables
Oct. 24th, Shenzhen, FS News– FS HD LC uniboot push-pull patch cables with integrated push-pull tab and unique QuickFlip polarity reversal design are the ideal solution for high-density patching environments, which allow users to easily manage more cables in a tight space.
As today’s networking environment becomes increasingly dependent on high-speed and high-density solutions, effective cable management also becomes more intractable than before. How to manage more cables in a smaller amount of space? Maybe you will think of the LC uniboot patch cables. FS LC uniboot patch cable utilises a special “round duplex” cable that allows duplex transmission within a single 3.0mm cable, which reduces cable management space by up to 70% comparing to standard LC patch cables. Besides, it has a unique QuickFlip polarity reversal design allows the fiber polarity to be easily reversed without the use of any tools, allowing this cable to facilitate improved airflow within a data center.
However, LC uniboot patch cable cannot meet the high-density cabling needs very well due to some design shortcomings. Therefore, FS also introduced a kind of HD LC patch cable. Similarly as LC uniboot patch cable, HD LC patch cable also has an uniboot connector design for neater and denser cable management. But unlike LC uniboot patch cable, HD LC patch cable is designed with a push-pull tab on top of the uniboot connector, which allows users easy accessibility in tight areas when deploying very high-density LC patch fields in data center applications. Besides, insertion Loss of our HD LC patch cable is available in 0.3dB standard types for common cabling applications and 0.1dB bend insensitive types for high-density applications.
Compared to LC uniboot patch cable, HD LC uniboot push-pull patch cable is more flexible and more convenient, which allow for rapid deployment of high-density permanent links in a single assembly for data center applications requiring high bandwidth, extended reach, and extremely low insertion loss. FS HD LC patch cables are available in single-mode types and 10G OM3 and 10G OM4 multimode types with PVC jacket or LSZH jacket. The lengths range from 1 m, 2 m, 3 m, 5 m to 10 m, 15 m and 20 m. Custom service is also available for your special requirements. For more details, please visit www.fs.com or contact over sales@fs.com.
FS is a leading manufacturer and supplier of fiber optic subsystems, components and solutions. With last four years growing, we have built our strong and professional teams in optical communication product R&D, systematic solution and supply chain management. Nowadays, we are doing business with more and more worldwide well-known corporations like CloudFlare, EXFO, Apple, MRV, JDSU, ADTRAN, Avago, EMC, etc., who have put large volume of our products into production for their Data Center or Cloud Computing application and speak highly of our service and products. We will be working together with our customers, partners and co-workers to benefit them more and contribute more to the global popularity of optical communication.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023