English

PC vs UPC vs APC Connector: Selecting the Right Fiber Connector Type

Updated on Dec 22, 2021 by
139.6k

When choosing fiber optic cables or fiber connectors, you may find that the description of the product noted the word “PC Polish”, “UPC Polish” or “APC Polish”. What do these words mean? What’s the difference between these connector types? This post will shed light on these connector types and their differences for you.

Introduction to Different Connector Types

To put it simply, PC, UPC, and APC refer to the polish styles of the ferrules inside the fiber optic connectors, just as the following figure shows. The ferrule is the housing for the exposed end of a fiber, designed to be connected to another fiber, or into a transmitter or receiver. When connectors are installed on the end of a fiber, light is reflected back up the fiber towards the source, disrupting the signal. To increase the efficiency of fiber, engineers began to upgrade the surface of the critical point of attachment, and that’s how ferrule polish technologies are introduced. There are four connector polish types, three of which will be highlighted below.

Ferrule polish.png

Figure 1: Ferrule polish

PC Fiber Connector

PC fiber connector refers to the connector that is polished in the physical contact style. It is the most common polish type that is found on OM1 and OM2 multimode fiber. PC fiber connector was generated to overcome the air gap between two surfaces from small imperfections in the original flat fiber connector. In PC fiber connector design, there is a slightly cylindrical cone head with the aiming to eliminate the air gap, so that the typical return loss in single mode applications is about -40dB, higher than the return loss of the original flat polish style (-14 dB or roughly 4%). Up to now, this polish style has been outdated and the evolution - UPC polish style has come into being.

PC.jpg

Figure 2: PC fiber connector

UPC Fiber Connector

UPC is the acronym for Ultra Physical Contact. It is an improvement of the PC fiber connector with a better surface finish after an extended polishing and the return loss is better than PC structure, nearly -50dB or higher. Though it has a relatively lower back reflection in comparison with the PC connector, it is not robust enough. Note that repeated connections and disconnections will bring about the degradation of the surface and ultimate performance.

UPC.jpgFigure 3: UPC fiber connector

APC Fiber Connector

Out of the pursuit of lower back reflection, APC fiber connectors were developed. APC refers to Angled Physical Connect, the ferrule endface radius of which is polished at an 8°angel, minimizing the back reflection as a result. Since adding the angled endface, the reflected light will leak out into the cladding instead of staying in the fiber core. It should be noted that APC connectors should only be mated with other angled-polished connectors rather than non-angled polished connectors, or it will cause very high insertion loss. The optical return loss of APC connectors is -60dB or higher, better than the other connector types.

APC.jpgFigure 4: APC fiber Connector

PC vs. UPC vs. APC: What Are Their Differences?

After the definition of three connector types, you will find that PC, UPC, and APC connectors vary in many aspects. The following lists their differences in appearance, performance, and application categories.

Appearance

The major difference in terms of appearance is the fiber endface. PC connectors and UPC connectors are both polished with no angle, though endface of UPC has a slight curvature. Instead, an APC connector is featured with 8° angle endface.

Another obvious difference is the color. It is visible to distinguish which type of polish style the connector features by the color of the connector body. Take an FS LC APC single mode fiber optic patch cable as an example, the connectors on both fiber ends are all green. While for an LC UPC single mode fiber optic patch cable, the connectors are generally blue. It is also a simple way to tell these connectors apart.

LC UPC VS LC APC.pngFigure 5: LC/UPC VS LC/APC

Performance

It used to be hard to achieve low insertion loss using APC connectors owing to the air gap in the apex offsets, yet nowadays the improvement of connector design and manufacturing push APC connectors to perform better. The insertion difference between APC and UPC has been diminished.

As for the performance of return loss, you may have noticed APC connectors have the lowest back reflection of all the fiber connectors mentioned owing to the angled endface. For this reason, the values of the return loss are different. According to the industry standards, the return loss of PC, UPC, and APC connectors is respectively about -40dB, -50dB, and -60dB or higher. The higher the return loss is, the lower the reflection and the better the connector performance will be. It proves that APC connectors are higher-performing among the connectors listed.

Application

Since some applications are more sensitive to return loss, APC connectors are preferred in these fields, for instance, in higher wavelength range like those used for RF video signals, especially FTTx applications and for applications such as passive optical networks and other WDM systems using high wavelength via single mode fiber.

For those applications where return loss is not paid much attention to, UPC or PC comes into play. PC connectors are generally seen in telecom operators' equipment, while UPC connectors are popular in digital TV, telephony and data systems.

Conclusion

It is improper to say whether PC, UPC or APC is the best polish type of fiber connectors. When choosing fiber connectors for specific applications, factors such as cost and operability should be considered. However, there is one rule that should be followed: for those applications which high precision optical fiber signaling matters, choose APC; for less sensitive digital systems, PC or UPC is capable.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k