Terminal Anti-Spoofing
What Is Terminal Anti-Spoofing?
Terminal anti-spoofing involves technologies for the detection, oversight, and governance of terminal devices. It acquires an understanding of the traffic patterns exhibited by legitimate terminals and uses this information to establish a model of expected traffic behavior. This established model aids in the recognition of counterfeit terminals. When such impersonated terminals are detected, the system promptly enacts strategies to quarantine them.
What Are Application Scenarios of Terminal Anti-Spoofing?
For example, the scenario depicted in the diagram below, where simple devices like printers, IP cameras, and IP phones gain network access via switches. Illegitimate terminals might mimic the IP or MAC addresses of authorized devices to launch attacks on the network. Consequently, it is advisable to activate the terminal anti-spoofing feature on access switches (such as SwitchA and SwitchB in the illustration) to detect and manage the access permissions of these fabricated terminals.
Application scenario of terminal anti-spoofing
Using printers as an illustrative case, this description outlines the protocol for information cataloging, detecting deviations, and enforcing isolation directives on terminals to prevent spoofing. This procedure is depicted in the accompanying diagram.
Interaction process for terminal anti-spoofing
Here’s a breakdown of the fundamental interaction sequence:
Initially, the network administrator sets up the terminal anti-spoofing feature on the switch. This setup includes registering details of the terminals, activating global anomaly detection, enabling detection for particular terminal categories, and establishing a policy for quarantining suspect terminals.When a legitimate terminal connects to the network, it communicates with the switch, which in turn intercepts ARP packets from the terminal.
The switch then aligns the information about the terminal, as entered manually by the administrator, with the ARP packets broadcast by the sanctioned terminal. Upon a successful match, and since the switch has global anomaly detection activated, it proceeds to create a corresponding terminal entry.The switch recognizes that the legitimate terminal adheres to the specific terminal type set for anomaly monitoring. It then records and scrutinizes the terminal's traffic behavior using sophisticated algorithms, ultimately concluding that the terminal's traffic pattern is consistent with normal activity.
Later on, a rogue terminal mimics the MAC or IP address of the legitimate terminal, attempts to connect to the network via the switch, and tries to mount an assault.
At this juncture, the switch observes and evaluates the traffic characteristics of the impersonating terminal with the same algorithms and identifies anomalies in its behavior. As a response, the switch enforces the predetermined isolation policy against this fraudulent terminal, thereby restricting its network access and effectively isolating it.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023