English
Posted on Aug 7, 2023
1.0k
Overview
There is no denying that DWDM technology has been the preferred solution for enterprises used in long-haul transmission for its unique advantages such as increasing bandwidth and maximum utilization of fiber. Our client needed a DWDM solution to achieve 10G data transmission, which allows network expansion in three sites.
- Challenge 1The customer wanted to deploy a DWDM network, including 3 links among 3 sites.
- Challenge 2Site A to B 16.8 km, Site B to C 26.05 km, Site A to C 42.85 km. And there was no power in site B.
- Challenge 3Ensuring end-to-end connectivity to meet present and future business demands.
Approach
Results
- Efficient Long-Distance Network Transmission Across Three SitesIn response to the customer's need to build three sites for network transmission, the FS technical team deployed two pairs of 16CH DWDM multiplexers/demultiplexers in the 42.85km long-distance transmission between site A and site C. And considering the customer's future network expansion, 8 channels are reserved between every two sites for future transmission.
- EDFA Enhances Signal Transmission to Reduce Fiber LossDue to the lack of power supply at site B and significant fiber loss during transmission, both site A and site C adopted EDFA. By introducing a preamplifier on the transmit side of the fiber end, the optical signal is enhanced.
- Achieving Signal Adaptation to Ensure Transmission EfficiencyTo further improve the network transmission efficiency at customer B site, FS technical team installed optical attenuators. This ensured the signals transmitted by the switch were consistent with those from A to C sites, achieving EDFA gain equalization. Additionally, an attenuator was added after the OPA to keep the TX value of the 10G DWDM transceiver within the proper range.
Tech support
First name
Last name
Email address
Details
0/5000
Case studies
News Letter
Email Address
Videos
01:28
Nov 20, 2023
656
0
FS Same Day Shipping Ensures Your Business Success
Recent Trend
Hot Tags
Popular
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023