English

Typical Home Network Building with Wireless LAN Access Points

Background

The increasing popularity of mobile terminals equipped with wireless local area network (LAN) functions has driven the installation of wireless LAN access points (APs) in families. Our customer prepared to build a home network with FS router, PoE+ switches, APs and fiber related products, but encountered some issues while installing. The following part illustrates the program designed by us and how it is put into use with the help our solution team.

Challenge

1. There are four VLANs, as shown in the table below. Only the management VLAN 16 is allowed to have access to all VLANs. The rest VLAN are all isolated from each other.

VLAN ID Name Device Included Port Allocation
VLAN 16 Management FS Router, S5500-48T8SP Switch, S1150-8T2F Switches, printers, NAS, (AP) Home WiFi Port 37-38 on S5500-48T8SP, Port 7-8 on S1150-8T2F (1st Floor), Port 2,4,6,8 on S1150-8T2F (2nd Floor)
VLAN 26 Security NVR, IP Cameras Port 17-24 on S5500-48T8SP, Port 1,3,5,7 on S1150-8T2F (2nd Floor)
VLAN 36 IoT Devices TVs, Smart Home System Port 27-28 on S5500-48T8SP, Port 1-6 on S1150-8T2F (1st Floor)
VLAN 56 Guest WiFi (AP) Guest WiFi Port 3-8 on S5500-48T8SP

2. A port on the router needs to act as the gateway of four VLANs.

3. The AP possesses dual SSID. Our customer wants to segregate them and assign them with DHCP addresses.

Solution

Configure the Access Control List at the TE1 port of S5500-48T8SP connecting to the router, so as to reject the mutual visits from VLAN 56, VLAN 26 and VLAN 36, and to allow the passage of all VLANs, that is to say, all VLAN can have access to VLAN 16.

Configure four sub-interfaces on S5500-48T8SP. S5500-48T8SP POE+ switches support APs, camera and TV while connecting the S3900-24T4S switch via the trunk link through which the tagged frame can be transmitted. The LACP is configured on the two fiber links between SS5500-48T8SP and S3900-24T4S, increasing the bandwidth and redundancy.

Allocate the two SSID into different VLAN under the bridge mode of the AP. Configure the link between wireless AP and S5500-48T8SP as the trunk link to realize the transmission of tagged frame from different VLAN and the management of APs.


topology

Conclusion

This solution is for a home network concerning VLAN, ACL, DHCP, NAT, subinterface, and Wi-Fi, taking into consideration both the cost efficiency and network redundancy. “The engineer is a great help, patient with me, I am learning as well”, said our customer who is satisfied with the whole solution.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k