English
Image from FS Community media library
Posted on May 31, 2022 by
3.2k
Image from FS Community media library

Adding a fiber link to my home network

Motivation

Despite using a FTTH internet connection since 2014, aside from the one fiber uplink, I had always used network gear with 1 Gbit/s links over regular old rj45 cat5(e) cables.

 

I liked the simplicity and uniformity of that setup, but decided it’s time to add at least one fiber connection, to get rid of a temporary ethernet cable that connected my kitchen with the rest of my network that is largely in the living room and office.

The temporary ethernet cable was an experiment to verify that running a server or two in my kitchen actually works (it does!). I used a flat ethernet cable, which is great for test setups like that, as you can often tape it onto the walls and still close the doors.

So, we will replace one ethernet cable with one fiber cable and converters at each end:

0.9mm thin fiber cables

Why is it good to switch from copper ethernet cables to fiber in this case? Fiber cables are smaller and hence easier to fit into existing cable ducts. While regular ethernet cable is way too thick to fit into any of the existing ducts in my flat, I was hoping that fiber might fit!

When I actually received the cables, I was surprised how much thinner fiber cables actually can be: there are 0.9mm cables, which are so thin, they can be hidden in plain sight! I had only ever seen 2mm fiber cables before, and the 0.9mm cables are incredibly light, flexible and thin! Even pasta is typically thicker:

Preparing a delicious pot of glass noodles ;)

Preparing a delicious pot of glass noodles ;)

The cable shown above comes from the fiber store FS.com, which different people have praised on multiple occasions, so naturally I was curious to give them a shot myself.

Also, for the longest time, it was my understanding that fiber connectors can only be put onto fiber cables using expensive (≫2000 CHF) machines. A while ago I heard about field assembly connectors so I wanted to verify that those indeed work.

Aside from practical reasons, playing around with fiber networking also makes for a good hobby during a pandemic :)

 

Hardware Selection

I ordered all my fiber equipment at FS.com: everything they have is very affordable, and products in stock at their German warehouse arrive in Switzerland (and presumably other European countries) within the same week.

If you are in the luxurious position to have enough physical space and agility to pull through an entire fiber cable, without having to remove any connectors, you can make a new network connection with just a few parts:

I recommend buying an extra fiber cable or two so that you can accidentally damage a cable and still have enough spares.

Total cost thus far: just under 100 CHF. If you have existing switches with a free SFP slot, you can use those instead of the media converters and save most of the cost.

If you need to temporarily remove one or both of the fiber cable connector(s), you also need field assembly connectors and a few tools in addition:

I recommend buying twice the number of field assembly connectors, for practicing.

Personally, I screwed up two connectors before figuring out how the process goes.

Total cost: about 160 CHF for the field assembly equipment, so 260 CHF in total.

To boost your confidence in the resulting fiber, the following items are nice to have, but you can get by without, if you’re on a budget.

With the visual fault locator, you can shine a light through your fiber. You can verify correct connector assembly by looking at how the light comes out of the connector.

The fiber cleaning swabs are good to have in general, but for the field assembly connector, you need to use alcohol-soaked wipes anyway (which FS.com does not stock).

The total cost for everything is just under 300 CHF.

 

Hardware Selection Process

The large selection at FS.com can be overwhelming to navigate at first. My selection process went something like this:

My first constraint is using bi-directional (BiDi) fiber optics modules so that I only need to lay a single fiber cable, as opposed to two fiber cables.

The second constraint is to use field assembly connectors.

If possible, I wanted to use bend-insensitive fiber so that I wouldn’t need to pay so much attention to the bend radius and have more flexibility in where and how I can lay fiber.

With these constraints, there aren’t too many products left to combine. An obvious and good choice are 0.9mm fiber cable using LC/UPC connectors.

 

FS.com details

As of 2020-08-05, FS.com states they have 5 warehouses in 4 locations:

  • Delaware (US)

  • Munich (Germany)

  • Melbourne (Australia)

  • Shenzhen (China)

They recently built another, bigger (7 km²) warehouse in Shenzhen, and now produce inventory for the whole year.

By 2019, FS.com had over 300,000 registered corporate customers, reaching nearly 200 million USD yearly sales.

 

Delivery times

As mentioned before, delivery times are quick when the products are in stock at FS.com’s German warehouse.

In my case, I put in my order on 2020-Jun-26.

The items that shipped from the German warehouse arrived on 2020-Jul-01.

Some items had to be manufactured and/or shipped from Asia. Those items arrived after 3 more weeks, on 2020-Jul-24.

Unfortunately, FS.com doesn’t stock any 0.9mm fiber cables in their German warehouse right now, so be prepared for a few weeks of waiting time.

 

Laying The Fiber

Use a cable puller to pull the fiber through existing cable ducts where possible.

  • In general, buy the thinnest one you can find. I have this 4mm diameter cable puller, but a 3mm or even 2mm one would work in more situations.

  • I found it worthwhile to buy a brand one. It is distinctly better to handle (less stiff, i.e. more flexible) than the cheap one I got, and thinner, too, which is always good.

In my experience, it generally did not work well to push the fiber into an existing duct or alongside an existing cable. I really needed a cable puller.

If you’re lucky and have enough space in your duct(s), you can leave the existing connectors on the fiber. I have successfully just used a piece of tape to fix the fiber connector on the cable puller, pushing down the nose temporarily:

fiber cable taped to cable puller

Where there are no existing ducts, you may need to lay the fiber on top of the wall. Obviously, this is tricky as soon as you need to make a connection going through a wall: whereas copper ethernet cables can be bent and squeezed into door frames, you quickly risk breaking fiber cables.

Luckily, the fiber is very light, so it’s very easy to fix to the wall with a piece of tape:

fiber cables on the wall

You can see the upstream internet fiber in the top right corner, which is rather thick in comparison to my 0.9mm yellow fiber that’s barely visible in the middle of the picture.

Note how the fiber entirely disappears behind the existing duct atop the door!

Above, you can see the flat ethernet cable I have been using as a temporary experiment.

Where there is an existing cable that you can temporarily remove, it might be possible to remove it, put the fiber in, and put the old cable back in, too. This is possible because the 0.9mm fiber cable is so thin!

I’m using this technique to cross another wall where the existing cable duct is too full, but there is a cable that can be removed and put back after pulling the fiber through:

fiber cable next to existing cable

…and on the other side of the wall:

fiber cable next to existing socket

Note how the fiber is thin enough to fit between the socket and duct!

Note: despite measuring how long a fiber cable I would need, my cable turned out too short! While the cable was just as long as I had measured, with distances exceeding 10m, it is a good idea to add a few meters spare on each side of the connection.

 

Field assembly connectors

To give you an overview, these are the required steps at a high level:

I thought the following resources were useful:

Beware: the little paper booklet that comes with the field assembly connector contains measurements which are not to scale. I have suggested to FS.com that they fix this, but until then, you’ll need to use e.g. a tape measure.

For establishing an intuition of their different sizes, here are the different connectors:

fiber cable connectors
  • 2.0mm fiber cable

  • cat6 ethernet cable

  • 0.9mm fiber cable (LC/UPC factory)

  • 0.9mm fiber cable (LC/UPC field assembly connector)

The 0.9mm fiber cables come with smaller connectors than the 2.0mm fiber cables, and that alone might be a reason to prefer them in some situations.

The field assembly connectors are pretty bulky in comparison, but since you can attach them yourself after pulling only the cable through the walls and/or ducts, you usually don’t care too much about their size.

 

Conclusion

Modern fiber cables available at FS.com are:

  • thinner than I expected

  • more robust than I expected

  • cheaper than I expected

  • survive tighter bend radiuses than I expected

Replacing this particular connection with a fiber connection was a smooth process overall, and I would recommend it in other situations as well.

I would claim that it is totally feasible for anyone with an hour of patience to learn how to put a field assembly connector onto a fiber cable.

If labor cost is expensive in your country or you just like doing things yourself, I can definitely recommend this approach. In case you mess the connector up and don’t want to fix it yourself, you can always call an electrician!

Stay tuned for the next part, where I upgrade the 1G link to a 10G link!


Original Source: Michael Stapelberg Blog - Adding a fiber link to my home network (2020)

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k