English

Still Worried About Bend Radius? Come and See the Bend-Insensitive Fiber Optic Cables

Updated on Dec 22, 2021 by
36.1k

Fiber optic market has witnessed the increased use of optical fiber cable assemblies. FTTx networks are the impetus for the adoption of fiber cables. During installation of these cables, more attention is focused on the effects of bend radius and the need to maintain a specified cable bend radius. So far, are you still worried about bending the fiber optic cables? Bend insensitive fiber optic cable can help you solve this problem.

 

Bend Radius of Fiber Optic Cable

Because fiber optic cable is sensitive to stress, light may leak out when the fiber is bent. As the bending becomes more acute, more light leaks out (shown in the picture below). Therefore, when installing fiber patch cables, especially in tight spaces of high-density fiber patching areas, you are not supposed to bend them beyond their bend radius. What exactly is the bend radius?

Bend Radius of Fiber Optic Cable

Figure 1: Bend Radius of Fiber Optic Cable

What Is Bend Radius and Minimum Bend Radius of Fiber Optic Cable?

Bend radius refers to the minimum radius an ethernet cable or fiber optic cable can be bent without causing damage to the cable or affecting its performance. It is a crucial parameter to consider during installation to ensure longevity and efficiency of fiber optic cable. When a fiber optic cable is bent excessively, the optical signal within the cable may refract and escape through the fiber cladding. Bending can also permanently damage the fiber by causing micro cracks. The result is known as bend loss: a loss of signal strength that may compromise the integrity of the data transmission.

Note: Excessive pulling tension and overly tight fasteners can also cause transmission problems and micro-bends in fiber optic cables.

Minimum Bend Radius of Fiber Optic Cable

Figure 2: Minimum Bend Radius of Fiber Optic Cable

The minimum bend radius is the smallest allowable radius for a given fiber optic cable to be bent around. The new standard ANSI/TIA/EIA-568B.3 sets performance specifications, minimum bend radius standards and maximum pulling tensions for 50/125-micron and 62.5/125-micron fiber optic cables. For inside plant cable, the fiber cable bend radius is 10 times the cable’s outside diameter under no pull load, and 15 times the cable’s outside diameter when subject to tensile load.

How to Calculate Bend Radius of Fiber Optic Cable?

In generally, the allowable bend radius varies based on fiber cable types, outside diameter (OD), and the condition of the cable under stress both during installation (tensile load) and after installation when the cable is reset (no-load). The following formula is used to calculate bend radius:
Minimum Bend Radius = Cable Outer Diameter x Cable Multiplier

The cable multiplier is determined by industry standards and cable type. For fiber optic cables, the cable multiplier is six times for cables rated 5000 volts or less, eight times for cables rated over 5000 volts.

 

What Is Bend Insensitive Fiber Optic Cable & Its Types?

Bend insensitive fiber patch cable is designed to transmit light with minimum loss even if they are bent beyond the bend radius. In these BIF optical cables, an optical “trench” - a ring of lower index of refraction material - is built into the fiber to basically reflect the lost light back into the core of the fiber, thereby minimizing data loss. Bend insensitive fiber cable offers greater flexibility in demanding environments than traditional fiber cable. It is typically used in data centers or any space constrained area where tight bends and flexibility are required. In terms of fiber cable types, like regular fiber optic cables, bend-insensitive fiber also has two major types: bend single mode fiber (9/125 SMF) and bend insensitive multi-mode fiber (50/125 OM1/2/3/4/5 MMF).

 

 Bend Insensitive Fiber

Figure 3: Bend Insensitive Fiber

Bend Insensitive Multimode Fiber Optic Cable (BIMMF)

Multimode fiber is popular in data centers and intra-building backbones. In the era of increased connectivity, more demands on the quality and performance of link components become more critical. New bend insensitive multimode fiber minimizes bend-induced attenuation, which helps maximize system reliability and minimize downtime. These BIMMF cables are available in all laser optimized grades, OM1, OM2, OM3 , OM4 and OM5 and achieve 10 times less signal loss in tight bend scenarios. The fiber can be installed in loops as small as 7.5mm radius with less than 0.2dB bending loss at 850nm and 0.5dB at 1300nm.

 Bend Insensitive Multimode Fiber Optic Cable (BIMMF)

Figure 4: Bend Insensitive Multimode Fiber Optic Cable (BIMMF)

Bend Insensitive Single-mode Fiber Optic Cable (BISMF)

In 2007, a new type of “bend-insensitive” single mode fiber was introduced. It can withstand stress from bending, twisting, or stretching without suffering significant performance loss. ITU recommendation G.657 specifies two classes of single mode bend insensitive fiber patch cables: G.657 A and G.657 B. The minimum bend radius of G.657. A1 fibers is 10mm, of the G.657. A2 and G.657.B1 fibers is 7.5mm and of the G.657.B2 fibers is 5mm. Compared with minimum bend radius of the standard single mode G652 fibers which is usually 30 mm, G.657 single mode bend insensitive fiber patch cables are much more flexible. Thus, BISMF cables can be confidently installed with a variety of installation methods and in the increasingly high-density application spaces of today’s data center.

 Bend Insensitive Single-mode Fiber Optic Cable (BISMF)

Figure 5: Bend Insensitive Single-mode Fiber Optic Cable (BISMF)

 

Advantages of Bend Insensitive Fiber Optic Cable

Flexible Installations: Bend insensitive fiber optic cables are highly suitable for indoor fiber cable installations as they can now be taken around walls, pillars, ceilings, ducts, and other uneven surfaces within the buildings without concerns about excessive fiber bends.

High Performance: Higher bandwidth applications can be confidently deployed using bend insensitive fibers as accidental excessive bending of fibers does not cause much of performance degradation.

Great Resilience: Bend insensitive fibers also show a great deal of resilience in situations where fibers are fixed to surfaces using clamping, tie-wrapping or stapling.

Small Incremental Cost: Compared to cabling regular fiber optic cables, the cost of cabling bend-insensitive fiber cables is not very high.

Same Splicing Methods: Bend insensitive fiber cables can be spliced using the same methods as the standard cables.

Compatibility of Bend Insensitive Fiber Optic Cable

Bend insensitive fiber optic cable has so many advantages. One question may arise: are these BIF optical cables compatible with regular fibers? The answer seems to be yes for all SMF cables. Since only one mode is guided in the core, the trench has a minimal impact on system performance and measurement. But for MMF cables, it is less clear. Measurement of core size, differential mode delay (DMD) and bandwidth was developed prior to the introduction of BIMMF designs. These measurements are in the process of being evaluated and updated, so measurement results may depend on the manufacturer of the BIMMF.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
384.5k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
366.9k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
334.0k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
419.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
293.2k