English

A Comprehensive Guide to Optical Chips

Posted on Aug 23, 2024 by
248

10-100G Module

Optical transceivers play a crucial role in modern communication networks, particularly in high-speed data transmission and large-scale network deployments. At the heart of these transceivers are optical chips, which directly influence their performance and stability. Different brands of chips offer distinct technological features and are suited to various applications. This article delves into the characteristics of mainstream optical transceiver chip brands and their unique attributes.

Introduction to Optical Chips

Optical chips, typically referred to as photonic chips, use light waves (electromagnetic waves) as carriers for information transmission or data processing. These chips rely on integrated optics or silicon photonics waveguides to transmit modulated light signals, integrating functions such as modulation, transmission, and demodulation of optical and electrical signals onto a single chip.

Optical chips are processed and packaged into Transmitter Optical Sub-Assemblies (TOSA) and Receiver Optical Sub-Assemblies (ROSA), which are then further integrated with electronic chips and structural components to form optical transceivers. As the foundational component for converting optical and electrical signals, the performance of optical chips is crucial for the transmission efficiency of optical communication systems. They are widely used in scenarios like data communications, telecommunications, and fibre optic access, making them indispensable components in modern networks.

Types of Optical Chips

Types of Optical Chips

In applications such as optical communications, optical chips refer to both laser chips and detector chips. These chips form a vital part of optoelectronic devices and represent cutting-edge research in modern optoelectronic and microelectronic technology.

Key Brands of Optical Chips

The global optical chip industry has gradually matured, with representative chip brands spanning from foundational research to manufacturing processes and commercial applications. Leading brands include Intel, Broadcom, Marvell, MACOM, and Mellanox, each with its strengths and ideal applications.

Intel

Intel's optical transceiver chips are known for their data processing capabilities, making them widely used in data centres and high-performance computing environments. Intel's innovations in silicon photonics technology also enable more compact and efficient data handling.

Advantages:

  • Powerful Data Processing: Intel chips excel in handling large volumes of data, making them suitable for cloud computing and data centres.

  • Unique Integration Technology: Intel’s hybrid laser wafer technology and direct integration methods lead to higher reliability and lower costs.

Disadvantages:

  • Relatively High Power Consumption: In high-performance modes, Intel chips tend to consume more power than some other brands.

  • Higher Price: Intel’s high-end chips are costly, and may not be suitable for projects with limited budgets.

Broadcom

Broadcom is one of the largest global manufacturers of optical transceivers and a key supplier of optical chips, mainly based on GaAs technology. They develop and produce low-speed laser chips such as 2.5G, 10G, and 25G, primarily used in FTTx fibre access applications.

Advantages:

  • High Performance: Broadcom chips typically feature high integration and energy efficiency, excelling in high-density data centres and networks.

  • Good Compatibility: Broadcom chips are widely compatible with systems and devices from different manufacturers, making integration easier.

Disadvantages:

  • Higher Cost: Broadcom's high-end chips are relatively expensive, which might increase the overall solution cost.

  • Strong Supply Chain Dependence: Broadcom’s dominance in the market could lead to supply chain dependency.

Marvell

Marvell’s chips are known for their high flexibility and adaptability, making them suitable for a variety of optical transceiver applications, including long-distance transmission. In 2021, Marvell Technology acquired Inphi, expanding its influence in the data centre and 5G network infrastructure sectors.

Advantages:

  • High Flexibility: The flexible chip design supports various protocols and interfaces, meeting different network requirements.

  • Low Power Consumption: Compared to other brands, Marvell’s chips excel in power management.

Disadvantages:

  • Powerful Smaller Market Share: Despite its advanced technology, Marvell’s market share is somewhat lower than giants like Broadcom.

  • Limited Ecosystem Support: Marvell’s ecosystem support is relatively limited compared to Broadcom.

MACOM

MACOM specialises in high-frequency and optoelectronic integration technology. Its optical transceiver chips perform exceptionally well in high-speed applications and complex optoelectronic integration, making them widely used in 5G networks and data centres.

Advantages:

  • Outstanding High-Frequency Performance: MACOM chips excel in high-frequency and millimetre-wave applications, ideal for 5G and high-speed data centre uses.

  • High Optoelectronic Integration: MACOM’s strength lies in optoelectronic integration, providing efficient solutions in complex optoelectronic systems.

Disadvantages:

  • High R&D Costs: Due to its focus on the high-end market, MACOM's research and development costs are high, leading to more expensive products.

  • Intense Competition: MACOM faces strong competition from giants like Broadcom in the high-end market, limiting its market share.

NVIDIA Mellanox

Mellanox optical transceiver chips are designed for high-performance computing and data centre networks, supporting ultra-high bandwidth and low-latency data transmission. Their products are mainly used in InfiniBand and Ethernet, widely employed in high-performance computing clusters and large data centres that require high throughput and low latency.

Advantages:

  • Low-Latency Design: Mellanox chips are renowned for their extremely low latency, making them ideal for latency-sensitive applications like financial trading, scientific computing, and ML training.

  • Hardware Acceleration: Mellanox chips integrate many dedicated hardware acceleration features, such as RDMA (Remote Direct Memory Access) and Virtual Switch Acceleration (VSA), significantly enhancing efficiency in high-performance computing environments.

Disadvantages:

  • High Cost: Mellanox chips are primarily targeted at the high-end market, focusing on high-performance computing and data centres, resulting in higher product costs.

  • Narrower Ecosystem: Mellanox chips hold an advantage in high-performance computing and data centre markets but have relatively weaker ecosystem support in broader markets.

Selecting the Right Optical Chips

Choosing the right optical transceiver chip is critical in modern data centres and high-performance networks. Different organisations have varying needs. FS collaborates with multiple leading international chip manufacturers, such as Broadcom, Marvell, Intel, and Mellanox, to offer customers rigorously tested and optimised optical transceivers and diverse optical transceiver solutions to meet the requirements of different application scenarios.

 Model  Wavelength  Chip  Reach  Connector
 OSFP-SR8-800G (2xSR4) 850nm  Broadcom  50m@OM4 30m@OM3  Dual MTP/ MPO-12APC
 OSFP-DR4-400G-FL 1310nm  Broadcom  500m  MPO-12/APC
 QSFP-SR4-200G 850nm  Inphi  70m@OM3/100m@OM4  MTP/MPO-12 UPC
 QSFP28-SR4-100G 850nm  Macom  70m@OM3/100m@OM4  MTP/MPO-8 MTP/MPO-12
 QSFP-SR4-40G 850nm  Macom  150m@OM4/100m@OM3  MTP/MPO-12
 SFP28-SR-25G 850nm  Macom  100m@OM4 70m@OM3  Duplex LC

Conclusion

When selecting optical transceiver chips, it's essential to consider application scenarios, performance requirements, and cost factors. Each brand of optical transceiver chip has its technological advantages, market positioning, and application scenarios, contributing to the growth of the optical communication industry. As future network demands continue to rise, optical transceiver chip technology will face new innovations and challenges, providing robust support for global communication networks.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
431.1k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
381.5k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
370.9k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
May 30, 2024
455.7k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
329.2k