How to Build Network Infrastructure by FS Horizontal Cabling
Overview
Today's enterprise network infrastructure is evolving due to convergence, building automation, and the rise of connected devices. These changes are placing new demands on networks and staff.
FS leads the way with efficient and scalable horizontal cabling solutions designed to improve connectivity and operational efficiency. From data centers to telecom rooms and office environments, well-designed end-to-end cabling infrastructure and connectivity solutions help drive business forward.
This article focuses on how FS’s horizontal cabling solutions optimize enterprise network infrastructure and meet the changing needs of modern businesses.
What is Horizontal Cabling?
Horizontal cabling is a distinct component of a structured cabling system that connects the telecommunications room to the individual outlet or work area. It is the central cabling infrastructure responsible for data transmission on a specific floor or area within a building. Structurally, it includes the cabling components, such as copper or fiber cables, patch panels, and cross-connects, laid out horizontally, hence the name. It is of paramount importance in telecommunications systems as it facilitates the efficient transmission of data, voice, and video signals across the network.
Horizontal cabling is usually installed in a star topology (as shown in the figure). It connects the various work areas to the telecommunications room through several key components:
Cabling Media: Usually consists of twisted-pair cables, fiber optic cables, or coaxial cables, depending on the required transmission speed and distance.
Connecting Equipment: This includes patch panels, outlets, and patch cords, which help connect different devices.
Cabling Standards: The horizontal cabling system must follow certain technical standards, such as the EIA/TIA 568 standard, to ensure signal quality and compatibility.
When designing a horizontal cabling system, you need to consider the following aspects:
Cabling Path: Keep the cable length and bends to a minimum to reduce signal loss.
Environmental Factors: Avoid areas with high electromagnetic interference to ensure clear signals.
Future Expansion: Plan for future growth by leaving enough space and interfaces for additional cabling.
Key Issues in Enterprise Network Infrastructure
The network infrastructure is facing greater pressure due to the rapid evolution of network technology. The sheer number and diversity of connected devices and systems are exploding. This surge impacts not only the design and implementation of network cabling systems but also directly affects operational efficiency and competitiveness.
Rising Mobile Connectivity: As employees become more mobile, businesses need to provide comprehensive wireless coverage.
Disorganized Wiring Systems: The diverse networking and wiring methods of various low-voltage systems within buildings create confusion and increase the risk of incorrect connections.
Lack of Unified Identification: Technicians may struggle to quickly identify the correct devices or cables, leading to errors that affect network performance.
Unverified Products or Materials: Using unverified products or materials can lead to potential issues, compromising the reliability and stability of network cabling solutions.
Compliance Requirements: Businesses must ensure that the products they use meet relevant standards and regulations to comply with industry or organizational requirements.
The most critical factor for reliable enterprise networks is a high-quality cabling infrastructure, yet many companies fall short in this area.
Benefits of FS Enterprise Horizontal Cabling Solutions
High Power POE Cabling Supports Wi-Fi
To enhance the performance of enterprise network infrastructure, FS uses Cat6 cables to easily meet the power requirements of different devices. These cables not only provide efficient data transmission, but also support Power over Ethernet (PoE), including PoE+ and PoE++.
The high-power PoE++ feature supports power transmission up to 90W, making it ideal for a variety of enterprise applications such as IP phones, wireless access points, security cameras and smart devices. This feature allows devices to be powered through a single cable, eliminating the need for additional power cords, and significantly simplifies the enterprise's horizontal wiring structure while reducing costs.
High-Quality Cabling for Improved Safety
When establishing network infrastructure, a high concentration of cables can present a fire risk. To address this, FS solutions incorporate a variety of flame-resistant cables that surpass the ANSI/TIA-568.2-D6 standard, including CM, CMR, and CMP classifications. Meanwhile, the RJ45 modular plug, PVC jacket and strain relief boot provide triple protection for the copper cable, extending the service life of the cable.
Integrating these high-quality flame-resistant cables into the horizontal cabling system allows businesses to ensure continuous operations while effectively minimizing potential hazards.
Unified Color & Label Management Simplifies Operations
Enterprise network infrastructure will greatly benefit from FS's enterprise horizontal cabling solution. The solution includes color-coding for cables such as copper, fiber optics, power cords, various jack modules and ties, and cable labels. This systematic approach aims to streamline identification processes, simplify maintenance tasks, and optimize cable management within the enterprise's network infrastructure.
The clear cable color coding can reduce the risk of accidental disconnection or damage, thereby improving operational safety and minimizing potential hazards in enterprise cabling. Through color and labeling, you can quickly find specific fault areas and identify lines, effectively reducing downtime. In addition, neatly arranged and brightly colored cables not only enhance the aesthetics of the installation, but also create a pleasant and comfortable environment.
Complete Cabling Products for Seamless Connection
From the communication room to the terminal, FS offers a comprehensive structured cabling product portfolio, including cabinets, cables, and accessories to keep your users connected anytime, anywhere. For example, OM4 fiber patch cables utilize superior cable assemblies to reduce light loss and easily build a powerful fiber optic network.
FS provides fiber and copper cabling solutions for wired and wireless connectivity. This helps you simplify the process of moving, adding, changing, and upgrading your workstations. Fewer materials and labor will be needed and OpEx over the life of the installation will be reduced. The management of facility infrastructure will be improved while minimizing installation disruptions.
Stable Transmission with Professional Testing
All copper cables and fiber optic jumpers deployed in FS's enterprise horizontal cabling solutions undergo rigorous performance and connectivity testing. To ensure high performance and stable transmission, these tests use instruments from leading brands like Fluke and Dimension. As a result, enterprises can have confidence in their network infrastructure.
Local Inventory Guarantees Fast Delivery
FS has extensive Australian stock for fast shipping and deployment. Equipped with automated management systems, FS guarantees 90% of orders for same-day shipping and supports self-pickup.
Conclusion
By using FS horizontal cabling solution, enterprises can establish an efficient, flexible, and reliable network infrastructure. As technology advances, FS remains committed to providing innovative solutions, building a strong foundation for digital transformation and supporting businesses in tackling future challenges.
Ready to elevate your network experience? With cutting-edge R&D and Australia warehouses, we deliver tailored solutions. Register for more information and experience our solution design services.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
May 30, 2024