Keystone Jack
What Is Keystone Jack?
Keystone jacks are modular connectors that snap into wall plates, patch panels, or surface mount boxes to provide a termination point for Ethernet cables. Keystone jacks provide a convenient way to install and manage network connections in wall outlets and other locations.
Types of Keystone Jack
There are several types of Keystone Jacks available, each designed for different types of cables and connectors. Here are some common types:
RJ-45 Keystone Jack
This jack is used for telephone lines and is compatible with standard telephone cables. It is commonly used for voice communication applications.
RJ-11 Keystone Jack
This jack is used for telephone lines and is compatible with standard telephone cables. It is commonly used for voice communication applications.
Coaxial Keystone Jack
This type of jack is used for coaxial cables, typically used for cable television or satellite signals. It allows for the transmission of video and audio signals.
HDMI Keystone Jack
This jack is used for USB (Universal Serial Bus) cables and allows for the connection of USB devices such as printers, keyboards, and external storage devices.
USB Keystone Jack
This jack is used for USB (Universal Serial Bus) cables and allows for the connection of USB devices such as printers, keyboards, and external storage devices.
Fiber Optic Keystone Jack
This type of jack is used for fiber optic cables, enabling high-speed data transmission over long distances. It is commonly used in network infrastructure that requires high bandwidth and reliability.
These are just a few examples of Keystone Jack types. There are other specialized types available for specific applications, such as Keystone Jacks for audio, video, security, and power connections. The specific type of Keystone Jack required will depend on the intended use and the type of cable or connector being used.
How to Use a Keystone Jack?
To use a Keystone Jack, follow these general steps:
-
Step 1: Cut the cable jacket to the length needed
-
Step 2: Separate the wires
-
Step 3: Ethernet cable passes through the top case
-
Step 4: Fix the cable cores as the photo
-
Step 5: Cut off the excess part
-
Step 6: Put the cable pressing cover into module line base
-
Step 7: Use both sides of the cover to grip
-
Step 8: Push the cable tie in and lock it
-
Step 9: Complete
After completing these operations, you can insert it into the adapted connection port.
Keystone Jack Applications
Keystone jacks are used to terminate Ethernet cables at wall outlets, patch panels, or surface mount boxes, providing a modular and customizable solution for network connectivity. Here are some common applications:
Networking and Data Centers
Keystone Jacks are extensively used in networking and data center environments. They provide a modular and flexible solution for creating network connections, such as Ethernet connections, in structured cabling systems. They are commonly used in patch panels, network switches, and wall plates to create network ports.
Telecommunications
Keystone Jacks are widely used in telecommunications systems for voice and data communication. They are used to create connections for telephone lines, allowing for the installation of phone jacks or outlets in residential and commercial buildings.
Audio/Video Installations
Keystone Jacks are utilized in audio and video installations to create connections for audio and video signals. They can be used for home theater systems, conference rooms, or multimedia setups where audio and video connectivity is required.
Surveillance Systems
Keystone Jacks are employed in surveillance systems to establish connections for security cameras and other surveillance equipment. They provide a convenient and organized way to connect and manage the wiring for surveillance systems.
Their modular nature and compatibility with various cables and connectors make them versatile for different industries and installations.
You might be interested in
Email Address
![FS Same Day Shipping Ensures Your Business Success](https://media.fs.com/images/community/erp/hmSze_974px548pxAQ2rQ.webp)
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
May 30, 2024