LRDIMM
What is LRDIMM?
Load-Reduced Dual Inline Memory Modules (LRDIMMs) are a type of memory designed to minimize electrical load and enhance signal integrity, thereby boosting memory performance. These modules deliver the highest memory capacity and are ideal for high-demand computing environments.
''Also Check- DIMM Types: UDIMM vs. RDIMM vs. LRDIMM
Features of LRDIMMs
-
Advanced Buffer Technology: LRDIMMs utilize a sophisticated buffer to lower electrical load and distribute electrical signals more efficiently.
-
Maximum Memory Capacity: They offer the highest memory capacity among DIMM types, making them suitable for tasks that require substantial memory resources.
-
ECC and Non-ECC Support: LRDIMMs can be configured with both ECC (Error-Correcting Code) and non-ECC, ensuring data integrity for critical applications.
-
Reduced Power Consumption: The advanced buffering technology also helps to decrease power consumption compared to other high-capacity DIMMs.
How does LRDIMM Work?
LRDIMM is designed to improve server performance by using memory buffers. Its working principle and the improvement of server performance are mainly reflected in the following aspects:
-
Reduced electrical load: LRDIMM reduces the bus load of the system by separating the electrical load of the DRAM from the system by adding one or more buffer chips (iMB isolated memory buffer chips) to each memory module. This design allows LRDIMMs to support higher operating frequencies and greater memory capacity without adding additional power consumption.
-
Improved signal integrity: Because LRDIMMs buffer all signals, including address, command and control signals, and data signals, this helps improve signal integrity and stability, which improves the speed and reliability of memory operations.
-
Increase memory capacity: LRDIMMs significantly increase the memory capacity of a server. For example, DDR3 LRDIMM technology can triple the memory capacity of a server and increase bandwidth by 57 percent. This high-capacity feature is especially suitable for applications that require large amounts of memory, such as high-performance computing clusters and database servers.
-
Compatibility: LRDIMMs are fully compatible with existing JEDEC standard DDR3 DIMM sockets, which means they can be seamlessly upgraded to LRDIMMs on top of existing hardware without the need to replace motherboards or other hardware components.
-
System abstraction: LRDIMMs use the internal buffering mechanism to make each quad-rank DRAM module appear as a dual-rank DIMM module in the system. This abstraction not only simplifies the management of the system but also improves the speed of memory operations.
Comparing LRDIMM and RDIMM
RDIMM called Registered DIMM, is a registered dual inline memory module. It attaches a register between the CPU and the DRAM chip for data transmission, which reduces the distance of parallel transmission and improves transmission efficiency. It is the largest capacity for server memory performance, widely used in the server memory market. RDIMM or LRDIMM can be a consideration when choosing the right memory module for a high-performance server. Both have their own characteristics in terms of performance and application scenarios.
Aspect
|
RDIMM (Registered DIMM)
|
LRDIMM (Load-Reduced DIMM)
|
Working Mechanism
|
Uses sophisticated registers to enhance signal and
drive memory particles, improving performance.
|
Reduces load and power consumption of the memory bus
through distributed buffering technology.
|
Transmission Efficiency
|
Improves transmission efficiency by reducing the
distance of parallel transmission.
|
Provides higher memory capacity support with reduced
power consumption.
|
Maximum Frequency
|
3200 MT/s
|
3200 MT/s
|
Memory Bandwidth Efficiency
|
N/A
|
Maintains high memory bandwidth efficiency at a high
capacity and high speed.
|
Power Consumption
|
Higher power consumption compared to LRDIMM.
|
Dual-Rank memory power consumption is only 50% of
RDIMM's, improving energy efficiency.
|
Applications
|
Commonly used in general server and workstation
applications with lower memory capacity and
performance needs.
|
Mainly used in enterprise-level servers requiring high
memory capacity and low power consumption.
|
-
In principle, LRDIMMs do not use complex registers but reduce the power load on the underlying motherboard through simple buffering. This design enables LRDIMMs to reduce the load and power consumption of the memory bus while providing higher memory capacity support. In contrast, RDIMMs use sophisticated registers to enhance the signal and drive memory particles, thereby improving memory performance.
-
In terms of performance, although the maximum frequency of both LRDIMMs and RDIMMs is 3200 MT/s, LRDIMMs can maintain high memory bandwidth efficiency at high capacity and high speed through its distributed buffering technology. In addition, LRDIMM's Dual-Rank memory power consumption is only 50% of RDIMM's, which further improves its energy efficiency ratio.
-
In the application scenario, LRDIMMs are mainly used in enterprise-level servers that require high memory capacity and low power consumption. Because of its optimized design, LRDIMMs can play an important role in large-scale server deployments, especially in enterprise environments that require large amounts of memory and high performance. Rdimms are more commonly used in general server and workstation applications, where memory capacity and performance requirements are relatively low.
LRDIMM memory changes the register chip of the RDIMM to an isolation memory Buffer (iMB) chip. The immediate benefits are reduced server memory bus load and further increased server RAM support capacity with little impact on memory performance. Lrdimms have relatively low power consumption and are also popular in the network server space.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
May 30, 2024