Global Optical Transceiver Market: Striding to High-Speed 400G Transceivers
The demand for higher Ethernet speed, coupled with the prevalence of Cloud computing, the Internet of Things, and virtual data centers, has driven the global optical transceiver market to evolve dramatically to catch leading edge broadband network capacity. The past decades have witnessed massive adoption of 1G, 10/25G to 40/100G optical transceivers, while higher-speed 200G and 400G transceivers are just on the horizon. The sales of high-speed optical components grow steadily and are expected to continue in the years to come.
10G, 25G, 40G and 100G: Seeing Broad Adoption in Data Center
As the network gets faster and virtualization gradually becomes the norm, data centers are undergoing a significant transformation. The trend emerging in the industry signifies a migration toward higher-speed transceivers and better service. With the widespread use of 10/25 Gbps, 40 Gbps, and 100 Gbps, high-bandwidth transceivers such as 200G and 400G transceivers are also gaining growing popularity.
10G Transceiver: Moving to the Edge
Initially offered in the early 2000s, 10G optics has matured now to become commonplace in data centers. Basically the 10G Ethernet is stacked to move to 40G and 100G at the access layer, following the upgrade path of 10G-40G-100G, which, however, will quadruple the cabling complexity, power consumption and overall cost. And this will be exacerbated when aggregating into 100G (10×10G) interface.
25G Transceiver: Pave the Road for 100G
So there comes the game changer: 25GbE for better economics and efficiency. SFP28 optical transceiver compatible with SFP+ is designed for 25G Ethernet, delivering 2.5 times higher speed per lane at lower power. As 25GbE makes the road to 100G smoother with reduced cost, lower power consumption and less cabling complexity, some users even plan to skip 10G and directly deploy 25G Ethernet for better scaling to 50G and 100G.
Figure 1: 10G, 25G, 40G and 100G
40G Transceiver: Affordable for Mass Deployment
Obviously, 10GbE is no longer fast enough for data centers handling large-scale applications, so 40G is designed to alleviate bottlenecks in the access layer. The cost of 40G is extremely high at first, making the implementation of 40G technology difficult. Luckily, we’ve seen significant cost reduction of 40G transceivers in the past several years, which accelerates their adoption in aggregation links, or in access links to connect servers.
100G Transceiver: Ramping up in Data Center
Currently 100G are the fastest Ethernet connections in broad adoption, which is growing sustainably. And the optical transceiver market indicates that 100G QSFP28 module price will continue to drop, making the cost difference between 40G and 100G even smaller. Moreover, 25G server and 100G switch became commonplace in most hyperscale data centers that replaced previous 10G servers and 40G switches. Vendors of 100G QSFP28 transceiver will continue to grow the product and push the limits of its versatility.
200G and 400G Transceivers - New Connection Speed Hits Data Center
Another foreseeable trend in the interconnect market is the phase-out of low-speed transceivers in the core of networks and in data centers. So here comes the major shift from 10G/25G/40/100G to 200G and 400G transceivers: next-generation 200G and data center 400GbE deploy started in 2018, and has gradually been mainstream by now. On the whole, the optical transceiver market is evolving to higher speed, more reduced power consumption, and smaller form factor. Let’s take a look at these future-proofing 200G and 400G optical transceivers.
-
200G SFP-DD transceivers: Short for Small From-factor Pluggable Double Density, which doubles the SFP bandwidth and supports fast line rates while maintaining SFP backward compatibility.
-
400G QSFP-DD/OSFP/QSFP112 transceivers: QSFP56, QSFP-DD, and OSFP are advanced optical transceiver form factors designed for high-speed data communication.
-
1. QSFP56: Features a compact design with four channels, each supporting 50Gbps, totaling 200Gbps.
-
2. QSFP-DD (Quad Small Form-factor Pluggable Double Density): Doubles the density with eight channels, supporting up to 400Gbps, ideal for dense data center environments.
-
3. OSFP (Octal Small Form-factor Pluggable): Provides eight channels, each up to 100Gbps, for a total of 800Gbps, offering high performance and scalability for next-gen networks.
These modules support diverse network applications and ensure efficient data transmission.
Figure 2: 200G and 400G
DAC and AOC: Lower Cost Stimulate Popularity
DACs (direct attach copper cables) and AOCs (active optical cables), with their inherent advantage of enhanced signal integrity and superior flexibility, have become the preferred, cost-effective interconnect for high-speed links at 10G, 25G, 40G and 100G for about all applications in hyperscale and enterprises, and is likely to be used for 200G and 400G as well. 400G DAC and 400G AOC are witnessing tremendous growth in the data interconnect market, and there is no doubt that sales will keep surging in the years to come.
Conclusion
According to a recent study, the global 400G optical transceiver market is expected to continue to increase in popularity and sales in the coming years, eventually reaching $22.6 billion by 2023. Global internet adoption, online commerce, streaming video, social networking, cloud services and software as a service (SaaS) all play into this business networking trend, as does the availability and cost-effectiveness of 400G transceivers. So just stay tuned and embrace the significant opportunities that lie ahead for the optical transceiver market.
Related Article:
400G Ethernet Wiki, 400G Transceiver, and 400G Transceiver Market
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
May 30, 2024