Tight-buffered
What Is the Tight-buffered?
Tight-buffered refers to a type of fiber optic cable construction where each individual fiber is directly coated with a protective buffer layer. In tight-buffered cables, the fiber is enclosed in a primary coating, commonly made of acrylate or similar materials, which tightly adheres to the fiber's surface.
Tight-buffered construction uses 900μm buffered fibers. The core is protected by a two-layer coating. The first is plastic and the second is waterproof acrylate. The core of the cable is never at risk of exposure, unlike the loose-buffered cable which can escape its confines. Fibers are surrounded by dielectric strength members (FRP) are protected by a rugged polyurethane outer jacket and provide superior environmental and mechanical protection. The fiber count for tight-buffered fiber cable varies from 1 to 144 fibers, but generally cables with 2, 6, 12, and 24 fibers are the most commonly used. Larger fiber counts such as 48 fibers, 96 fibers, and 144 fibers are also available for specific applications.
What Are the Different Types of Tight-buffered Fiber?
Tight-buffered cables can be further categorized as unitized or non-unitized based on their construction. Here's an explanation of each type:
-
1. Unitized Tight-Buffered Cable: Unitized tight-buffered cable, also known as multifiber tight-buffered cable, consists of multiple tight-buffered fibers grouped together within a single overall jacket. In this construction, the individual fibers are color-coded or numbered for easy identification. Unitized cables are typically used in applications where multiple fibers need to be terminated and managed as a single entity. They are commonly used in patch panels, fiber distribution hubs, and backbone installations.
-
2. Non-Unitized Tight-Buffered Cable: Non-unitized tight-buffered cable, also referred to as single-fiber tight-buffered cable consists of individual tight-buffered fibers, each with its own jacket. In this construction, each fiber is independent, and they are often bundled together within an outer protective jacket. Non-unitized cables are used in applications where individual fibers need to be accessed or terminated separately. They are commonly used in patch cords, pigtails, and short-distance connections.
Both unitized and non-unitized tight-buffered cables have their advantages and are suited for different applications. Unitized cables simplify the installation and management of multiple fibers, as they can be treated as a single entity, reducing bulk and improving organization. Non-unitized cables provide flexibility and ease of termination for individual fibers, allowing for more specific and customized connections.
What Are the Advantages of Tight-buffered Fiber?
Tight-buffered fiber optic cables offer several advantages over other types of fiber optic cable constructions. Here are some key advantages of tight-buffered fiber:
-
1. Enhanced Protection: Tight-buffered fiber cables provide a high level of protection to the optical fibers. Each fiber is individually coated with a tight buffer layer that acts as a primary layer of protection. This buffer layer shields the fiber from external factors such as moisture, chemicals, temperature variations, and physical stresses. It helps ensure the long-term reliability and performance of the fibers.
-
2. Easy Termination and Connectorization: The tight buffer layer on each fiber provides a convenient surface for termination and connectorization. It simplifies the process of stripping the cable and preparing the fiber for termination, making it easier and faster compared to other cable designs. This advantage is particularly useful in field installations or situations that require frequent moves, adds, or changes.
-
3. Compact and Lightweight: Tight-buffered fiber cables have a compact and lightweight design. The tight buffer layer directly surrounds the fiber, resulting in a smaller overall cable diameter and reduced weight. This makes tight-buffered cables easier to handle, install, and route in tight spaces or congested cable trays.
-
4. High Fiber Density: Tight-buffered cables can accommodate a high fiber density within a single cable. The individual fibers are grouped closely together, and the tight buffer layer minimizes the space between them. This allows for a greater number of fibers within a given cable diameter, making tight-buffered cables suitable for applications that require high fiber count in a limited space.
-
5. Resistance to Mechanical Stress: The tight buffer layer provides excellent resistance to mechanical stresses, such as bending, pulling, or twisting. It helps absorb and distribute these stresses along the length of the fiber, minimizing the risk of fiber breakage or signal loss. This advantage makes tight-buffered cables suitable for applications that involve frequent handling or movement.
-
6. Direct Connectorization: Tight-buffered fibers can be directly terminated with connectors without the need for additional buffer tubes or fan-out kits. This simplifies the termination process and reduces the overall size and complexity of the cable assembly. It also allows for easier connectivity in tight spaces or when a high fiber density is required.
What Are the Applications of Tight-buffered Fiber?
In fact, properly designed and manufactured tight-buffered cable has been sufficiently proven to be suitable for both indoor and outdoor applications in the past two decades. Tight-buffered fiber optic cables offer the flexibility, direct connectivity, and design versatility necessary to satisfy the diverse requirements existing in high-performance fiber optic applications. Such applications include medium-distance transmission for telco local loops, LANs, SANs, WANs, and point-to-point links in cities, buildings, factories, office parks, and campuses.
Tight-buffered cable has many advantages over traditional outdoor cable spliced to indoor cable. The first advantage is an improvement in reliability. Link reliability will be reduced anytime there is a splice transition. Tight-buffered indoor/outdoor cable comes into the building directly as far as needed for final termination. Thus connectors are assembled onto the fiber cable at the final patching center, not at an inappropriate, hard-to-reach transition zone. The second advantage is that tight-buffered indoor/outdoor cable is generally easier to terminate than traditional outdoor-rated cables. There is no injected gel to clear off prior to the termination process. Overall, we can say tight-buffered cables provide fast, easy, economical termination with no chemical cleaning required.