Voice VLAN
What Is Voice VLAN?
A voice VLAN( virtual local area network) is a dedicated virtual local area network specifically assigned for voice data streams. It enhances the quality of voice traffic by prioritizing its transmission over other types of traffic. This means that when voice traffic is sent alongside other services such as data and video, the voice service will be given higher forwarding priority, ensuring better transmission quality.
How Does Voice VLAN Work?
To prioritize voice data streams, they must first be identified. Voice VLAN can recognize voice data streams in two ways: one is by identifying the source MAC addresses of the received packets (MAC address-based mode), and the other is by identifying VLAN tags of the received packets (VLAN-based mode).
In the MAC address-based mode, a network switch can determine whether a data stream is a voice data stream based on the source MAC address field in a data packet that enters its interface. As illustrated in the picture below, after receiving packets from the PC and the IP phone, the switch processes them as follows: If the source MAC address matches the OUI (Organizationally Unique Identifier) configured on the switch, the voice VLAN tag is added to the packet, and its priority is increased. If the source MAC address does not match the OUI, the VLAN tag of the PVID is added to the packet, and it is not prioritized for transmission.
In VLAN-based mode, a network switch identifies whether a data packet is a voice packet by examining the VLAN ID of the incoming packet. As illustrated in the picture below, the IP phone initially sends packets to the network switch. The switch receives these packets and returns them after embedding the voice VLAN information into the appropriate fields. Once the IP phone receives packets with the voice VLAN information, it sends the tagged voice packets again. If the tag matches the voice VLAN configured on the switch, the switch prioritizes the forwarding of the packet. This mechanism ensures that voice packets are given transmission priority during periods of network congestion.
What Can We Benefit From Voice VLAN?
Security Benefits
Voice VLANs offer enhanced security measures for voice communications. By segregating voice traffic from data traffic, a voice VLAN minimizes the risk of eavesdropping and unauthorized access. This separation ensures that sensitive voice data is isolated from the general network traffic, making it harder for potential attackers to intercept or tamper with voice communications. Additionally, using a dedicated VLAN for voice traffic allows for a more straightforward application of security policies and access controls, further protecting the integrity and confidentiality of voice communications.
Performance Optimization
Implementing a voice VLAN significantly optimizes network performance. By isolating voice traffic from other types of network traffic, it reduces congestion and potential collisions. This dedicated bandwidth allocation ensures that voice packets are transmitted with minimal delay and jitter, leading to clearer and more reliable voice communications. Furthermore, the prioritization mechanisms inherent in voice VLANs, such as 802.1p CoS or DSCP, guarantee that voice traffic is always given the necessary priority over other less time-sensitive data, thereby maintaining high-quality voice service even under heavy network load.
Scalability and Ease of Management
Voice VLANs simplify network scalability and management. As businesses grow and add more VoIP devices, a voice VLAN provides a straightforward way to integrate new devices without disrupting existing network configurations. The segregation of voice traffic simplifies troubleshooting and monitoring, allowing network administrators to quickly identify and resolve issues specific to voice communications. Additionally, voice VLANs enable more efficient use of network resources by clearly defining traffic types, which helps in better capacity planning and management. This structured approach facilitates smoother network expansion and ensures consistent performance across all connected VoIP devices.
Voice VLAN Configuration and Use
Configuring
There are two methods to configure a voice VLAN, based on different principles.
MAC Address-Based Mode:
-
Create a VLAN on the switch and add interfaces to it to enable Layer 2 interworking.
-
Configure the OUI to match the source MAC address of the incoming packets.
-
Enable the voice VLAN function on the designated interface.
MAC Address-Based Mode:
-
Create a VLAN on the switch and add interfaces to it for Layer 2 interworking.
-
Designate a specific VLAN as the voice VLAN and configure it accordingly.
Applicable Scenarios
Voice VLAN is particularly useful in environments with numerous IP phones, such as large enterprises and the financial sector. IP phones are essential for frequent multi-party communications in these settings, where offices are spread out and staff are dispersed. Conference rooms often use voice VLANs when there's no need to connect PCs for data services.
Network Switches Supporting
Not all network switches support voice VLAN technology. PoE switches that provide power for IP phones, like the FS S3410-24TS-P, S3260-8T2FP, and S5860-24XB-U, support voice VLAN. Some other switches, such as the FS S3900, S5800, and S5850 series, may support voice VLAN but do not provide power to connected IP phones.
Note: The S3410-24TS-P model now supports both AC and DC power supplies.