OCSP
What is OCSP?
The Online Certificate Status Protocol (OCSP) is an Internet Protocol (IP) used to verify the validity of digital certificates and determine if they have been revoked. It serves as an alternative to the Certificate Revocation List (CRL), addressing the issue of frequent updates that must be downloaded to keep the list current.
When a user attempts to access a server, OCSP sends a request for the certificate status. The server responds with a status indicating whether the certificate is "current," "expired," or "unknown." This protocol defines the communication between the server, which holds the certificate status, and the client application.
OCSP enables real-time status checks on security certificates and is essential for the extended validation of Secure Socket Layer (SSL) and Transport Layer Security (TLS) certificates. For instance, when establishing an HTTPS connection, the browser typically performs an OCSP check with the Certificate Authority (CA) that issued the certificate. This ensures the certificate is valid and has not been revoked, though it may occasionally cause short delays in the SSL handshake. Additionally, OCSP allows users with expired certificates limited access to servers before renewal.
How Does OCSP Work?
When a request is made to check a certificate's validity, an OCSP request is sent to an OCSP responder—a server managed by the issuing CA. This responder verifies the request with a trusted CA and provides a response indicating whether the certificate is valid, revoked, or unknown. Major web browsers, including Apple Safari, Internet Explorer, Microsoft Edge, and Mozilla Firefox, support OCSP.
OCSP and CRL
Web browsers employ various methods to determine if a site’s certificate has been revoked, with OCSP and CRLs being the most common. A CRL (Certificate Revocation List) is a list of serial numbers for certificates that have been revoked by a CA; however, it can become outdated and requires periodic downloads to remain current.
OCSP enhances security by allowing for real-time checks of a certificate's revocation status, incorporating signatures that confirm the certificate's validity. This process is more efficient than downloading a list, as it provides immediate status updates.
OCSP Stapling
While OCSP is effective, it can introduce challenges, such as increased costs for CAs and privacy concerns. Live OCSP checks can expose private browsing data since requests are sent via unencrypted HTTP and are linked to specific certificates. Consequently, this can reveal a user's visited websites to anyone monitoring the network traffic between the browser and the OCSP responder, potentially leading to slower browsing experiences due to reliance on third-party validation.
To mitigate these issues, OCSP stapling was developed. This technique involves embedding a current OCSP response within the HTTPS connection, reducing the need for browsers to send individual requests. By doing so, it minimizes traffic between the server and the browser, enhancing privacy and performance.
Advantages of OCSP over CRL
OCSP offers several key advantages over CRL in certificate validation processes:
-
1. Real-Time Validity Checking: OCSP provides immediate verification of certificate status, allowing for the instant blocking of revoked certificates. In contrast, CRLs are updated periodically, which can lead to delays in revocation propagation.
-
2. Flexible Architecture: OCSP can be scaled independently to manage high traffic loads, and Certificate Authorities (CAs) can delegate the handling of OCSP requests to third-party responders, enhancing efficiency.
-
3. Lightweight Operation: OCSP requests are minimal in size, requiring less bandwidth compared to CRLs, which may involve downloading large lists of revoked certificates. This results in lower network overhead.
-
4. Useful Diagnostics: The OCSP responder can provide detailed information about the certificate status and reasons for revocation, going beyond a simple "good" or "revoked" response.
-
5. No Fixed Update Periods: OCSP allows for continuous requests without waiting for scheduled updates, making it more responsive to changes in certificate status.
These advantages make OCSP a preferred choice for environments requiring up-to-date and efficient certificate validation.
-
CDN Solutions for OTT & IPTV
By building a distributed CDN solution with PicOS®Data Center Switches and AmpCon™ Management Platform, we can optimize user experience while relieving access pressure on core data centers, reduce user bounce rate in a low-cost and highly available way, a
-
Two-tier Network Architecture Solution for Data Center Fabric Network
Currently, the industry is driving the evolution of data center networks towards full Ethernet, and it is gradually becoming a fact standard in data center networks scenarios.
-
CDN Data Center Network Solution
Constantly optimized user experience is the core competitiveness of Internet vendors, but due to the bandwidth pressure of core data centers and transmission distance between visitors, it is difficult for networks to respond to user requests quickly.