PSTN
What is PSTN?
PSTN (Public Switched Telephone Network) refers to the traditional circuit-switched telephone network, primarily used for voice communication. It is also known as Plain Old Telephone Service (POTS). PSTN provides the infrastructure and services for wired telephone systems, enabling voice calls through the establishment of a dedicated point-to-point connection. The PSTN network is composed of terminal equipment (such as landline phones), local and long-distance switching offices, and various signaling systems, which allow voice and other forms of communication to be transmitted via twisted copper wires, fiber optic cables, and other media, with a wide range of applicability.
In addition, the PSTN has high reliability and stability, and was once the primary choice for home and business communications. However, with the development of the Internet and digital technologies, the PSTN faces growing challenges, especially in terms of bandwidth, functionality and cost-effectiveness. Nevertheless, the historical significance and technical underpinning of the PSTN have provided a solid foundation for the evolution of modern communications.
How PSTN Works?
PSTN (Public Switched Telephone Network) primarily operates based on circuit-switched technology, delivering voice communication services through a series of complex hardware and software components. These components include user terminal devices, switching centers, transmission media, and transport networks.
In simple terms, at the user device end, PSTN converts your voice into electrical signals, which are transmitted to a switching center. The switching center then directs the user's call signal to the target terminal, and the destination terminal translates the signal back into sound, allowing the call to reach the corresponding phone number. During this process, signals are transmitted via copper wires, fiber optics, and satellite networks. Once the call is answered, the digital signals are converted back into voice, enabling real-time communication.
The working process of PSTN involves several components and steps, from user dialing, signaling processing, switching and routing, to establishing and ending the communication. The entire process relies on circuit-switched technology, ensuring a stable and high-quality voice connection during the call.
PSTN vs VoIP
While PSTN has been the dominant technology for voice communication for a long time, IP-based network communication is gradually replacing PSTN as digital information technologies evolve. PSTN is scheduled for a phased retirement by 2030 in most countries, meaning that traditional landlines will no longer be in use. Thus, the transition from PSTN to VoIP has become an inevitable choice for businesses.
PSTN (Public Switched Telephone Network) and VoIP (Voice over Internet Protocol) are two distinct telecommunication methods, and they differ significantly in terms of working principles, transmission methods, costs, and functionality. Below is a key comparison between the two:
Feature | VoIP | PSTN |
---|---|---|
Working Principle | Based on packet-switched technology, transmits voice over the internet. | Based on circuit-switched technology, a dedicated physical line is established during the call. |
Call Costs | Lower costs since voice is transmitted over the internet. | Higher call costs. Calls are usually charged per minute based on distance and duration. |
Stability | Relies on internet and power supply. If the network or power is down, VoIP calls will be unavailable. | Highly reliable, especially in emergencies, since it does not depend on the internet or power supply. |
Security | Depends on your network security; relatively more vulnerable. | Highly secure due to the use of dedicated lines. |
Features | Rich in features, including easy setup for conference calls, video calls, voicemail, and seamless integration with modern business systems (like CRM). | Limited functionality, mainly offering basic voice calling features. |
Scalability | Highly scalable, allowing more users by increasing bandwidth or equipment, suitable for business expansion. | Adding phone lines requires limited scalability and physical infrastructure expansion (such as new wiring or switches). |
Conclusion
PSTN, as a fundamental communication technology, has undergone a long journey from its inception in the late 19th century to becoming the backbone of global voice communication in the 20th century. Its development has marked significant milestones, from the invention of the automatic switch to the introduction of digital switching and fiber optic technology. However, with the emergence of IP-based technologies and the increasing dominance of VoIP, the traditional circuit-switched model is gradually being phased out.
The historical contributions of PSTN cannot be overlooked, but the advantages of VoIP will lead communication into a new digital era. The growing demand for flexible, cost-effective, and scalable communication solutions has driven the gradual integration of PSTN with the internet and IP (Internet Protocol) technologies, enabling interoperability between traditional telephone services and IP telephony (VoIP). Many businesses are opting for hybrid communication systems, and this incremental migration strategy avoids large-scale investments and technical risks all at once, allowing companies to gradually transition from PSTN to VoIP and upgrade their communication infrastructure according to their needs and budgets.
-
Smart Hotel Video Surveillance Solution
Nowadays, many hotels are facing various problems, such as large guest mobility, complex identity of personnel entering and exiting, opening of the overall hotel environment, safety of guests' belongings, the unified management of parking lot vehicles and
-
VoIP Solution for Governments
Governments are developing toward the integration of IP voice and data to achieve information and intelligence at government offices. Featuring multi-lingual and multi-level IVR services, the governments' service hotlines allow citizens (callers) to solve
-
VoIP Solution for Schools and Universities
A growing number of colleges and universities are gravitating to VoIP to reduce infrastructure and maintenance costs for communications services. Through FS VoIP solutions, administrators can provide students and teachers with the best communication tools