PVC
What is PVC (Polyvinyl Chloride)?
Polyvinyl Chloride (PVC or Vinyl) is an economical and versatile thermoplastic polymer. It is widely used in the building and construction industry to produce door and window profiles. It also finds use in drinking and wastewater pipes, wire and cable insulation, medical devices, etc. It is the world’s third-largest thermoplastic by volume after polyethylene and polypropylene.
It is a white, brittle solid material available in powder form or granules. PVC is now replacing traditional building materials in several applications. These materials include wood, metal, concrete, rubber, ceramics, etc. in several applications. This is due to its versatile properties such as being lightweight, durable, low cost, and easy processability.
What are the Key Properties of PVC?
PVC is a very versatile and cost-effective material. Its main properties and benefits include:
-
1. Electrical Properties: PVC is a good insulation material. Thanks to its good dielectric strength.
-
2. Durability: PVC is resistant to weathering, chemical rotting, corrosion, shock, and abrasion. It is the preferred choice for many long-life and outdoor products.
-
3. Flame Retardancy: Because of its high chlorine content, PVC products are self-extinguishing. Its oxidation index is ≥45. Antimony trioxide has been extensively used in combination with phosphate ester plasticizers. This gives excellent fire performance and mechanical properties.
-
4. Cost/Performance Ratio: PVC has good physical as well as mechanical properties. It also provides excellent cost-performance advantages. It has a long life span and needs low maintenance.
-
5. Mechanical Properties: PVC is abrasion-resistant, lightweight, and tough.
-
6. Chemical Resistance: PVC is resistant to all inorganic chemicals. It has very good resistance against diluted acids, diluted alkalis, and aliphatic hydrocarbons. Some grades are attacked by ketones and esters, chlorinated and aromatic hydrocarbons, aromatic ethers and amines, and nitro-compounds.
Applications of PVC
-
1. Pipes and Fittings: PVC is a commonly used material for manufacturing various pipes and fittings, widely used in water, drainage, and gas delivery systems.
-
2. Cables and Wires: PVC is extensively used as an insulation layer and sheathing material for electrical wires and cables.
-
3. Plastic Products: PVC can be made into a variety of plastic products, such as floor tiles, window frames, awnings, automotive interiors, etc.
-
4. Medical Devices: PVC can be used to manufacture medical devices, such as intravenous bags, catheters, gloves, etc.
-
5. Packaging Materials: PVC is widely used to make packaging containers for food, pharmaceuticals, and other products.
-
6. Toys and Sporting Goods: PVC can be used to manufacture various toys and sporting goods, such as dolls, footballs, etc.
-
7. Building Materials: PVC can be used to make building materials, such as window and door frames, piping, etc.
-
8. Agricultural Applications: PVC can be used to manufacture agricultural greenhouses and other facilities.
![FS Same Day Shipping Ensures Your Business Success](https://media.fs.com/images/community/erp/hmSze_974px548pxAQ2rQ.webp)
-
25G/100G Data Center Network Solution
With the evolution of data center virtualization technology and the popularization of distributed computing, the internal traffic of the data center has increased exponentially. The 25G/100G data center network adopts the large two-layer structure of IP C
-
Migration to High Density 400G Data Center
The storage and computing requirements supported by data centers present new challenges to connectivity within the data center, in terms of bandwidth, transmission distance, power consumption and cost. High-density 400G Data Center Solution provide key be
-
Data Center Structured Cabling Solution
Nowadays, the surge of Internet data traffic has promoted the rapid growth of data processing demand and storage demand. Higher speeds and more bandwidth requirements are driving equipment and architecture choices in data center. FS's high-density data c