English

EIGRP vs OSPF: What's the Difference?

Updated on Dec 15, 2021 by
98.5k

EIGRP vs OSPF mainly lies in algorithm, routing metrics, convergence time, etc.

EIGRP (Enhanced Interior Gateway Routing Protocol) and OSPF (Open Shortest Path First) are two common Interior Gateway Protocols (IGP) specifying how routers or data switches communicate with each other. They are often applied in different situations for varied performance on speed, delay, etc. What are their differences on earth? Get all you want to know through the detailed description of EIGRP vs OSPF comparison below.

EIGRP vs OSPF: What Is EIGRP Protocol in Networking?

EIGRP is an advanced Cisco-based distance vector routing protocol that works on the principles of Interior Gateway Protocol. It uses incremental and triggered updates that improve the operational ability and fast converging rate. It can determine the shortest path distance vector and uses metrics like bandwidth, load, and delays to calculate the shortest optimal network route. EIGRP is a complex protocol but can be configured and runs easily in small and large networks.

EIGRP protocol is used for passing the information from one to neighboring routers in the same area.

EIGRP vs OSPF: What Is OSPF Protocol in Networking?

OSPF, a link-state routing protocol, collects link state information from routers in the network and determines the routing table information to forward packets. This occurs by creating a topology map for the network. OSPF only exchanges routing information when there’s a change in network topology. OSPF protocol best fits for complex networks that comprise multiple subnets working to ease network administration and optimize traffic. It effectively calculates the shortest path with minimum network traffic when the change occurs.

OSPF protocol is used for passing the information from one adjacent area to another one.

EIGRP vs OSPF: What's the Difference?

One of the FAQs on EIGRP vs OSPF is “which protocol is better, EIGRP or OSPF?”. To answer this question, you’d better get to know the difference between EIGRP and OSPF and have a thorough understanding of their pros and cons.

Features EIGRP Protocol OSPF Protocol
Routing Protocol Type Hybrid (it merges the features of distance vector routing and link-state routing protocol) Link State Routing Protocol (analyzes different sources like the speed, cost, and path congestion while identifying the shortest path)
Standards-based on Cisco Proprietary IETF Open Standard
Administrative Distance 90 (Internal) 170 (External) 110
Algorithm Used DUAL distance vector Dijkstra link state
Routing Metrics Combination of bandwidth, reliability, load, and delay Interface bandwidth
Updates Updates and queries as needed to a multicast address Flooding as needed and periodically to a multicast address
CPU Requirements Lower CPU and memory needs Require high CPU and memory
Ease of Implementation Easy but no provision of auto-summary Complicated
Hierarchical Design No Yes
Convergence Time Fast Slow
Unequal Path Load Balancing Yes No
Network Application Small and large networks Large networks

Table: Key Differences Between EIGRP and OSPF

Explanations to Some Key Differences

EIGRP vs OSPF: Algorithm.EIGRP is based on DUAL (Diffusing Update Algorithm) while OSPF uses Dijkstra's Shortest Path Algorithm with the major difference in how they calculate the shortest routing path. Shortest Path only depends on bandwidth for metric calculation of the cost of a particular link, while DUAL uses bandwidth and delay to calculate the composite metric with a complex formula.

EIGRP vs OSPF: CPU Usage.OSPF maintains the complete information about the routers in its area. Each time there is a change within the area, all routers need to re-sync their database, which makes it more CPU intensive. EIGRP, on the other hand, has triggered and incremental updates and will not send all the information about the network rather just the information that has changed will be shared.

EIGRP vs OSPF: Convergence Time. EIGRP’s DUAL algorithm maintains a loop-free alternative path. When a network becomes unreachable from the best path, EIGRP can fall directly to the alternate best path. OSPF, however, involves a small time to install a new route and re-route traffic once a failure occurs. So EIGRP can provide a shorter convergence time with minimal network traffic.

EIGRP vs OSPF: Service Provider and Data Center Support.OSPF is a better choice when your network is hosted in a data center or cloud-based solution. As OSFP is widely running in most data center networks, it could do some fine-tuning in the network infrastructure underlying and exchange routing information with the firewall.

EIGRP vs OSPF: Scalability. The scalability of the OSPF is higher than EIGRP because EIGRP is complicated and vendor-specific and incapable of migrating from one vendor to the other. Conversely, OSPF is an open standard and simple protocol through which the network can be scaled easily.

EIGRP vs OSPF: Unequal Path Load Balancing. EIGRP is the only protocol supporting unequal path load balancing which helps routers route traffic across links of different bandwidth, while OSPF does not have this feature.

EIGRP vs OSPF: Which One to Choose?

Given all the comparisons on EIGRP vs OSPF, you may have a clear understanding of the two routing protocols. Both of them could be widely deployed in Internet Protocol (IP) networks for data communication. EIGRP is a popular choice for routing within small and big campus networks. While OSPF is the best choice when your network hardware devices come from various vendors. In addition, If you are using MPLS as the WAN technology, OSPF is also a better option as it has MPLS traffic engineering support with CSPF (Constrained Shortest Path First). If you are looking for enterprise campus network switches supporting OSPF for small/medium-sized & large-scale campus network aggregations, FS S5860 and S3910 series are the favorite choices of many customers for their high reliability, strong multi-service support capability, and easy network maintenance.

Also look for the wiki for RIP vs OSPF vs EIGRP vs BGP? Here are some related articles:

RIP vs OSPF: What Is the Difference?

OSPF vs BGP: Which Routing Protocol to Use?

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k