English

Webcam Selection: How to Choose the Best Webcam for My Laptop or PC

Updated on Sep 1, 2021 by
14.3k

Overview

Webcams may seem like some simple tools to use, although they require your close attention before you can choose any of them for your laptop or PC. Built-in and standalone webcams with different features are designed for various business needs. If you want to have more functions or better experiences, an external webcam may be a good fit for you. The factors discussed in this article are what you should consider before choosing your best webcams.

Basic Parameters to Consider When Choosing a Webcam

Resolution

High-Def vs. Ultra HD

The quality of the image mainly depends on the resolution of the device. Many webcams today capture high-definition videos. If you want to accomplish more professional work, such as uploading videos to YouTube, acquire a full HD 1080p camera.

NOTE: "P" is a short form of "progressive scanning."

However, if you need the absolute best quality, look for webcams, which record resolutions above 1080p up to 4K Ultra HD. 4K refers to one of two high-definition resolutions, namely, 3840 x 2160 pixels or 4096 x 2160 pixels. 4K is four times the pixel resolution of 1080p (1920 x 1080 pixels). Normally, users with monitors that support the High-Def and Ultra HD resolutions gain enhanced picture clarity.

Frame Rate

A frame rate, also termed the refresh rate, is essential for selecting the ideal webcam for your business. A frame rate is measured in units called frames per second. A decent webcam will possess a frame rate of at least 30 frames per second (fps). Anything lower than this is out of date, and images appear to shake and vibrate.

Lens

A high-end webcam for pc possesses a glass lens, whereas a moderately priced model has a plastic lens. Several plastic lenses are ideal for Skype video calls plus other video chat software. To produce professional videos, acquire a glass lens.

Wide Angle

For video conferencing, always choose a web camera with a wide-angle lens ranging from 90° and above to cover all the participants in your business meetings. Besides, the size of the room should also be taken into consideration.

Automatic Light Correction

If your room lighting isn't enough, your video image may get cast in shadows or look washed out. Auto light correction promptly detects and rectifies poor lighting as you conduct your video calls or meetings. A good webcam has a low-light correction, a color boost, and can adjust exposure, making you look your finest amidst harsh and dim lighting.

Webcam Automatic Light Correction Function

Audio Performance

Most webcams have built-in microphones with sound-enhancing qualities. A premium webcam microphone will include noise-reduction technology. High-end webcams come with dual microphones to give you HD stereo audio.

Fidelity

A high fidelity microphone on a webcam for pc enables the production of more natural, detailed sound from all over the room and not just in front of the webcam. Also, a webcam's high fidelity resolution gives you smooth video results.

Additional Functions to Consider When Choosing the Best Webcam for Laptop

Autofocus

The webcams available on the market today have fixed focus or autofocus two choices. If you need a webcam with a faster and more precise autofocus feature, ensure that you have some more money to acquire it because it's a bit more expensive than webcams without this feature. To obtain a natural and vibrant look in your formal videos, get a professional webcam for pc whose technology can distinguish people from walls and windows and apply the necessary optimization and focus.

Webcam Autofocus Function

AI Positioning

If you need a webcam with automatic detection of human faces, the number of attendees, and other things in the room despite movements during meetings, use a web camera that can support AI positioning.

Privacy Cover

Suppose you aren't using your external webcam, it'd be better to turn it OFF to block being spied on. If you use a built-in webcam, ensure that you install good computer security software to keep off hackers.

Supported Software & OS

If you use platforms for your video meetings frequently, then make sure to pick a kind of web camera support major software like Microsoft Teams, Skype, Zoom, BlueJeans, Cisco WebEx, GoToMeeting, etc. Also, it's important to confirm whether the web camera supports the operating system of your computer before buying a webcam.

Other Factors to Consider When Choosing the Best Webcam for PC

Webcam connection options: The webcam connection options enable faster transmission of data. Most webcams have USB (2.0 or 3.0) connections. You need at least a 1.5-meter cable to minimize webcam installation problems if you own a desktop computer.

Webcam mounting options: Before making a suitable webcam selection, these are the three mounting options you need to consider as discussed below;

  • ① The desktop option. This is ideal in case you have a lot of space on your desktop.

  • ② On the pin option. This is where your webcam is mounted on the monitor or laptop.

  • ③ Mounting on a stabilizer. This is when your webcam can be mounted onto a stabilizer, e.g. a stand, or a tripod.

FS Webcam Mounting Options

Related Articles:

Webcam Selection: How to Choose the Best Webcam for My Laptop or PC

Why Is External Webcam Better Than My Built-in Laptop Camera?

You might be interested in