English

How To Repair the Accidentally Cut Fiber Optic Cable?

Updated on Sep 29, 2021 by
217.1k

Fiber optic cable can be accidentally damaged, cut or smashed. According to the Electronic Technicians Association, one of the main cause of optical fiber failure is “backhoe fade” , during which the optical fiber cable is cut or damaged while digging. For this occasion, you can easily look for backhoe and get the cut cable. However, if it is caused by moles, it will likely be difficult to troubleshoot it. On the flip side, it means that the cost to repair fiber optic cable might be a little bit expensive because of the equipment involved. Here are a few tools and steps suggested for you to repair broken fiber optic cable.

Fiber Optic Cable Repair Kits That You May Need

(1) OTDR (Optical Time Domain Reflectometer)

The OTDR is widely used for the measurement of fiber length, transmission attenuation, joint attenuation and fault location. For more information about OTDR, please refer to Working Principle and Characteristics of OTDR.

OTDR

(2) Fiber Optic Cutter / Stripper

Fiber optic cable cutter and fiber optic stripper are important tools in the fiber optic splicing and some other fiber optic cable cutting applications.

Fiber optic cable cutter and fiber optic stripper

(3) High Precision Fiber Optic Cleaver

Fiber optic cleaver is used to cut the fiberglass for fusion splicing, also ideal for preparing fiber for pre-polished connectors to make a good end face. So it is very important in the fiber splicing process, and it usually works together with the fusion splicer to meet the end needs.

High Precision Fiber Optic Cleaver

(4) Fusion Splicer

Fiber optic fusion splicer may be the act of joining two optical fibers end-to-end using heat. The machine is to fuse both the fibers together in such a way that light passing with the fibers is not scattered or reflected back from the splice.

Fusion Splicer

Steps to Repair Fiber Optic Cable

Step 1: Use OTDR to Identify the Break in Fiber Optic Cable

The first thing you need to do is to look for the break in your fiber optic cables. Commonly, the fiber-optic technicians utilize a device which is known as an OTDR. With the ability to work like radar which sends a light pulse right down to the optical fiber cable. It will be deflected to your device when it encounters break. It helps technician know the position of the break.

Step 2: Use Fiber Optic Cutter to Cut Out the Damaged Fiber Optic Cable

After knowing the location of the break, you should dig up the fiber optic cables with the break. The fiber optic cutter is used to cut out the damaged section.

Step 3: Strip the Fiber Optic Cable by Fiber Optic Stripper

You should use fiber optic stripper to strip the fiber on the both end and peel the jacket gently to expose the fiber-optic tube inside. Then, cut any sheath and yarn by fiber optic cutting tools.

Strip the Fiber Optic Cable by Fiber Optic Stripper

Step 4: Trim Any Damage on the Optical Fiber Ends by High Precision Fiber Cleaver

The following picture lists the main 6 steps for fiber cleaving by high precision fiber cleaver.

6 steps for fiber cleaving by high precision fiber cleaver

Step 5: Clean the Striped Fiber Optic Cable

This step is crucial to ensure that your terminal will get a clean wire strip. You have to clean the stripped fiber with alcohol and lint-free wipes. Ensure that the fiber doesn’t touch anything.

Step 6: Splice the Fiber Optic Cable

Generally, there are two methods to splice optical fiber cable: (1) mechanical splicing; (2) fusion splicing.

(1) Mechanical Splicing

If you want to produce a mechanical connection, you need to put inline splice quick-connect fiber-optic connectors to the fiber. Hold the two fiber ends in a precisely aligned position thus enabling light to pass from one fiber into the other. (Typical loss: 0.3 dB)

(2) Fusion Splicing

In fusion splicing, a fusion splicer is used to precisely align the two fiber ends. You have to convey a fusion splice protector to the fiber, and place the fibers which is spliced within the fusion splicer. Then, the fiber ends are “fused” or “welded” together using some type of heat or electric arc. This produces a continuous connection between the fibers enabling very low loss light transmission. (Typical loss: 0.1 dB)

Step 7: Perform the Connection Test of Fiber Optic Cable with OTDR

The very last thing would be to see the connection of fiber-optic using the OTDR. Then put back those splices into the splice enclosure. Close the enclosure after which rebury the fiber optic cables.

Fiber Optic Cable Repair Kit Price

Item Description Price
OTDR FOTR-202 Handheld OTDR with FC/SC Connector $ 1,000.00
Fiber Optic Cutter Fiber Optic Kevlar Cutter $ 21.00
Fiber Optic Stripper FO 103-T-250-J Original Miller Triple Holes Fiber Optic Stripper $ 110.00
High Precision Fiber Optic Cleaver FS-08C High Precision Fiber Optic Cleaver $ 110.00
Fusion Splicer DVP-740 Mini FTTx Fusion Splicer $ 3,000.00

Conclusion

The failure of optical fiber cable will lead to a interruption for data transmission, so to fix the damaged optical cable in time is an important task. After going through the steps for repairing the fiber optic cable, you may wonder whether you should chose the mechanical splicing or fusion splicing. Here the suggestion is if the price is not a factor, you should go with fusion splicing since the signal loss is low. If you have a tight budget, you can consider mechanical splicing, which doesn’t requires an expensive tool.

Related Article: What Kind of Fiber Patch Cord Should I Choose?

Tags

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k