English

Layer 3 Switch Vs Router: What Is Your Best Bet?

Updated on Nov 24, 2020 by
132.5k

In the networking world, term like layer 3 switch and router gets thrown around often – both are seeing broad deployment in network data transmission. Generally speaking, a layer 3 switch connects hosts to form local area networks (LANs) while routers connect multiple LANs into wide area networks (WANs). We may get confused regarding layer 3 switch vs router: they bear much similarities as they both support the same routing protocols, inspect incoming packets and make dynamic routing decisions based on the source and destination addresses inside. But they also differ in performance, flexibility, cost and etc. So we’re going to explain them in an explicit way, and help you to make the right decision.

layer 3 switch vs router

Layer 3 Switch: Mix And Match Layer 2/3 Switching

A layer 3 switch is a device that forwards traffic (frames) based on layer 3 information (mainly through mac-address). Layer 3 switch supports all switching features, while also has some basic routing functions to route between the VLANs. Layer 3 switch is conceived as a technology to improve network routing performance on large LANs. Of a layer 3 switch, layer forwarding is performed by specialized ASICs – it is faster than routers, but they usually lack some of the advanced functionalities of routers. Unlike routers, a layer 3 switch is less likely to experience network latency since packets don’t have to make additional steps through a router. Given that layer 3 switches perform functions associated with both layer 2 and layer 3, it is also refer to as “multilayer switch”, and some 10GbE switch and Gigabit PoE switch are of this type.

layer 3 switch

Router: For Different Networks & Protocols

Router is a ubiquitous hardware applied in home and small business networks. It allows communication between devices that attached to it and the internet. A router can forward traffic (packets) based on layer 3 information using IP address. This allows the network to go across different Protocols. Routers also serve as the first line security that protecting the network from any attack and intrusion. Working to route the packets to their destination, a router analyzes the layer 3 destination address of every packet, and decides the best next hop for it. This process takes time, and hence every packet encounters some delay because of this.

basic router connection

The basic features of layer 3 switch vs router are listed below:

Features
Layer 3 Switch
Router
Layer 3 basic routing
Yes
Yes
Traffic management
Yes
Yes
WIC card support
No
Yes
Advance routing features
No
Yes
Forwarding Architecture
Hardware-ASIC
Software-IOS
RMON support
Yes
No
Policy performance
High
Low
WAN support
No
Yes
WAN interfaces
No
Yes
QoS features
No
Yes
NAT
No
Yes
LAN capabilities
Yes
No

Layer 3 Switch Vs Router: Similarities and Differences

Similarities:

A layer 3 switch is both a switch and a router: it can be regarded as a router with multiple Ethernet ports and with switching function. layer 3 switch enable packets switching by inspecting both their IP addresses and their MAC addresses. Layer 3 switches are thus able to segregate ports into separate VLANs and perform the routing between them. Like traditional router, a layer 3 switch can also be configured to support routing protocols such as RIP, OSPF, and EIGRP.

Differences:

Hardware - The key difference between layer 3 switch vs router lies in the hardware. The hardware inside a layer 3 switch blends that of traditional switches and routers, improving some of a router’s software logic with integrated circuit hardware to offer better performance for LANs. Additionally, designed specifically for use on intranets, a layer 3 switch usually has no WAN ports and features a traditional router usually gets. So layer 3 switch is most used to support routing between VLANs.

Interfaces - Another difference regarding a layer 3 switch vs router is that a Layer 3 switch is limited in interfaces it supported (usually just Ethernet for RJ45 and single mode/multimode fiber). While a router have more options like SDH, SONET, E1/T1 etc. Moreover, routers were devices that connected the LAN to the WAN and switches were just LAN devices.

Working Principle – Layer 3 switch looks at the MAC address of the destination host and sends the frame only to that recipient. A router refers to the target IP address instead of its MAC address, thus it generally provides more functionality than mere packet routing, such as IP address assignment (DHCP) and firewall filtering.

Except for the three major differences concerning layer 3 switch vs router, some other aspects are summarized in the following chart to help distinguish layer 3 switch from router.

Attribute
Layer 3 Switch
Router
Scope
LAN for office, data center and campus environment
WAN for office, data center and campus environment
Key Functionality
Routes across different subnets or VLANs on a campus LAN
Routes across different networks across WAN are communicated and routed by a router
Edge Technologies Support
Not supported
NAT, firewalling, tunneling, IPSec
Size of Routing Table
Smaller routing table compared to router
Considerably bigger to support multiple route entries
Forwarding Decision
Forwarding is performed by specialized ASICs
Performed by software
Interface Support
Ethernet ports (copper/fiber)
Ethernet ports (copper/fiber), interfaces like SONT, OC-N, T1/T3 etc.
Throughout
High throughput
Lower than Layer 3 switches
Switching Capacity
High switching capacity
Lower than Layer 3 switches
Cost
Low cost
High cost
Port Density
High
Low

Layer 3 Switch Vs Router: How to Choose?

One of the general talk relating layer 3 switch vs router is that if there is a router why we required layer 3 switch. In fact, they each can be deployed to various situations and scenarios. Based on the similarities and differences we’ve explained, your choices actually depends on your network design and what you are trying to accomplish.

For Layer 3 Switch:

Lack of WAN ability, the application of layer 3 switches often falls into intranet environments with a sufficiently large scale of device subnets and traffic. It can justify the following scenarios:

Departments need their own broadcast domains for performance or security.
Connect your Hub rooms and make a layer 3 decision, providing more Ethernet interfaces for direct server form connectivity than router.
Connect your inter-offices via layer 2 circuits by the ISP, you can directly terminate the link on the layer 3 switch and configure routing on it at the same time.
When you need more through-put and direct access and inter-VLAN communication, a layer 3 switch is the best bet.
Network with a lot of broadcasts that needs better performance VLANS.

For Router:

As WAN links become more Ethernet based, there is an increasing trend to substitute layer 3 switches for routers. However, router still possess some special features that a layer 3 switch cannot support. It is unreplaceable in these situations.

If you’re about to connect an ISP directly to provide internet, router is made for this.
If you need to build tunnels between your offices, for example, to connect two offices over public internet in a more secured way, a router can better suit the need.
If you are a CE participating in MPLS configuration then you need a router.

Conclusion

When regarding to choose between a layer 3 switch vs router, you need to understand the business requirement before make your decision: in general, it is proper to get a router when most of the time your device does the routing, otherwise, a layer 3 switch may fit better when you need more ports, better network performance and VLAN segmentation. FS.com provides a full set of network switch solutions and products, including SFP switch, copper switch and higher-end 40/100G switch. For more details, kindly contact us via sales@fs.com.

Related Article: What Is VPN Router and Why You Need It?

You might be interested in

Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge