English

Muxponder vs Transponder: What's Their Difference in OTN Network?

Updated on Mar 8, 2022 by
12.7k

Enterprise data centers and ISPs are facing increasing demands for low latencies, data security, higher speed and longer transmission distance in networks. Both transponders and muxponders are key components for enhancing their networks by meeting those demands. In Optical Transport Network (OTN), both of them belong to the optical transform unit (OTU)/wavelength conversion unit. Then what's the difference between muxponder vs. transponder? In this post, we will dig into the difference and their applications in the OTN network.

Muxponder vs. Transponder: Overview

What Is Optical Muxponder?

In fiber optical communications, muxponders can combine multiple services into a single wavelength/uplink by utilizing ITU optical transport network (OTN) protocol for mapping the services over the same uplink. A muxponder can maximize the fiber capacity by reducing the number of wavelengths that are needed to transport data, enabling more efficient use of fibers and making them ideal for future network growth. Carriers, ISPs and other industries often adopt muxponders since they have carrier-grade features like flexible remote monitoring and management, link diagnostic tools, and bi-directional performance monitoring of the client service interfaces and uplink.

Optical Muxponder

What Is Optical Transponder?

Optical transponders are often adopted to extend the optical transmission distance by wavelength conversion. It converts the optical signal of the customer side into an electrical signal by performing the 3Rs (retiming reshaping and re-amplifying) or by mapping it into the optical transport network, and then converts it back to an optical signal toward the line side. Performing 3Rs can ensure a reliable error-free optical communication link.

A transponder can eliminate the need for generators by mapping the signals into standard OTN which supports forward error correction (FEC) in long-haul and metro amplified links. Optical transponders are usually classified according to their data rates and signal transmission range. Carriers, ISPs and other industries often deploy transponders to build their carrier-grade backbones and DCI networks, or for providing managed services to enterprises.Optical Transponder

Main Difference Between Muxponder vs. Transponder in OTN Network

In fiber optical communications, both transponders and muxponders are the elements that receive and send the signals over the fiber. Muxponders combine multiplex low-capacity services into a single high-capacity wavelength/uplink. Transponders convert each optical signal from the customer equipment to a wavelength.

The main difference between muxponders vs. transponders is that muxponders have the additional capacity to combine multiple services into a single wavelength by multiplexing several channels to a higher-order signal, which enables more efficient use of fibers than a transponder.

otn 100g Muxponder

Optical Transponder

Applications of Transponder and Muxponder

Functions of Transponder & Muxponder in WDM Network

Transponders and muxponders are used to conduct OEO (Optical-Electrical-Optical) applications in the WDM network. The functions mainly include:

  • Amplify the optical signal- They can convert a weak input signal into a strong output signal.

  • Multimode to single-mode- Extend the transmission distance by multimode to single-mode conversion.

  • Fiber type conversion- Maximum the fiber capacity by fiber type conversion.

  • Optical wavelength conversion- Achieve WDM solution by fiber wavelength conversion.

When to Use Transponders and Muxponders?

Transponders and muxponders can automatically receive, amplify and re-transmit signals on new wavelengths without any changes to the data carried over the signal at all, which can not be achieved by only adopting transceivers.

 Transponders and Muxponders

A WDM solution based on active transponders or muxponders is a better choice, especially when transceivers and switches are not fully compatible or when transceivers alone are not to enough meet your needs. For instance, you may need higher speed, longer transmission distance, and higher security than that achieved by the combination of switches and routers already installed. Below are some cases where using a transponder-based solution can solve common challenges:

1. If you want to encrypt your networks, muxponders and transponders will contribute to protecting sensitive data and meet regulatory requirements with encryption.

2. If the data needs to be transmitted over a very long distance which the transceivers don't support long-distance WDM, an OEO-based solution with transponders and muxponders can extend the distance of WDM network with FEC error correction.

3. If ISPs need to hand off a gray (i.e. non-WDM) signal to end-users, transponders and muxponders can realize it and make it easier for ISPs to restrict the bandwidth of optical connection.

4. If the data needs to be transmitted at a higher rate in WDM networks than that achieved by transceivers, transponders and muxponders are another way to support a faster rate without turning to faster transceivers which could be larger than the vendors prefer.

FS Transponder-based Solution to Meet Your Needs

Generally, it's highly individual when it comes to whether you need transponders and what transponders you need. There are many factors you should take into consideration before purchasing, such as the compatibility with the existing switches and transceivers, the speed and distance you intend to cover and other requirements.

FS provides the best 10G/25G/100G transponders and 10G/100G/200G muxponders, together with professional chassis and accessories to meet all your needs.

Muxponder vs. Transponder

Related Article:

The Versatile Optical Transponder (OEO) in WDM System

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k