English

Open Source vs Open Networking vs SDN: What's the Difference

Updated on May 24, 2022 by
9.6k

FS Data Center Switches

Open source, open networking, and SDN (software-defined networking) are all common concepts related to open in networking. These three terms are often intertwined together and confuse a lot of people. This article will provide a comprehensive introduction to open source and make a comparison of open source, open networking, and SDN.

What Is Open Source?

Open source is a term indicating that something is publicly accessible. It most commonly refers to software or a program whose source code can be freely used, modified, and shared by anybody.

This term originated from software development and refers to a specific approach to creating computer programs. With the development of the Internet, the demand for reworking plenty of source code is increasing. When the source code is opened to the public, people can freely view, learn, share, modify or possibly improve the software when they have access to that code. It is convenient for creating diverse communication paths and interactive technical communities. It also can help construct multiple network equipment such as Ethernet switches. Therefore, open source draws more and more attention. Many people who focus on developing specific software, such as developers, engineers, service providers, vendors, etc., joined open source projects.

What Is Open Networking?

Open networking is based on open standards (such as the OpenFlow protocol) and bare-metal hardware with flexible choices of networking operating system (OS). It aims at breaking down the propriety nature of software and hardware to deliver an agile, scalable, and programmable network, which can adapt to the varying requirements. Open networks offer high flexibility for enterprises, such as the freedom to choose devices, software, and network operating systems, which enables businesses to reduce their costs, increase capabilities and drive better ROI.

What Is Software-defined Networking?

Software-defined networking (SDN) is an architecture that decouples the control plane from the packet-forwarding (data) plane within the network to create a software-programmable infrastructure. It is an approach to network virtualization and containerization, with which network configuration and management are performed from a central dashboard instead of connecting every specific switch or server through the network. It allows enterprises and service providers to optimize network resources and respond quickly to changing business requirements.

Comparison

Open Source vs Open Networking

Just as their names imply, both open networking and open source hinge on the concept of being open. But there is a clear difference between open networking and open source. Open networking and its network operating systems do not require open source.

Open networking allows users to choose OS freely such as Cumulus Networks' Cumulus Linux, Big Switch Networks' Switch Light, and Pica8's PicOS® installed on commodity hardware or vendor hardware. Though these network OSs are commonly based on Linux, they do not need to be open source.

To summarize, open source is any software or program available for public use and modification, while open networking is based on software designed to create more flexibility, interoperability, and automation for networking devices.

Open Source vs SDN

SDN and open source play important roles in helping achieve open networking, but they are definitely not the same thing.

A typical SDN has three parts - applications, controllers, and networking devices. SDN controller communicates with applications through northbound application programming interfaces (APIs). While it communicates with switches or routers using southbound interfaces such as OpenFlow. Since the OpenFlow protocol is an example of a pervasive open source component of networking, some people hold that SDN is the same as open source software. Actually, most SDN architectures remain using proprietary or open source software on third-party or commodity hardware.

In addition, as stated, SDN allows for open networking. This makes some people consider that SDN is open source as well. Actually, SDN can be done in a more limited environment without open networking, let alone open networking is not necessarily open source.

All in all, SDN itself is not open source. It is valued for its ability of functional separation, network virtualization, and automation through programmability.

Aspect Open Source Open Networking SDN (Software-Defined Networking)
Definition Software with source code accessible and modifiable by anyone Networking model that encourages open standards, interoperability, and programmability Network architecture that separates control plane from data plane, enabling centralized control
Focus Code accessibility and modification rights for software Promotes open standards, collaborative development, and interoperability in networking Centralized control, programmability, and abstraction of network infrastructure
Objective Encourages community-driven collaboration and transparency in software development Aims for open, flexible, and interoperable networking solutions Enhances network agility, scalability, and management through centralized control and programmability
Examples Linux, Apache, Firefox OpenFlow, ONAP, OpenDaylight Cisco ACI, VMware NSX, Open vSwitch
Influence Revolutionized software development with collaborative, transparent models Pushes for open standards and interoperability in networking hardware and software Alters network architecture, allowing programmable, centralized network control
 

Conclusion

In conclusion, understanding the differences between open source, open networking, and SDN is crucial for professionals and enthusiasts in the networking field. Open source promotes collaboration and transparency, open networking fosters flexibility and innovation, while SDN revolutionizes traditional networking architectures. Integrating these concepts allows for the creation of agile, scalable, and future-proof networks that can adapt to evolving business needs.

You might be interested in

Knowledge
See profile for Howard.
Howard
What Is Open Networking?
Jun 1, 2022
6.1k
Knowledge
See profile for Howard.
Howard
What Is Software-Defined Networking (SDN)?
Jun 1, 2022
10.3k
Knowledge
See profile for Howard.
Howard
Cloud Networking: A Comprehensive Guide
Jun 17, 2022
2.9k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge