English

SD-WAN vs MPLS: Pros and Cons

Updated on May 25, 2022 by
11.6k

FS Data Center Switches

As the demand for cloud-based applications and bandwidth requirements continue to grow and branch offices expand, some enterprises and service providers begin to deploy wide area network (WAN) services. MPLS and SD-WAN are the two most important technologies in WAN services. This post will compare MPLS and SD-WAN to give you an idea of which technology is best for you.

MPLS Basics

MPLS (Multiprotocol Label Switching) is a protocol for efficient network traffic flow between multiple locations. MPLS operates similarly on Ethernet switches and routers, sitting between layers 2 and layer 3 networks. MPLS uses labels with important information so that traffic can be delivered to its destination without the need for in-depth packet analysis by routers. This enables fast packet forwarding and routing within a network, eliminating the inefficiencies of traditional Internet routing. In the MPLS network, the MPLS switch transfers data by popping off its label and sending the packet to the next switch label in the sequence. MPLS network provides customers with a method of prioritizing traffic, thus bringing a sense of traffic predictability within the network. This allows users to leverage a single network connection for multiple applications, providing high-performance and reliable connectivity for critical application traffic.

As illustrated in the figure, time-sensitive applications such as video and voice can take the highest priority while less critical applications would take the lowest priority and still function properly.

MPLS Network

SD-WAN Basics

Data centers and enterprises are demanding more flexible, open, and cloud-based WAN technologies, rather than proprietary or specialized WAN technology that often involves expensive, fixed circuits, or proprietary hardware. Therefore, SD-WAN (Software-Defined Wide Area Network) is developed and widely applied for WAN connections. SD-WAN erases geographic boundaries, enabling communications between different network endpoints. Thus, it is ideally suited for connectivity between branch offices and central enterprise networks, or between data centers separated by geographic distance. Featuring zero-touch deployment, SD-WAN simplifies management and reduces recurring network costs.

In the SD-WAN architecture, a company can benefit from end-to-end encryption across the entire network, including the wireless WAN, the Internet as well as the private MPLS. All devices and endpoints are completely authenticated thanks to the scalable key-exchange functionality and software-defined security from cloud services in the SD-WAN architecture.

MPLS Pros and Cons

Advantages of MPLS:

  • High Performance: MPLS predetermines network paths and transports traffic only along the paths. And it uses labels to isolate packets and assign a higher priority to important network traffic, which eliminates the complexity of routing traffic and provides higher performance.

  • Reliability: MPLS ensures reliable delivery of packets and maintains the quality of real-time protocols.

Disadvantages of MPLS:

  • Time-consuming Deployment: Configuring and deploying MPLS circuits is a slow process. Organizations using MPLS have difficulty reacting quickly to sudden increases in bandwidth demands.

  • Cost: With MPLS, the price per bandwidth is much higher than a broadband Internet connection.

  • Accessibility: It is made exclusive for point-to-point connectivity, meaning that cloud applications and SaaS cannot be accessed directly using MPLS.

SD-WAN Pros and Cons

Advantages of SD-WAN:

  • Performance: SD-WAN increases business agility and assures application performance.

  • Costs: SD-WAN removes expensive routing hardware and provides developers the freedom of choice without vendor lock-in constraints, bringing substantial savings. And it can leverage lower-cost services to reduce WAN connectivity costs.

  • No Geographic Restrictions: SD-WAN erases geographic boundaries and can add and remove connections at any site based on business needs.

  • Visibility and Control: SD-WAN can control the network more proactively and enable enterprises to mix and match connections based on content priorities.

  • Operation: SD-WAN simplifies operations through zero-touch provisioning and cloud-based management.

Disadvantages of SD-WAN:

  • Security: SD-WAN lacks on-site security features. SD-WAN makes every branch connected to the Internet, leaving every site open to attacks. And a data breach on one site could affect the entire organization.

  • Errors: SD-WANs may experience jitter and packet loss.

SD-WAN

SD-WAN vs MPLS: Key Differences

After looking through the pros and cons of SD-WAN and MPLS, the differences between SD-WAN and MPLS might be much clearer. To help you fully understand these two technologies, MPLS and SD-WAN are compared in three key areas: cost, reliability, and security.

Cost

Managing the costs of WAN links is a challenge for global enterprises. As mentioned before, the traditional MPLS networks have been proven to be very expensive, and the emerging alternatives SD-WAN presents compelling price as well as performance benefits. Because MPLS networks contain bandwidth-hungry multimedia content, such as videos and AR/VR, the high cost per megabit required for MPLS is unattainable. In contrast, SD-WAN provides optimized multi-point connectivity by distributed, private data traffic exchange and control points, effectively reducing costs.

Reliability

The reliability of the traffic flowing for businesses is a key concern for enterprises. SD-WAN tends to deliver a business-class, secure, and simple cloud-enabled WAN connection with open and software-based technology. MPLS technology, on the other hand, provides reliable, high-performance connectivity over dedicated network circuits. And it can effectively avoid packet loss. The reliability of both technologies is especially important for maintaining the quality of real-time devices, such as VoIP telephony, video conferencing, or remote desktops.

Security

MPLS does not provide built-in security functionality and any sort of analysis of the data. For MPLS connectivity, traffic needs to be inspected for malware or other vulnerabilities, which requires network firewalls and additional security features to be deployed at the endpoints of the connection. To be fair, many SD-WAN solutions suffer from the same problem. But some SD-WAN solutions include integrated security by unifying secure connectivity.

Can SD-WAN Replace MPLS?

Although SD-WAN and MPLS have advantages and disadvantages in different aspects, SD-WAN can offer similar performance and reliability to dedicated MPLS circuits.

SD-WAN enables organizations to save on network investment by using relatively low-cost network links for most traffic. And SD-WAN also improves organizational WAN flexibility by eliminating the limitations of MPLS circuits. SD-WAN supports bandwidth expansion according to organizations' needs, without the delays associated with MPLS configuration. It optimizes routing so that traffic can be efficiently delivered to its destination, not limited to predefined MPLS circuit paths. And SD-WAN traffic can be routed anywhere, regardless of the geographic restriction the MPLS circuit suffers. That's why SD-WAN can replace MPLS to some extent.

Can SD-WAN and MPLS Work Together?

SD-WAN and MPLS have complementary advantages. The two technologies can work together to address some of their previous limitations. SD-WAN is an overlay technology defined by software, and MPLS sits underneath it to provide transport services.

You don't have to choose between SD-WAN or MPLS. In fact, you can use them together to provide a free network architecture to support your current and future business.

You might be interested in

Knowledge
See profile for Howard.
Howard
What Is Open Networking?
Jun 1, 2022
6.1k
Knowledge
Knowledge
See profile for Howard.
Howard
What Is Software-Defined Networking (SDN)?
Jun 1, 2022
10.3k
Knowledge
See profile for Moris.
Moris
VPN vs MPLS: What’s the Difference?
Jul 8, 2022
57.9k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge