English

Switch Stacking vs Trunking vs Uplink: Which to Choose for Connecting Switches?

Updated on Dec 14, 2021 by
40.4k

Normally, in a network system, several network switches are combined together to meet network needs (port number, certain functions, etc.) when one switch can't. There are various approaches to connect multiple switches, among which switch stacking vs trunking vs uplink are the most prevailing ones. This post aims to elaborate on the three switch connection methods and indicate which one to choose in practice.

What Are Switch Stacking, Switch Trunking, Switch Uplink?

What Is Switch Stacking?

Switch stacking is to combine multiple stackable switches via a dedicated stacking port and stack cable to operate as one logical unit and share the same IP address. Not all network switches support stacking, it depends on different brands. And stacking can be achieved only between the same switch models or the same series of a brand, like between FS S5860-20SQ switches or mixed stacking for S5860-20SQ and S5860-24XB-U switches shown in the figure below. The port density of a stack unit is the sum of the combined ports and the switching capacity will be much augmented as stacking connects the backplane of the switches thus having full backplane speed connectivity between the switches. The performance of the whole network system has been largely enhanced, so has the management for these switches. Know more information about switch stacking here: Switch Stacking Explained: Basis, Configuration & FAQs.

Figure 1: Switch Stacking Using FS S5860-20SQ, S5860-24XB-U.

What Is Switch Trunking?

Switch trunking refers to a method that a network system provides network access to many switches by sharing a set of links instead of providing them individually. It is similar to the structure of a tree with one trunk and many branches. Based on layer 2 technology, trunking is often used to form internetwork including LANs, VLANs, and WANs. It enables packets encapsulated for multiple VLANs to cross exactly the same port and then retains the traffic separation among them. Just as the figure below shows, each trunk switch is configured with 2 VLANs (10 and 20). There is a single communications channel (VLAN trunk link) between the two switches, over which traffic for both VLANs can pass. In the VLAN trunking link, each switch has a port designated as a trunk port to allow data flow between these VLANs.

Figure 2: VLAN Trunking with two FS S3910-48TS 48-Port Switches

What Is Switch Uplink?

Switch uplink is a subjective concept which means that the cascading of ports between two switches is facilitated via a so-called “uplink port”. Uplink ports often have relatively higher data rates than normal ports and are used to connect larger networks via a straight-through cable or direct attach cable. As shown below, to build uplinks to achieve high availability for campus networks, connect the uplink port on one switch to the standard port on another uplink switch to help expand the network’s size, and a 3-layer cascading are implemented. When you connect two devices, the uplink port on only one of them is used. If you connect two uplink ports via straight-through cable, the result is the same as using two normal ports - makes the devices fail to communicate. This is where the difference between switch stacking vs cascading lies.

Figure 3: Switch Uplink with FS S3910-24TS, S5860-20SQ, N8560-48BC

Switch Stacking vs Trunking vs Uplink: What Are the Differences?

The table below shows the differences among switch stacking vs trunking vs uplink.

Feature Switch Stacking Switch Trunking Switch Uplink
Port Density The port density of a stack unit is the sum of the combined ports The ports of the switches can't be superposed The ports of the switches can't be superposed
Switch Interoperability Switch stacking requires the same model or series of Ethernet switches from one vendor Most network switches support trunking regardless of models or vendors, ensuring connections between different VLANs Switch uplink offers a perfect fit for connecting switches from the different product family
Number of Switches Switch stacking is stricter about the number of switches to be stacked(different vendors may have their own standards) Switch trunking is flexible in the number of switches. You can just add as many switches for trunking based on your needs Switch uplink is flexible in the number of switches. You can just add as many switches for uplink based on your needs
Port Connection Through dedicated stacking ports (when a switch has) or through uplink ports Any port can be designated as a trunk port to realize switch trunking Generally, only uplink ports can be used to achieve switch uplink
Performance Each stack member shares a single IP address and acts as a whole unit There is a single communication channel (VLAN trunking link) between the connected switches, over which traffic for all VLANs can pass Each switch connected stands alone and works independently
Application When you need to expand your bandwidth or provide link redundancy to prevent failure in the link. Even if one link breaks in the stack unit, the other switches can continue to work. You can handle multiple signals simultaneously and extend your configured VLANs. It’s suitable for public places such as apartments or dormitories that cover many sub-networks. Uplink port is usually utilized to connect to aggregation switch or core switch

Switch Stacking vs Trunking vs Uplink: Which One to Choose?

Switch stacking vs trunking vs uplink, which one to choose depends on your real needs. In general, switch stacking offers more bandwidth while simplifies network management, proven as a more cost-effective alternative to chassis-based higher-end switches. Switch trunking is a great option for inter-network including LANs, VLANs, and WANs, which requires network integrity as well as retains the traffic separation. Switch uplink is preferred when you want to upgrade your network while leveraging the existing infrastructure. For example, in the network application of 10G-to-40G, you can connect the QSFP+ uplink port on a 10GBase-T switch to a 40G switch in common cases.

Related Article

How to Connect Multiple Ethernet Switches

MLAG vs. Stacking: What Is Your Option?

MLAG vs. Stacking vs. LACP

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k