English

Understanding the Role of Fiber Enclosure in Data Center

Posted on Feb 1, 2024 by
498

In the ever-evolving landscape of data centers, efficient cable management is paramount to ensure optimal performance, reliability, and longevity of networking equipment. Fiber enclosures, encompassing both wall mount and rack mount varieties, have emerged as essential components in creating high-density and secure cabling environments. This article delves into the practical applications of fiber enclosures, exploring the role of fiber enclosure in data center cabling.

What Is Fiber Enclosure?

Fiber enclosures come in two primary types: wall mount and rack mount. Wall-mount fiber enclosures are typically installed on walls, facilitating the housing and distribution of fiber optic cables for indoor applications. On the other hand, rack-mount fiber enclosures are employed between or within racks, offering a versatile solution for fiber cable connectivity. These fiber enclosures are commonly used together with fiber optic panels, such as LC, SC, or MTP®/MPO, and may include fiber splice trays or MTP®/MPO-LC fiber cassettes. Further, rack-mount fiber enclosure has different open-close designs such as a toolless removable top cover, sliding and tilt-down drawer, detachable cable lacer panel, and bar. The elaborate design of various fiber enclosures allows different deployment scenarios and better caters to specific requirements. You can choose the fiber enclosure through 1U Rack Enclosure Types and Selection Guideline | FS Community.

What's the Role of Fiber Enclosure in Data Center?

Next, we will take the fiber optical enclosure of FS as an example to show its various applications and advantages in data center cabling.

The Cable Management Function of Fiber Enclosure

As the trend in data center cabling leans towards high density, fiber enclosures have become indispensable tools for cable management. Such as rack-mount fiber enclosure, by using a cable manager or cable tray, cables can be organized and arranged neatly, which can reduce cable confusion and entanglement and improve the efficiency of maintenance and troubleshooting. At the same time, it houses and fixes fiber optic panels or fiber optic cassettes in a box for better management and protection. The following figure shows the FS FHD® (FS High Density) rack mount fiber enclosures installed on racks to manage the OS2 and OM4 fibers to provide versatility and flexibility with a fully modular solution for cable management in data center cabling.

Understanding the Role of Fiber Enclosure in Data Center

Realizing Multi-functional Cabling in Data Centers

Hybrid Solution for Mixing Fiber and Copper Cabling

Sometimes, the data center needs to carry out photoelectric hybrid wiring to ensure the normal operation of network services (some devices need power transmission, such as POE cameras, and some need high-speed transmission of optical cables). Blank Fiber enclosure can realize this wiring, which can be matched with an FHD® 6-port multimedia copper/fiber modular panel, and users can carry out photoelectric combined wiring according to the actual situation (as shown below). Adapters and connectors can be used to enable the termination and connection of the optical fiber cables, while RJ45 connectors or other appropriate connectors can be used for the network cables. By using an FHD-FPP5DRL fiber enclosure, you can house and manage both the optical fiber cables and network cables in a unified manner.

Understanding the Role of Fiber Enclosure in Data Center

Fiber Splice Cabling in Fiber Enclosures

Besides the applications mentioned above, fiber splicing is also viral in data center cabling. It is usually evitable to splice fiber optic cables with fiber pigtails in the data center cabling, which requires a lower space requirement and has a better network performance compared with other fiber optic termination methods. Fiber splice trays are usually installed in fiber enclosures to provide a safe and easy-to-manage environment for fiber splices. Here is the example of a fiber splice tray used in the FHD-1UFCE fiber enclosure of FS.COM as shown in the following picture. It is a 96-fiber enclosure with four 24-fiber optic panels on the front panel. This fiber enclosure can hold up to four 24-fiber splice trays to provide the space for 96 fiber optic splices.

Understanding the Role of Fiber Enclosure in Data Center

High-Density Cabling

Fiber enclosures play a crucial role in high-density cabling systems to help manage thousands of fiber optic cables in the data center cabling. For instance, the FS FHD-4UFCE rack-mount fiber enclosure can be configured with 12 fiber optic panels or fiber cassettes, allowing the termination of 432 fibers serving as intermediate connections between data center backbones and patching cabling. The sliding drawer of the fiber enclosure enables it to slide to the front for maximum access to fiber connections. It is ideal for high-density cabling in confined spaces and reducing installation time.

Understanding the Role of Fiber Enclosure in Data Center

Protecting Cables and Reducing Signal Loss

Fiber enclosures protect cables and minimize signal loss in multiple ways.

Electromagnetic Interference

Firstly, they shield against electromagnetic interference from electronic devices, wireless signals, and power lines, which can degrade cable quality.

Physical Protection

Secondly, they provide physical protection by housing cables internally, safeguarding them from pressure, tension, bending, or squeezing. Additionally, the enclosures incorporate cable management systems to secure and minimize cable movement, reducing the risk of damage.

Airflow and Cooling

Lastly, the fiber enclosures, effectively organizing and routing cables, prevent restrictions to cool air reaching networking equipment ports. This mitigates the risk of early equipment failure due to inadequate cooling safeguards cable quality and extends their lifespan.

Conclusion

In the dynamic landscape of data centers, where the demand for efficient and high-performing networks is ever-increasing, the strategic deployment of fiber enclosures will play a pivotal role in ensuring the seamless operation of data centers.

You might be interested in

Knowledge
See profile for Margaret.
Margaret
Fiber Optic Closure Basics and Selection Guide
Jul 27, 2020
27.7k
Knowledge
See profile for Margaret.
Margaret
Data Center Cabling Guide
May 19, 2023
31.4k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge