English

Can We Use Third-party Dell SFP for Dell Switches?

Updated on Jul 21, 2021 by
19.3k

Using third-party transceiver module or Original Equipment Manufacturer (OEM) optical transceivers for major brand switches has remained controversial. It is no doubt that most enterprises and individual users use third-party transceiver modules because they are more money-saving based on the same quality as the OEM optical transceivers.

But one concern about using third-party optics are based on assumption is that 3rd-party hardware will void OEM device warranty and support. As one popular networking equipment provider, Dell also made such notice about warranty policy. “DELL:What is covered by this limited hardware warranty? - This limited hardware warranty covers defects in materials and workmanship in your Dell-branded hardware products, including Dell-branded peripheral products. ” (Resource: http://www.dell.com/learn/us/en/id/terms-conditions/art-limited-hardware-warranties)

Why network equipment vendors have such strict warranty policy?

This is because the original network equipment could make more profit. Most of the time, a network equipment vendor’s sales rep would threaten their customers that if they install third-party transceiver modules in their networking or server equipment, this will make their warranty policy invalid. In this way, the manufacturer tries to coerce customers into purchasing branded transceiver modules from them, usually at much higher prices than third-party charges. In the end, branded vendors can make more profit.

Dell’s official notice of using Non-Dell optics

Besides strict warranty policy, network equipment vendors like Dell has official notice of using Non-Dell optic modules in Dell products as well. “If a non-Dell optic is plugged into a Dell switch, the switch may continue to perform as well as the optic allows. If a non-Dell DAC cable, which is standards compliant, is plugged into a Dell switch, the switch will continue to perform as well as the cable allows.” (Resource: http://en.community.dell.com/techcenter/networking/w/wiki/11905.faq-optics-and-cables#A3)

That means we can use 3-rd-party optics in Dell switches as long as the standard allows. However, in Dell’s community, customers are generally discouraged from installing non-Dell optics in Dell switches. As the Dell Support claim, in order to ensure that users enjoy the most reliable network experience with Dell switches, Dell goes through a very stringent and lengthy process of optics validation, qualification, and certification. If any of reported issue is caused by the use of non-Dell optics, then they will recommend that customer replace the unsupported non-dell optics with qualified Dell optics. So Dell recommends that end user test non-Dell optics appropriately, prior to deploying them in production environment.

Does 3rd-party transceiver ensure same working & quality standards as DELL OEM Optics?

Definitely yes! The total amount of manufacturing fiber optics can be counted in the world, and they produce fiber optics for everyone. Those heavily-discounted third-party devices may be made in the same facilities as the official Cisco, HP, or Juniper units. And since optical transceivers are fully specified by internationally agreed-upon standards anyway, there's no risk of incompatibilities.

dell-sfp-transceiver

Thanks to a multi-source agreement (MSA). It is defined by users and manufacturers of transceiver modules to define standards—are standardized for use in a variety of devices such as switches and routers. As a result, there is absolutely no difference in hardware for official branded transceiver and reliable 3rd party optical transceiver, as much as four or ten times cost difference. The performance is the same because all manufacturers follow same rules same standards.

Can 3rd-party manufacturer provide all the Dell compatible optics?

For Dell optics, almost every 3rd-party optics manufacturer could produce the every module of it. Like being said, the standards of all transceiver modules are already being defined. Thus, 3rd-party optics vendor could absolutely offer all the Dell compatible optics. Actually, they could offer more transceiver modules than the OEM manufacturer.

FS.com offers a series of Dell compatible optical modules and optical cables, including SFP, SFP+, SFP28, QSFP+, QSFP28, DACs and AOCs. All of them are fully tested and can work with Dell series switches, including Dell networking, Dell Force10, Dell PowerConnect, and etc. Our compact, high-density and high-speed Dell compatible optical transceivers, DACs and AOCs are able to offer cost-effective options for Dell brand favors. If you are eager to read more about comparison between 3rd-party optics and OEM optics, you can further read this article 3rd-party Optics Vs. OEM Optics.

Are there any other reasons we should buy from FS.com?

In addition to Dell OEM optics, FS.com also provided custom service. You can customize the transmission distance, temperature and etc. We could meet almost all the special requirement of transceiver modules. The production of transceiver optics is taking place according to the respective current MSA standard. The continuous control of product quality before, during and after the manufacturing process is the top priority. Each produced batch is scheduled with standardized quality assurance procedures and the production process is constantly monitored and supervised.

We truly understand the value of compatibility and interoperability to each optics and the necessity of test assured program. In order to achieve the full compatibility on Dell switches, we tested our different Dell compatible optics on various Dell switches, including Dell-Force10-S4810P, Dell S50-01-GE-48T-AC-SX, Dell S60-44T-AC-R-SX, DELL-N4032F, Dell PowerConnect 5324, FORCE TM S60-44T, DELL-Mellanox M3601Q, DELL ME-M3601Q 4OG, Dell PowerConnect 6224 and Dell PowerConnect 3448. The below figure shows our compatibility test of Dell SFP on Dell N4032F switch.

dell switch

Conclusion

This article mainly compared the transceiver module from original brand manufacturer and third-party network equipment vendors. We can definitely use third-party optical modules for optical networking equipment of major brands. How to choose a reliable supplier from so many third-party Dell compatible optics manufacturers? Before buying transceiver modules, the quality, compatibility, price, shipping, after-sales service should be considered. As one of well-known 3rd-party optics manufacturers, FS.com is suggested to be a good choice for Dell compatible optics.

Related article: FS.com SFP+ Optical Modules Solution How Many Types of SFP Transceivers Do You Know A Quick Overview of Cisco 1000BASE-T GLC-T SFP Copper Module

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k