What Is PicOS-V and How to Use It
What Is PicOS-V?
Looking for better software for your network switch? If you are used to using Cisco or Juniper CLI or Linux, Pica8 is a good choice.
Now, you have the opportunity to test Pica8's PicOS® switching software through PicOS-V.
PicOS-V is a free virtual machine (VM) provided by Pica8 designed to help users familiarize themselves with the PicOS® software switch. The VM is used to validate PicOS® configurations at no cost to the user. PicOS-V is able to run on VMware, VirtualBox, and the GNS3 hypervisor without the need for a bare-metal switch or dedicated hardware.
Available now, PicOS-V emulates the PicOS® software switch running in hardware with 48 10G ports and four 100G ports. You can test L2 and L3 functionality at your own pace and easily explore the powerful features of PicOS® without worrying about any associated costs.
PicOS-V Benefits
What advantages does PicOS-V offer you as a free virtual machine? Read on to find out:
-
No need to wait for switching hardware
-
Free and no license required
-
Get familiar with PicOS® Software Switches
-
Validate configuration of PicOS® switches
-
Prototype network operations before you commit
-
Test features without any risk – L2, L3 and upgrade
-
Test Automation with PicOS-V
-
Simulate open network switch hardware by simply changing models (and serial numbers)
What Is the Difference Between PicOS-V and PicOS®?
PicOS-V VM is the same PicOS® Network Operating System (NOS) software supported on open network switches and includes all the same software features, but in a VM format. Unlike PicOS®, PicOS-V is not intended to run on production switches or carry production data traffic.
PicOS-V provides full data plane functionality with Layer 2 and Layer 3 functionality, with no costs associated. Due to the specific implementation of the hardware, PicOS-V does not support some features. Hardware-centric features such as PoE are not supported. OpenFlow, CrossFlow, and EVPN are not supported in the current version, but will be supported in the next version.
So while you wait for the hardware, take Pica8's CLI for a test drive and see if it's right for your enterprise campus, data center, and distributed site use cases.
How to Test Out PicOS-V?
Setting up PicOS-V is a swift process. Once you import the virtual machine (VM) into the hypervisor, access the VM console to log into PicOS-V, and you'll be ready to take it for a spin.
Configure the Ethernet management port (eth0) by assigning a static IP address. Follow the steps outlined below:
admin@Xorplus> configure
Entering configuration mode.
There are no other users in configuration mode.
admin@Xorplus# set system management-ethernet eth0 ip-address IPv4 “192.168.42.112/24”
admin@Xorplus# set system management-ethernet eth0 ip-gateway IPv4 192.168.42.1
admin@Xorplus# set system hostname PicOS-V
admin@Xorplus# commit
Commit OK.
Save done.
admin@PicOS-V#
After configuring the Ethernet management interface on the console, you can effortlessly connect to the PicOS-V VM using SSH and start using its features. No extra software licenses are needed. It's a straightforward setup, allowing you to access and use all its functions right after the initial configuration.
How FS Can help
FS and Pica8 have entered into a strategic partnership. FS is now licensed to sell the full range of Pica8 products, including the PicOS® family, PicOS-V and AmpCon™ Network Manager.
You can experience PicOS-V online at FS, or sign up for a free trial. Try it now!
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023