English

5G Is Coming – the New Wireless Revolution to Change Our Life

Updated on Sep 24, 2018 by
4.2k

With the rapid development of the mobile communication industry, 5G has become a hot topic globally. Compared to 2G, 3G and 4G, the future of 5G network cannot be underestimated. 5G will be built upon the foundation created by 4G LTE to allow people to send texts, make calls, and browse the web. It will increase the speed at which data is transferred across the network. How will this new wireless revolution change our life and what can we do to prepare for the upcoming 5G network?

5G Network

What Is 5G Network and Why Is It an Urgent Necessity?

5G stands for the fifth generation of the next wireless mobile standard. The 5G New Radio (NR) specification was released by standards body 3GPP in late 2017, with the chips already being built '5G-ready'. The upgraded 5G performance targets include high data rate, lower latency, energy saving, cost reduction, higher system capacity and massive device connectivity.

Greater Speed: 5G vs 4G

How fast is 5G? It is estimated that the data transmitted over 5G wireless broadband connections could travel at rates as high as 20 Gbps. Unlike 4G, the 5G wireless signals will be transmitted via large numbers of small cell stations located in places like light poles or building roofs. Consequently, the demands for optical transceivers deployed in the 5G cell stations will greatly increase accordingly.

Lower Latency with Higher System Capacity

The 5G network will reduce latency significantly with faster load times. It is estimated to offer latency of 1 ms or lower for applications that require real-time feedback. It means that you’ll see very little delay or lag when you browse on your networking devices.

Network Type Latency (Milliseconds)
3G 120 ms (actual)
4G 45 ms (actual)
5G 1 ms (theoretical)

Thanks to the more available bandwidth and advanced antenna technology, the 5G network will enable a sharp increase in the amount of data transmitted over the wireless systems. Meanwhile, the expenses involved in 5G network will be reduced substantially.

Massive Device Connectivity

Another key goal of 5G is to dramatically improve the quality of service, and extend that quality over a broader geographic area. 5G network architectures are much more likely to be networks of small cell stations, even down to the size of home routers or data switches instead of huge towers radiating great distances. The more cell stations you have, the more devices you can connect into the network.

How Does 5G Work?

Due to the increase in the data transfer speed, the 5G deployment needs to upgrade the optical transport network it bears. Compared with the BBU and RRU two-level architecture of the 4G LTE access network, the 5G RAN will evolve into a three-level structure of CU (Centralized Unit), DU (Distribute Unit) and AAU (Active Antenna Unit). In terms of the application scenario, the 5G communication optical modules show 3 types: Front-haul, Middle-haul, and Back-haul transmission.

how does 5g work

In the Front-haul transmission, the 6G/10G optical transceivers used in 4G network can't meet the 5G network demand already. The upgraded 5G network requires optical transceivers that can support 25G high-speed interface with ultra-low latency and low power consumption. The auto-adaption feature in services, rates, and wavelengths is also demanded. Consequently, the low-cost 25G optical transceivers will play a big part in constructing the 5G network.

From the Middle-haul and Back-haul transmission perspective, the demand for networks with large capacity and scalability is already there, and the use of WDM would become very common. WDM systems based on silicon photonics coherent or incoherent 100G, 400G networks will become mainstream in the future. The DWDM system will spring up but it needs better versatility and manageability.

When Is 5G Coming and How Can We Prepare for 5G Network?

5G mobile connectivity is just around the corner. It just depends on process of the completion of mobile core standards by 3GPP and should arrive in late 2018. 5G cellular services will be rolled out in 2019, when the first 5G-enabled devices are expected to become commercially available.

when is 5g coming

No matter which kind of network implementation is hosted by 5G technology, the 5G communication optical module is ultimately indispensable. The cost-effective and high-rate optical transceivers which can support long-distance transmission are the most powerful backups to achieve a broad and low-cost 5G network coverage. The future development of 5G communication optical modules will be dominated by 25G optical modules and 100G optical modules. To pave the way for the upcoming 5G network, the first step is to scale the 25G tunable optical module industrialization, and then minimize 100G optical transceivers’ expenses, especially in long-haul transmissions. FS is striving to be the innovator in 5G communication optical transceivers manufacturing. We’re developing the diversified standard 5G communication optical modules including the 25G SFP28, 100G QSFP28, and DWDM transceivers to comply with the industrial standard of the 5G network.

Related Article: Will the Powerful 5G Wireless Abandon Fiber?

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
390.8k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
369.4k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
339.3k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
423.1k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
298.6k