English

Can PoE Switch Be Used with Non-PoE Switch?

Updated on Mar 24, 2023 by
59.8k

A PoE switch is a regular network switch that has Power over Ethernet functionality integrated. It allows compatible devices, such as VoIP phones, network surveillance cameras or wireless access points to work in places where power outlets or network connections don't exist. But many people still wonder: Can PoE switches be used with non-PoE switches? Can they be connected to non-PoE devices? Here are the answers.

 

Can PoE Switch Be Connected to a Non-PoE Switch?

PoE and non-PoE switches are both network switches, is there any difference between them? Compared to a PoE switch, a non-PoE switch is surely cheaper, but it can't provide any power to any devices. But the PoE switch is not an independent entity in the entire network. It can access the aggregation switch at the upper end and the distributed switch at the lower end. General PoE switches have a port called uplink port, which is interconnected with ordinary switches, so, there is no problem of being unable to connect to other non-PoE switches.

PoE switch connects to Non-PoE switch

Can PoE Switch Pass Through Non-PoE Switch?

For those who have both PoE and non-PoE switches, they may wonder whether the PoE switch can supply power to the device through the non-PoE switch? The answer is NO!

PoE will only be provided to devices directly connected to the PoE switch, and only on request. PoE doesn't carry through additional switches, the last switch before the device has to be the PoE switch.

If you have a PoE switch and want to pass PoE to client devices, you should not use non-PoE switches in between, because most PoE switches will not turn on the power to ports that are connected to non-PoE client devices at all, and some older non-PoE switches not only fail to pass power, but they may make matters worse by shorting unused pairs 1 and 4 (connecting them to the ground). So, if you want a non-PoE switch to "power" other PoE devices, all you need is a PoE injector.

PoE Switch and Non-PoE switch connecting to PoE device

Can PoE Switch Be Used with Non-PoE Devices?

PoE switches are great, but can I still use them with other non-PoE devices? What happens if I plug a non-PoE device into a PoE switch? Here are the answers.

PoE switches that comply with the standard PoE(we also call it active PoE switch), has a detection and identification function before power supply. When the device is connected, the PoE switch will send a signal to the network to detect whether the IP terminal in the network has a powered device that supports PoE. If it does, the PoE switch will only supply power to it, if it does not support PoE switches, it will not supply power. So, you can plug a non-PoE device into a PoE switch. It will only transmit data. Don't worry if it will burn up your devices.

However, not all PoE switches are standard PoE switches. You have to verify the type of PoE, to figure out whether it’s active or passive. The one to be wary of is the passive PoE. Passive PoE switches do not adhere to any IEEE standard, which means it always sends electric current out over the Ethernet cable at a certain voltage regardless of whether the terminal device supports PoE or not. So using passive PoE switches may burn out the terminal non-PoE devices.

Note: Any PoE switch that shows support for IEEE standards 802.3af (15.4W max), 802.3at (30W max), and 802.3bt (60W or 100W) is active. Generally speaking, most modern switches support active, but you better check the specs.

Can PoE and Non-PoE Devices Be Used with PoE Switches Simultaneously?

The PoE switch can automatically identify the terminal device that needs power, whether it is a PoE device or a non-PoE device. Therefore, PoE does not interfere with normal switch operation. PoE and non-PoE devices can be mixed on the same switch at the same time. There is no problem at all. In addition, many PoE switches can automatically disable the PoE port of the signal for ports that do not need it, making them more power-efficient.

PoE Switch connecting to PoE devices

Can I Use a PoE Switch as a Normal Switch?

Yes, a PoE switch can also function as a normal switch. For instance, just like a regular switch, a PoE switch can transfer data over an Ethernet cable. PoE switches can also transfer power, unlike normal ones. So, if you want to use a PoE switch as a normal switch, all you have to do is turn off the power button. It should then be able to function as a regular switch.

Can I Use a PoE Port for a Non-PoE device?

Likewise, the answer is yes. PoE switches have auto-sensing PoE ports. This means that the PoE port will detect if the connected device is a PoE device or not. But you have to check if the PoE device is 802.3af or 802.3at compliant to make sure that it is compatible with the PoE switch. In addition, you can also choose to disable the PoE capability per port on the PoE switch.

Conclusion

In summary, the PoE switch is not totally different from the non-PoE one. It can be connected to either a non-PoE switch or a non-PoE device. You just have to make sure that your PoE switch is rated to be IEEE 802.3af, IEEE 802.3at or IEEE 802.3bt compliant.

You might be interested in

Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
387.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
368.0k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
336.4k
Knowledge
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
421.1k