English

Unlocking the Secrets of PoE Switches — A Complete Guide

Updated on Mar 16, 2023 by
102.8k

Power over Ethernet (PoE) switches have become a popular solution for businesses looking to provide power and data to devices over a single connection. In this complete guide, we will explain different types of PoE switches, their benefits and applications, and discuss how to select the right PoE switch for your needs.

What is a PoE Switch?

A PoE switch is a device that combines the functionality of a switch and a power source in one. It has multiple Ethernet ports that can be used to connect other devices, such as VoIP phones, wireless access points, and IP cameras. The switch is responsible for providing power to the connected devices, eliminating the need for separate power cables. PoE network switches are often used in network deployments where power outlets are scarce or when the devices are located in hard-to-reach places.

The technology behind PoE switches is known as power over ethernet (PoE). PoE is a technology that enables the transmission of both data and electrical power over Ethernet cables. It uses a combination of a power source and power injectors to send power to connected devices. Power injectors act as a bridge between the power source and the connected devices, and they are responsible for the transmission of both data and power. Also Check- PoE switch

 

PoE Switch

Types of PoE Switches

When choosing a PoE switch, it is important to understand the different types of PoE network switches available. There are two main types of PoE network switches.

The Unmanaged PoE Switch

An unmanaged PoE switch is a straightforward, plug-and-play solution tailored for smaller setups. It's user-friendly and uncomplicated in configuration. However, it lacks customization, management features, and security options, making it best suited for applications with minimal network complexity, such as home networks or small-scale environments with fewer than 5-10 computers.

The Managed PoE Switch

Managed PoE switches, offering advanced features, excel in scenarios that demand precise network management. With heightened control and robust security, they are ideal for applications like enterprise networks, data centers, and large-scale surveillance systems, which require complex features such as VLANs, QoS, port mirroring, and enhanced port security.

Benefits of PoE Switches

Given how PoE switches work, the benefits of PoE switches are obvious.

Simplicity: PoE network switches are also easy to install and configure. Most PoE network switches are plug-and-play devices, so there is no need for complicated wiring or configuration. The switches also come with built-in features such as port mirroring, VLANs, and QoS, which can help to streamline network management.

Cost-Efficiency: Another benefit of PoE switches is their energy efficiency. PoE network switches can be configured to provide the necessary power for each connected device, eliminating the need for an oversized power supply. This helps to reduce energy costs and can result in long-term savings.

Flexibility: Devices powered by PoE are simple to move to areas without power outlets. Thus, PoE switches can be placed in places that are difficult to reach or less close to a power source. Security cameras are one example of this, as power outlets are rarely found above ceilings.

Future application: The Internet of Things (IoT) industry is booming. When PoE switches are incorporated into your network infrastructure, it is guaranteed that it will be able to accommodate the increasing number of devices designed to make use of this technology.

PoE Switch Applications

This rapid expansion of network-connected devices means that PoE technology and PoE switches will grow in importance to most networking infrastructures. While PoE switches have numerous applications, we mainly discuss the three most common application scenarios.

  • VoIP Phones: VoIP phones are PoE devices, with PoE allowing for a single connection to the wall socket and the ability for remote powering down

  • IP Cameras: Security cameras can be connected to PoE switches to enable fast deployment and simple repositioning.

  • Wireless: Many wireless access points are PoE compatible. Thus, PoE switches allow for easy relocation and remote positioning.

  • Smart Home Automation: LED lighting, heating and cooling systems, appliances, voice assistants, and electric car charging stations.

How to Select the Right PoE Switch

When selecting a PoE switch, it is important to consider your application requirements, the features and limitations of the PoE network switch. Of course, the power requirements of connected devices are also important. Some PoE network switches are designed to power devices that require up to 30 watts, and some are even designed for power devices that require up to 60 watts.

Features of PoE Switches to Consider

In addition to the type of switch and power requirements, there are a number of features to consider when selecting a PoE switch. These features include port speed, port count, port types, PoE budget, power savings, and port security.

  • Port speed: Maximum speed a port can achieve. It is important to choose a switch with a port speed that can support the connected devices. The port count is the number of ports available on the switch. It is important to choose a switch with enough ports to accommodate all of the connected devices.

  • Port type: Common port types include RJ45, SFP, and SFP+. It is important to choose a switch with the right port type for connected devices.

  • PoE budget: Maximum amount of power that can be allocated to connected devices. It is important to choose a switch with a PoE budget that can accommodate all of the connected devices.

  • Power savings: Designed to conserve energy by automatically turning off unused ports. This can help to reduce energy costs. You can read the article "Eco-Friendly Networking: Green Enterprise Switch Technologies" to learn more.

  • Port security: Designed to protect connected devices from unauthorized access.

Limitations of PoE Switches

Nonetheless, there are some limitations to PoE variation that you should be aware of:

  • Restrictions on distance: Typically, PoE switches can transmit over Ethernet up to a distance of up to 100 meters. The 100-meter distance restriction presents a challenge for large campuses, restaurants, and businesses implementing PoE. However, there are still devices like power extenders and powered fiber cables that can be used to extend the PoE range.

  • Power: If you require high power over poe networks, you must ensure that the power capacity of your PoE switches meets your requirements due to the power limitation imposed by PoE standards and Wattage.

Also Check- Powered Fiber Cables: Solution for Extending POE

 

FAQs about PoE Switch

Q: Non-PoE vs. PoE Switch: How do they differ?

A: Non-PoE switches cannot deliver power to connected devices, necessitating the use of midspan power sourcing equipment (PSE), such as a PoE injector. This setup adds power while transmitting data to powered devices (PDs). In contrast, PoE switches offer a simpler solution, directly delivering power and data to PDs with just a network cable and a power cable.poe vs. non-poe Also Check- PoE vs PoE+ vs PoE++ Switch: How to Choose?

 

Q: Do PoE Switches Require Special Cables?

A: No. The Ethernet cables that should be used for PoE network switches primarily depend on the data rate of the PoE port; for instance, Cat3 or better cables can be used for 10/100M; Cat5/Cat5e/Cat6 cables are required for 1000M. In the future, Cat6a or higher cables may be required for the installation of 2.5G/5G/10G PoE devices.

Also Check- Ethernet cables

 

Q: Active vs Passive PoE Switch: Should I Choose Active or Passive PoE Switches?

A: Active PoE network switch complies with standard PoE. On the contrary, passive PoE network switch does not adhere to any IEEE standard. There are many ways that active and passive PoE switches differ from one another, like how the PoE power supply pinout looks and whether or not they support Ethernet.

 Also Check- Active vs. Passive PoE Switch: Which Should We Choose?

 

Q: Can the PoE Switch be used with a computer or other non-PoE devices? And will a PoE switch harm devices that do not use PoE?

A: Yes, a PoE switch can be used with non-PoE devices like computers. The switch automatically detects whether a connected device is PoE-compatible and will only supply power to PoE-enabled devices. So, it won't harm non-PoE devices; they just won't receive power through the switch.

Also Check- Can PoE Switch Be Used with Non-PoE Switch/Devices?

 

Q: Is it possible to connect two PoE switches?

A: You could, yes. The PSE only supplies PD with power when it determines that the device can handle it. As PSEs, the two PoE switches will only be used for data communications.

 

Q: What is the maximum transmission distance of PoE? How to extend the transmission distance of PoE?

A: Whether using IEEE 802.3af (PoE) or 802.3at (PoE+), data and power transmission are limited to a distance of 100 meters over Ethernet cables in standard PoE. Media converters and PoE extenders, for example, can extend the range to up to 300 meters if you want to increase the maximum distance.

Conclusion

PoE switches are an effective solution for businesses looking to provide power and data over a single connection. They can simplify installation, reduce clutter, and improve energy efficiency. When selecting a PoE network switch, it is important to consider your application requirements, the power requirements of the connected devices, and the features of the switch. It is also important to consider the cost and long-term cost savings of using a PoE network switch.

If you are looking for a reliable and cost-effective PoE switch, check out FS PoE Switches.

You might be interested in

Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
419.7k
Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
384.6k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
366.9k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
334.1k
Knowledge