English

Data Center Switch Wiki and Buying Guide

Updated on Jun 16, 2022 by
23.8k

FS data center switch

The data center switches are emerging as a new class of switch since data center networking infrastructures have become more disaggregated. Unlike the network switch for traditional three-tier hierarchical networks, data center class switches are designed to support data and storage for mission critical applications. Now with various data center switches and vendors in the market, buying a good one can be a difficult task. Here will help you learn what a data center switch is, the requirements for data center switches, as well as some useful buying tips.

 

What Is a Data Center Switch?

Generally speaking, the data center switch is a high performance switch mainly for large enterprises and cloud providers who rely heavily on virtualization. It can be deployed throughout the data center, or to anchor a two-tier (spine-leaf) or one-tier flat mesh or fabric architecture. Data center switches share some common features as follows:

  • They can handle both north-south and east-west traffic flows;

  • All data center switches are used both in top-of-rack (ToR) and end-of-row (EoR) architecture;

  • They support high-bandwidth interconnections using both standard LAN Ethernet protocol and SAN protocols. For example, Fibre Channel and Fibre Channel over Ethernet;

  • All components of a distributed data center switch can be managed from a single management interface for ease of use.

 

Things To Consider When Buying Data Center Switches

Choosing a data center switch can be a difficult task, no matter if you are deploying a new data center or deciding to upgrade the existing network infrastructure. There are many factors to consider and here lists some of the most important ones in several aspects.

Functions

All switches have the same basic functionality, such as using standards-based protocols or maintaining a MAC address-to-port table. Based on their use cases and applications, different switches have unique characteristics. You should ask yourself a few questions to decide what functions are needed. Are you going to use enterprise-level applications? Are you considering redundancy? Do you have a virtualized infrastructure? For example, a reliable data center switch should have the capability to automate as well as support newer protocols such as EVPN and VXLAN. And some data center switches support Ansible/OpenFlow configuration and automation tools for easy management.

Size, Number of Ports, and Data Rate

Data center switches come in varying sizes. Choosing the right size for your business will depend on the current and future data flow. A large switch requires more resources to install and will serve your current and future needs. A smaller switch is economical, but you'll have to install it in a top-of-rack manner to prevent bottlenecks.

The size of the fiber connections that you'll need should also be well considered. It's advisable to make up your mind early enough on the connectivity that you will be using. Fiber connectivity varies from 10 Gbps, 25 Gbps to 40 Gbps, and even more. Nowadays the adoption of 100Gps has gained momentum in most data centers and some hyperscale data centers are moving towards higher speed 400Gbps, which paves the way for the development of 400G data center switches.

Data center switches also have varying port types and numbers, based on which specific cabling and transceivers are selected, so you should know what you need now and make a reasonable estimate of what you'll need in the future.

Hardware and Software

With cloud data centers growing and the trends of virtualization and new applications showing up these years, new data center switch types are coming to the market, such as white box switches and bare metal switches, of which the OS is open. As for data centers where large amounts of traffic are required to handle all the time, the white box switches or bare metal ones give network engineers an alternative choice other than brand-name switches, which brings both offering flexibility as well as low costs. Meanwhile, for data centers to upgrade, it is important to make clear what brands of switches, and what OSs are currently used on the network.

Data Center Architecture and Configuration

Modern data centers use spine-leaf architecture and the switches located at each layer have their own requirements. Generally, spine switches are supposed to handle more traffic with higher capacity and better performance than leaf switches. For more details about data center leaf and spine switches buying tips, please refer to How to Choose Data Center Spine and Leaf Switches?

Whether to use ToR or EoR configuration determines what types of data center switches you will need. If you already have an end-of-row network cabling in place, it’s better to make use of the existing wiring and deploy larger capacity data center EoR switches. If you plan to build a new data center or new cabling, Using ToR data center switches for the ToR network is a better idea, for they will offer more flexibility in terms of physical port coverage across the data center.

Switch Vendor

After considering all of these vital factors above, you've got a sense of what should you keep in mind. But remember, the data center switch’s performance, price, and support service vary from one vendor to the other, so please check out your vendor list and make sure you'll work well with the selected vendor.

Go through the user testimonials and reviews to find one with a good reputation. Evaluate them by their services, i.e., software advancements and configurations, hardware spare and replacements, and troubleshooting support. You may consider buying the switches from different vendors as the SDN is emerging. However, unless you use a truly open SDN platform, buying from a single vendor is a wise choice for it is future-proofing. We should select a data center switch vendor that offers the most premium features and services at the most competitive price.

Cooling and Airflow

Before buying a switch, you should know that the way you install and connect the switches will affect the quality of airflow and cooling. If the cables block the airflow, that could mean a reduced lifetime due to overheating, which could cause premature failure.

Similarly, the airflow direction of the switches influences the data center cooling. For instance, if the connections are located in the front of the servers, you should choose front-to-back cooling. However, if the connections are located on the back of the servers, you should go for back-to-front cooling.

A small disruption for a couple of hours or days may not cause serious harm inside the data center. However, a design problem that's overlooked for months and even years could mean frequent downtimes and even costly repairs and upgrades.

There are other considerations that are also important, and making good use of these points can make your network stronger.

  • Redundancy: You should consider the level of redundancy that you need for your data center switches. You need to ensure that your switches have redundant power supplies, fans, and other critical components.

  • Management: You need to consider the management capabilities of your switches. You should choose switches that have a robust management interface that allows you to monitor and manage your network effectively.

  • Security: You should consider the security features of your switches. You need to ensure that your switches have advanced security features that can protect your network from cyber threats.

Picking the Right Data Center Switch

Now that you know what factors to consider in choosing a data center switch, what's left is to narrow down your options to find the type you want. When picking a data center switch from the flooded market, a rule of thumb is to seek professional advice, i.e., if you aren't an expert in the field. Where possible, have one of your IT guys around. A professional will better understand some technical terms such as buffer size, latency, and even port speeds, helping you avoid confusion so you can pick the right product.

As a leading provider of optical communication solutions, FS has a variety of data center switches, such as N8560 series switches or 400G modular switches. If you order an FS data center switch, you will also enjoy full-process services and a 5-year warranty to ensure your network reliability.

You might be interested in

Blog
See profile for Howard.
Howard
FAQs about FS.COM 100G Switches
May 28, 2022
10.0k
Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
390.7k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
369.4k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
339.3k
Knowledge