English

How to Choose Data Center Spine and Leaf Switches?

Updated on Jun 11, 2022 by
7.7k

25G Switch

The development of leaf-spine architecture not only solves the problems of the rapid growth of traffic in the data center and the continuous expansion of the scale of the data center but also meets the needs of high-speed interconnection within the data center. This network architecture requires the configuration of corresponding data center switches, and how should spine and leaf switches be selected and configured to function fully? This article will tell you the answer.

Why Do You Need Spine-leaf Architecture?

Spine-leaf architecture can provide predictability of network latency. In leaf-spine architecture, you always know how many docks each packet goes through. Correspondingly, the traffic and distance that these packets must cover are also consistent, reducing network latency between leaf switches. Apart from that, the leaf-spine architecture with deleting the STP protocol supports layer 3 routing to achieve a more stable network environment.

Leaf-spine network architecture greatly improves network efficiency, especially in high-performance data centers or high-density bandwidth cloud networks. When the link traffic is too large, additional spine switches and leaf switches can be added, or VXLAN technology to achieve more comprehensive traffic coverage and load balancing. The leaf-spine architecture not only solves the transmission bottleneck of horizontal network connections but also exhibits its high scalability and can be adapted to almost all large, medium, and small data centers.

What Are Spine and Leaf Switches?

Spine and leaf switches are the two main components of the leaf-spine architecture in data center. Spine switches can be regarded as core switches in a leaf-spine network architecture. But the difference is that the 100G switches with high port density are sufficient for spine switches. Leaf switches are equivalent to access layer switches. Leaf switches provide network connections to endpoints, servers, and upwards to spine switches.

What Is Spine Switch

Spine switches can handle layer 3 network traffic with high port density for scalability. Each of its L3 ports is dedicated to connecting to an L2 leaf switch and cannot connect or find any servers, access points, or firewalls. Therefore, the number of ports available on the spine switch determines the number of switches at the spine and leaf layers, which in turn determines the maximum number of servers that can be connected to the network.

In a high-density data center network, evenly distributing the uplink connections of leaf switches between the boards of the spine switches and reducing traffic by cross modules can significantly improve the performance of spine switches. Of course, data center spine switches generally need to have a large cache, high capacity, and virtualized performance. They usually need to be equipped with 10G/25G/40G/100G ports and a complete software system, complete protocols, and application functions, such as EVPN-VXLAN, stacking, MLAG, etc., to facilitate rapid network deployment.

What Is Leaf Switch

Leaf switches are commonly used devices in data centers, mainly to control traffic between servers, and forward layer 2 and layer 3 traffic. The number of uplink ports of a leaf switch restricts the number of spine switches it is connected to, and the number of downlink ports determines the number of devices connected to the leaf switch. Generally, the uplink ports support the speed of 40G/100G, while the downlink ports can vary from 10G/25G/40G/50G/100G depending on the model you plan to use.

As server devices continue to grow, it is necessary to select leaf switches that support larger rates and more ports. To prevent link traffic congestion, leaf switches should have an oversubscription ratio of less than 3:1 for uplink and downlink port bandwidth, or apply virtualization technologies to balance link traffic. For related virtualization technologies, like spine switches, they can also add VXLAN, PFC, stacking, or MLAG technologies, and support both IPv4 and IPv6 for better network management and expansion.

spine-leaf 4

Spine and Leaf Switches Recommendation

Based on the advantages that leaf-spine architecture brings to the network environment, spine and leaf switches emerge one after another. It is critical to choose the right spine and leaf switches based on individual business needs. For example, the FS data center spine switches are available in 1U and 2U form factors, equipped with comprehensive performance and virtualization technologies to achieve low latency, zero packet loss, high throughput, and service forwarding rates to meet the growing demands of data center environments. These features include industry-leading chips, redundant hot-swappable power supplies, fans, VXLAN, MLAG (VAP), PFC, ECN, and more. At the same time, FS data center spine switches also have ports with different rates, and you can choose the number of ports and bandwidth rates according to business needs.

Products N8560-32C N8550-32C N8560-64C NC8200-4TD
Ports 32x 100G QSFP28 32x 100G QSFP28, 2x 10Gb SFP+ 64x 100G QSFP28 128x 10G/25G, 64x 40G, or 32x 100G
CPU Intel® Xeon D-1527 (Quad-core, 2.2 GHz) Intel® Xeon® D-1518 processor quad-core 2.2 GHz Cavium CN7230 (Quad-core, 1.5 GHz) /
Switch Chip BCM56870 Broadcom BCM56870 Trident III BCM56970 BCM56870
Switching Capacity 6.4 Tbps 6.4 Tbps full duplex 12.8 Tbps 6.4 Tbps
Forwarding Rate 4.76 Bpps 4.7 Bpps 9.52 Bpps 4.76 Bpps
Number of VLANs 4K 4K 4K 4K
Memory SDRAM 8GB DRAM 2x 8 GB SO-DIMM DDR4 SDRAM 4GB SDRAM 4GB
Flash Memory 240GB 2x 16MB 8GB 8GB

FS data center leaf switches provide high-performance switches with 10G/25G/40G/100G/400G ports to meet the diverse requirements for the number of uplink ports and downlink ports. Like spine switches, they also apply related virtualization technologies to meet the increasing data demand, fully realizing zero packet loss, low latency, and non-blocking lossless Ethernet, ensuring your network reliability. They feature the software technologies of layer 3 IPv4 and IPv6 routing protocols, VXLAN, MLAG, etc. FS N8550 and N5850 series switches are tested to apply in most network operating systems, such as SONiC, IP Infusion OcNOS™, Pica8 Inc. PicOS®™, etc. They are suitable for small and medium data centers and large and medium campus network design.

Products N5860-48SC N8560-48BC N8550-48B8C N5850-48S6Q NC8200-4TD NC8400-4TH
Ports 48x 10G SFP+| 8x 100G QSFP28 48x 25G SFP28| 8x 100G QSFP28 48x 25G SFP28, 2x 10Gb SFP+, 8x 100G QSFP28 48x 10G SFP+, 6x 40G QSFP+ 128x 10G/25G, 64x 40G, or 32x 100G 32x 100G, or 16x 100G, 4x 400G
CPU Cavium CN7130 (Quad-core, 1.2 GHz) Cavium CN7130 (Quad-core, 1.2 GHz) Intel® Xeon® D-1518 processor quad-core 2.2 GHz Intel Atom C2538 processor quad-core 2.4GHz / /
Switch Chip BCM56770 BCM56873 Broadcom BCM56873 Trident III Broadcom BCM56864 Trident II+ BCM56870 BCM56980
Switching Capacity 2.56 Tbps 4 Tbps 4 Tbps full duplex 1.44 Tbps full duplex 6.4 Tbps 25.6 Tbps
Forwarding Rate 1.90 Bpps 2.98 Bpps 2.9 Bpps 1 Bpps 4.76 Bpps 1.905 Bpps
Number of VLANs 4K 4K 4K 4K 4K 4K
Memory SDRAM 4GB SDRAM 4GB DRAM 2x 8 GB SO-DIMM DDR4 DRAM 8GB SO-DIMM DDR3 RAM with ECC SDRAM 4GB SDRAM 8GB
Flash Memory 8GB 8GB 2x 16MB 16MB 8GB 64GB
System FSOS FSOS / / FSOS FSOS

Summary

High-density networks in data centers require higher-performance switches that also support network scalability. Leaf-spine architecture can achieve low network latency and scalability through east-west traffic monitoring and prediction, while FS data center switches provide complete protocol functions and virtualization application technology, which exactly fit the advantages that spine-leaf switches should have and show.

You might be interested in

Knowledge
Knowledge
Knowledge
Blog
See profile for Howard.
Howard
FAQs About FS Data Center Switches
May 31, 2022
3.6k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
387.0k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.9k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
336.2k
Knowledge