English

FBT Splitter vs. PLC Splitter: What Are the Differences?

Updated on Mar 26, 2024 by
25.5k

Fiber optic splitter is a passive optical device that can split or separate an incident light beam into two or more light beams. Basically, there are two types of optical fiber splitter classified by their working principle: FBT splitter (fused biconical taper splitter) and PLC splitter (planar lightwave circuit splitter). There are lots of differences between FBT splitter and PLC splitter, which is confusing for many users. This tutorial will walk you through the main ones between them.

What Is PLC Splitter?

PLC splitter is based on planar lightwave circuit technology. It comprises three layers: a substrate, a waveguide, and a lid. The waveguide plays a key role in the splitting process which allows for passing specific percentages of light. So the signal can be split equally. In addition, PLC splitters are available in a variety of split ratios, including 1:4, 1:8, 1:16, 1:32, 1:64, etc. They also have several types, such as bare PLC splitter, blockless PLC splitter, fanout PLC splitter, mini plug-in type PLC splitter, etc. You also can check the article How Much Do You Know About PLC Splitter? for more information about PLC splitter. The following table shows the advantages and disadvantages of PLC splitter.

Advantages Disadvantages
  • Suitable for multiple operating wavelengths (1260nm - 1650nm).

  • Equal splitter ratios for all branches.

  • Compact configuration, smaller size, small occupation space.

  • Good stability across all ratios.

  • High quality, low failure rate.

  • Complicated production process.

  • Costlier than the FBT splitter in the smaller ratios.

What Is FBT Splitter?

FBT splitter is based on traditional technology, involving the fusion of several fibers from the side of each fiber. The fibers are aligned by heating them at a specific location and length. Due to the fragility of the fused fibers, they are protected by a glass tube made of epoxy and silica powder. Subsequently, a stainless steel tube covers the inner glass tube and is sealed with silicon. As technology continues to develop, the quality of FBT splitters has significantly improved, making them a cost-effective solution. The following table outlines the advantages and disadvantages of FBT splitters

Advantages Disadvantages
  • FBT splitter is made out of materials that are easily available and low-price, so it is cheaper.

  • Splitter ratios can be customized.

  • Restricted to its operating wavelength (850nm, 1310nm, and 1550nm).

  • The maximum insertion loss will vary depending on the split and increase substantially for those splits over 1:8.

  • Because an exact equal ratio cannot be ensured, the transmission distance can be affected.

  • High Temperature Dependent Loss (TDL).

  • Susceptible to failure due to extreme temperatures or improper handling.

FBT Splitter vs PLC Splitter: What Are the Differences?

1. Operating Wavelength

FBT splitter only supports three wavelengths: 850nm, 1310nm, and 1550nm, which makes its inability to work on other wavelengths. The PLC splitter can support wavelengths from 1260 to 1650nm. The adjustable range of wavelength makes PLC splitter suitable for more applications.

 

FBT vs PLC splitter, Operating Wavelength

Figure1: Operating Wavelength Comparision

2. Splitting Ratio

Splitting ratio is decided by the inputs and outputs of an optical cable splitter. The maximum split ratio of FBT splitter is up to 1:32, which means one or two inputs can be split into an output maximum of 32 fibers at a time. However, the split ratio of PLC splitter is up to 1:64 - one or two inputs with an output maximum of 64 fibers. Besides, FBT splitter is customizable, and the special types are 1:3, 1:7, 1:11, etc. But PLC splitter is non-customizable, and it has only standard versions like 1:2, 1:4, 1:8, 1:16, 1:32, and so on.

 

FBT vs PLC splitter, Splitting Ratio

Figure2: Splitting Ratio Comparision

3. Splitting Uniformity

The signal processed by FBT splitters cannot be split evenly due to a lack of management of the signals, so its transmission distance can be affected. However, PLC splitter can support equal splitter ratios for all branches, which can ensure a more stable optical transmission.

 

FBT vs PLC splitter, Asymmetric Attenuation Per Branch

Figure3: Splitting Uniformity Comparision

4. Failure Rate

FBT splitter is typically used for networks requiring the splitter configuration of less than 4 splits. The larger the split, the greater the failure rate. When its splitting ratio is larger than 1:8, more errors will occur and cause a higher failure rate. Thus, FBT splitter is more restricted to the number of splits in one coupling. But the failure rate of PLC splitter is much smaller.

 

FBT vs PLC splitter, Failure Rate

Figure4: Failure Rate Comparision

5. Temperature-Dependent Loss

In certain areas, the temperature can be a crucial factor that affects the insertion loss of optical components. FBT splitter can work stable under the temperature of -5 to 75℃. PLC splitter can work at a wider temperature range of -40 to 85 ℃, providing relatively good performance in the areas of extreme climate.

6. Price

Owing to the complicated manufacturing technology of PLC splitter, its cost is generally higher than the FBT splitter. If your application is simple and short of funds, FBT splitter can provides a cost-effective solution. Nevertheless, the price gap between the two splitter types is narrowing as the demand for PLC splitters continues to rise.

7. Size

FBT splitters typically have a larger and bulkier design compared to PLC splitters. They demand more space and are better suited for applications where size is not a limiting factor. PLC splitters boast a compact form factor, making them easily integrable into small packages. They excel in applications with limited space, including inside patch panels or optical network terminals.

Conclusion

Although the outer appearance and size of FBT and PLC fiber splitter seem rather similar, their internal technologies and specifications differ in various ways. Over the past few years, splitter technology has made a huge step forward in the past few years by introducing PLC splitter. It has proven itself as a higher reliable type of device compared to the traditional FBT splitter. If high split counts, small package size, and low insertion loss are required, you are suggested to choose PLC splitter rather than FBT splitter.

You might be interested in

Knowledge
See profile for John.
John
What Is an Optical Splitter?
Mar 15, 2023
102.0k
Knowledge
See profile for John.
John
How Much Do You Know About PLC Splitter?
Mar 26, 2024
33.8k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
387.0k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.9k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
336.2k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
421.0k