English

User Guide for FS S3800-24T4S 24-Port Stackable Managed Switch

Updated on Jan 11, 2022 by
3.5k

Note: FS has discontinued S3800 series switch. As per our policy, customers will continue to get support from FS technical assistance team, and the valid warranty provided is maintained on the product. For customers who are interested in FS S3800 series switch, you can choose S3900 series switches.

 

FS S3800-24T4S is a 24-port stackable managed switch that provides high-density performance by its Layer2+ Gigabit static routing with 10GbE uplinks. The administrator can flexibly choose the suitable SFP/SFP+ transceiver according to the transmission speed or the transmission distance required to extend the network efficiently. With 128Gbps switching fabric and stacking feature, FS S3800-24T4S 24-port switch can handle extremely large amounts of data in a secure topology linking to backbone or high capacity servers for ISP and enterprise networks. Here is a comprehensive user guide for FS S3800-24T4S 24-port Gigabit stackable managed switch.

FS S3800-24T4S 24 Port Switch

Figure 1: FS S3800-24T4S 24-Port Stackable Switch

Highlights of FS S3800-24T4S Switch

As a high-performance network switch for enterprise networks, FS S3800-24T4S 24-port switch enables users to directly connect to a high-performance storage server or deploy a long-distance uplink to another switch. With the outstanding features listed below, you can build and expand networks easily, scalably and efficiently.

Carrier-Class Design

FS S3800-24T4S 24-port switch is a carrier-grade Ethernet access switch ideal for Ethernet service demarcation, extension, and aggregation. It consists of 24 10/100/1000BASE-T ports and 4 10GbE SFP+ ports. Any of the port combination forms can be flexibly assigned as 10GbE fiber or 10/100/1000BASE-T copper connections to subscriber-side devices. All in all, FS S3800-24T4S 24-port stackable managed switch is ideal for locating at the edge of broadband-access networks to aggregate traffic from multiple services.

IP Stacking With Layer2+ Routing Support

FS S3800-24T4S 24-port switch can not only function as a standalone switch but also support IP stacking to help network managers easily configure up to 4 of the same model via one single IP address instead of setting each unit one by one. For efficient management, FS S3800-24T4S 24-port Gigabit stackable managed switch is equipped with console, Web and SNMP (Simple Network Management Protocol) management interfaces. With the built-in Web-based management interface, FS S3800-24T4S 24-port switch offers an easy-to-use, platform-independent management and configuration facility. FS S3800-24T4S stackable switch supports Lay2+ switch class and 4K VLAN entries. Therefore, it is suitable for IP MAN convergence layer and large-scale enterprise zone as well as the core of the network layer.

Excellent and Secure Traffic Control

FS S3800-24T4S 24-port switch is loaded with powerful traffic management and WRR (Weighted Round Robin) features to protect and enhance the transmission of multimedia services. The WRR functions include wire-speed Layer2+ traffic classifiers and bandwidth limitation which are particularly useful for multi-tenant unit, multi-business unit or network service applications. The ACL (Access Control List) flow filtration supported by this switch can classify the traffic by source/destination IP addresses, source/destination MAC addresses, IP protocols, IP precedence, time ranges and ToS. FS S3800-24T4S 24-port switch also provides IEEE 802.1x port based access authentication which can be deployed with RADIUS, thus ensuring the port level security and block illegal users.

How to Stack Multiple FS S3800-24T4S Switches

As mentioned above, FS S3800-24T4S 24-port stackable managed switch offers edge to core stacking to help you build and expand networks easily. By using 4 10GbE SFP+ ports, FS S3800-24T4S 24-port switch comes with true stacking capability, allowing you to configure, manage and troubleshoot multiple physical switches as a single unit. The following part will demonstrate the stacking procedures for two, three and four of FS S3800-24T4S switches respectively.

Two S3800-24T4S 24-Port Switches Stacking

Stacking two FS S3800-24T4S switches is very simple. As shown in Figure 2, you just need to use two 10G SFP+ direct attach cables to insert into two 10G SFP+ slots on each switch. Then the two switches are stacked successfully and you can manage either of them via the console port.

Stacking Two S3800-24T4S 24 Port Switches

Figure 2: Stacking Two S3800-24T4S Switches

Three S3800-24T4S 24-Port Switches Stacking

Stacking three FS S3800-24T4S switches is more complex. As shown in Figure 3, in this stacking system, each 10G SFP+ port on the four switches is used as an uplink port to connected to the SFP+ port on the other switch with 10G SFP+ to SFP+ direct attach cables. This process is repeated until three models are linked together. And the first stackable switch is connected with the last one to complete the stacking topology. Every time you stack a switch in this process, certain configuration changes are applied across the whole stack. You can manage each of these three switches from the console port, or make some changes to any of the switches in the stack.

Stacking Three S3800-24T4S 24-Port Switch

Figure 3: Stacking Three S3800-24T4S Switches

Four S3800-24T4S 24-Port Switches Stacking

Stacking four FS S3800-24T4S switches is the same case with stacking three of them. As shown in Figure 4, you only need to add one more switch and two more SFP+ to SFP+ direct attach cables to complete the whole stacking topology. But remember that each time you add a switch, certain configuration changes will be made. After four of the switch models are stacked together, the port density of the stacking system is the sum of the combined switches, namely 96 Gigabit RJ45 ports and 16 10G SFP+ ports per physical stack. Thus it provides up to 512Gbps total switching capacity for the network.

Stacking Four S3800-24T4S 24 Port Switches

Figure 4: Stacking Four S3800-24T4S Switches

FAQs About FS S3800-24T4S 24-Port Switches

Here we list some frequently asked questions about FS S3800-24T4S 24-port stackable managed switch in order to get a better idea about this switch when buying it.

1.Does FS S3800-24T4S 24-port switch support export and import traffic monitoring?

Yes, FS S3800 series switches (including S3800-24T4S ) can support export and import traffic monitoring by sflow.

2.Does FS S3800-24T4S 24-port switch have the ability to assign IP addresses?

Yes, FS S3800-24T4S switch is a stackable switch and supports DHCP (Dynamic Host Configuration Protocol) which can assign IP addresses automatically to internal networks or network service providers.

3.Can FS S3800-24T4S 24-port switch provide over current and over voltage protection?

Yes. If this switch work during limited voltage, alternating current (AC): 100 to 240V and direct current (DC) : - 50 to -60 v, over current and over voltage protection is supported.

4.What is the partition mode of VLAN and ports mode for FS S3800-24T4S switch?

FS S3800-24T4S switch supports port based VLAN and adopts package form of IEEE 802.1Q. All ports support tagged and untagged mode and protocol-based VLAN , MAC-based VLAN, IP subnet-based VLAN, etc.

Conclusion

As a key element of FS comprehensive portfolio of Gigabit switches, FS S3800-24T4S stackable managed 24-port switch offers an optimum approach to speed up your network, simplify deployment and maintenance, and reduce the total investment. It provides easy and secure access to mission critical applications for enterprises and data centers. By delivering super high availability and increased capacity, it is the perfect solution to expand your networking and better align the networks with today’s dynamic business environments.

 

Related Articles 

FS 24 Port Gigabit Switch Selection Guide 

24 Port Managed PoE Switch: How Can We Benefit From It?

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k