English

24 Port Managed PoE Switch: How Can We Benefit From It?

Updated on Nov 24, 2021 by
11.7k

Note: FS has discontinued the 24-port managed PoE switch solution. For customers who are interested in FS 24 port managed PoE switches, you can check FS PoE switches page.

With network traffic everywhere increasing at an unprecedented rate, the demand for larger bandwidth and great speeds is getting higher than ever. Managed PoE switch with unsurpassed advantages in enhancing flexibility & reliability and decreasing OPEX, is intensively applied to keep network at peak utilization. Among the various port design, a  24 port managed PoE switch is considered as a decent option for both business and home network. So when to make a move toward a managed 24-port PoE switch? How to deploy a managed PoE switch 24 port to optimize your network? That’s what we are going to explore in this article.

When to Get a 24 port Managed PoE Switch?

Like standard Ethernet switch, PoE switch comes into two variants: unmanaged and managed PoE switch. Each has places in networking industry, but with different feature and functionality. Experience from those who have dealt with 24 port managed PoE switch demonstrates that it’s a journey well worth taking – it delivers so many flexibilities and scalabilities to a network, as well as multiple management methods. Then when should we introduce a 24 port managed PoE switch to keep up with the growing business requirement? If you need some of the following features, maybe it’s time to go with a managed switch.

Demand for QoS: If you want to tailor your network traffic for QoS, redundancy, port speed, etc. And require more priority and reliability for certain computers, then get a managed switch. A 24 port managed PoE switch will let you remotely disable the power on individual ports, which is useful in case you need to reboot a single AP and don’t want to get up from your chair.

Superior Management of Network: It is nice to have management features when you need them: things like VLANs, port security, port monitoring and other functions becomes even useful when business grows. A 24 port managed PoE switch allows you to see what’s going on in the switch, and what is connected to each port. You can look at error statistics for a port to know if there is a cabling or device problem, you can remotely see which ports are actively in use, and you can also mirror ports to monitor traffic.

VLAN and VoIP Support: Ever want to have Wifi deployment and have a guest network? VLANs can help with this. It is much easier to go with a managed switch if you are going to have multiple subnets/VLANs or need to configure and manage specific ports etc. Moreover, Anything to do with VoIP configuration should always involve managed PoE switches.

FS.com 24 Port Managed PoE Switch Solution

Given the growing demand for faster network performance and maintaining Ethernet economics. The demand for a PoE switch to connect and power IP endpoints continues to soar. FS.com with years of commitment to studying customers’ preference and needs, develops S1600-24T4F PoE switch to better serve your business requests. This 24 Port managed PoE switch is built with 24 10/100/1000Base-T RJ45 Ethernet ports that are fully complaint with IEEE 802.3af/at, 2 SFP/RJ45 combo ports and 2 SFP ports. As a managed PoE switch, FS S1600-24T4S support various advanced management including WEB, CLI, TELNET, SNMP. Besides, it enables much more control over voice and data traffic, allowing you to configure and manage virtual LANs (VLANs), and giving you the ability to segregate high priority VoIP traffic over more routine data traffic. You can deploy this 24 port managed PoE switch to fit your SMB or entry-level enterprise that demands industrial, surveillance, IP phone, IP camera or wireless applications.

24 port managed poe switch

The specifications of FS 24 port managed PoE switch S1600-24T4S are listed as follows.

Switch Class Layer 2+ Switching Capacity 52 Gbps
Forwarding Rate 38.69 Mpps Web Management Interface Supported
Max. Power Consumption 600W Power Consumption per PoE Port Max. 30W
PoE Standard IEEE 802.3af/at VLANs Up to 4K
Jumbo Frames Up to 9KB Mounting Method Rack-mountable

Applications of FS.com 24 Port Managed PoE Switch

Apart from segmenting your network, a 24 port managed PoE switch can also offer a broad range of options in setting up network connections. Some common applications are demonstrated as following.

Collapsed Backbone for a LAN

FS S1600-24T4S 24 port PoE switch is a perfect choice for mixing Ethernet and Fast Ethernet installations, which paves the way for any expected future expansion. When the need occurs, just connect to another hub or switch via one of the switch’s Fast Ethernet or Gigabit Ethernet ports. The figure below shows a 24 port PoE switch operating as a collapsed backbone for a small LAN. It provides dedicated 10 Mbps full-duplex connections to workstations and 100 Mbps full-duplex connections to power users and servers. Besides, connected IP phones and wireless access points are receiving PoE power from the switch.

24 port managed poe switch for lan

Remote Connections With Fiber Cable

1000BASE-LX SFP or 1000BASE-LH SFP can be used on this 24 port managed PoE switch to interconnect remote network segments, or used to create a link to other buildings in a campus setting. 1000BASE-SX SFP transceivers can be used for Gigabit fiber connections between floors in the same building. The figure below illustrates this PoE switch connecting multiple segments with fiber cable.

24 port managed poe switch for remote connection with fiber

Making VLAN Connections

This 24 port managed PoE switch supports VLAN configurations, allowing it to organize any group of network nodes into separate broadcast domains. VLANs confine broadcast traffic to the originating group, and can eliminate broadcast storms in large networks. This provides a more secure network environment to protect your sensitive information.

24 port managed poe switch vlan configuration

Conclusion

A 24 port managed PoE switch is an optimal and future-proofing choice if you ever anticipate advanced network features to meet business growth. It perfectly fits for SMB network with its full configuration capability, advanced feature sets and improved security controls. If you have a plan for deploying a 24 port PoE switch, FS.com will offer you efficient solution and professional tech support. No more hesitation, contact us via sales@fs.com right now!


Related Articles:

FS 24-Port PoE Switch: Power Your Network for High-quality VoIP
Managed vs Unmanaged Switch: Which One Can Satisfy Your Real Need?

Understanding IEEE 802.3bt High Power PoE (Hi-PoE)
FS S5860-24XB-U PoE Switch Guarantees High-reliability Power Supply

Tags

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k