English

Why Choose FS Optics for 400G Deployment?

Updated on Jun 23, 2022 by
2.7k

The increase in global data traffic has fostered the development of optical devices, which has led to data centers facing increasing challenges in cloud access, processing power, storage, and transmission bandwidth. Because of this, the 400G transceiver market is growing rapidly, and the choices of general optical modules are gradually diversifying. Customers also have many concerns when choosing optical products, so how do FS 400G transceivers solve these concerns to meet the needs, please read this article.

Concerns for Choosing 400G Transceivers

The choice of general 400G optical modules will face many problems. Customers usually struggle with how to choose good quality 400G optical modules and have some concerns, such as the choice of suppliers, the performance and compatibility of the optical module, etc.

General Transceivers or OEM Optics?

It is well known that general optical modules have cost advantages over their OEM counterparts and are provided on demand. In the rapidly growing 400G transceiver market, diversified suppliers have increased the difficulty of selecting general optical modules, and there also be some problems: incompatibility with existing equipment, prone to network delays leading to system restarts, or other unqualified after-sales services. Therefore, it is important to choose a supplier you trust.

400G Transceiver Quality Issues

The most common quality issues with 400G transceivers from general optical product suppliers are compatibility and reliability. Because ensuring compatibility means achieving high precision when coding optics to interoperate with OEM hardware, this problem is common among inexperienced suppliers. Failures caused by these quality issues can range from a lack of relevant functionality in equipment operation to catastrophic failures such as network, system reboots, or network outages. Whether the long-term performance of the optical module can remain as efficient as the first deployment is also a factor that customers need to consider. Otherwise, it will cause trouble later.

Consequences of Incorrect 400G Transceivers

OEM warranty is a recurring issue. There is a saying that using general products in their OEM hardware voids the warranty. But the optical module itself is unlikely to damage OEM equipment because 400G ethernet QSFP modules convert electrical data from devices into optical signals, which can prove that there is no input power from the optical port to damage the device.

At this point, the optical module will not function properly or appear to be incompatible with your equipment environment, and the IT manager needs to re-plan to take the necessary alternative strategies to resolve the failure. In this case, it takes a certain amount of time to communicate with optical product suppliers and arrange for engineers to conduct fault diagnosis. If a problem is diagnosed, the faulty product should be returned and a new product delivered for redeployment and equipment testing. Essentially, the resolution to these problems costs a lot of time and effort for IT managers, adding to the cost of wasted time.

Benefits of FS 400G Optical Modules

Compared with the existing optical module supplier market, FS optical modules have certain OEM equipment compatibility and reliability, can meet various transmission needs, and have high-quality after-sales service. At the same time, FS also has a one-stop procurement platform to support the procurement of a set of 400G optical products, which greatly improves your purchase efficiency and saves costs.

Transceiver Reliability

How FS ensures the reliability of its 400G optics? It is first reflected in their production process. FS 400G optical modules adopt the original equipment manufacturer (OEM) compatibility programming core capability, featuring interoperability with multiple suppliers. These transceivers provide high-quality optical connections at a lower cost and the same performance quality as the OEM brand. Also, the transceiver's standardized features to OEM specifications ensure high component quality and suitability.

The second is the rigorous testing of the transceivers. FS optical modules are tested for compatibility on equipment by a professional technical team, as a way to eliminate errors and reduce the need for workarounds and system downtime. Even the equipment in use in your computer room can be tested to meet your expectations. This reduces the risk of network failures and ensures that the business remains up and running, providing uninterrupted service to customers. FS adheres to a 99.98% reliability rating, allowing you to enjoy quality products and services.

Multiple Choice and Trusted Services

FS can provide a variety of transceivers, and some may not be available from the OEM. FS has set up a global warehouse base with a large inventory of optical modules to connectivity needs of your network projects.

FS laboratory has an experienced team of professional technical experts and features perfect after-sales service. If you have any questions about the use of the product, you can directly contact the one-to-one sales representative to solve it. For example, if you want to know whether Juniper QSFP/OSFP works on Cisco platforms, FS will tell you based on specific lab tests and experience. Moreover, when you need to perform remote compatibility testing, the FS remote demo service can provide you with a better testing experience.

400G transceivers

Cost-effectiveness

When you choose optical products for your 400G project, 400G optical transceivers may not be the only thing you require, network devices, optical cables and corresponding accessories, such as switches, wiring, or other accessories are also needed. Of course, when applying these components, you also need to consider their loss and fit. To better solve this problem, the FS 400G product series supports one-stop procurement to help you solve your deployment problems and make the products perfectly fit your needs, which can improve your procurement efficiency and save manpower and material costs. In addition, with its professional capabilities, FS can complete the testing, collection, distribution, acceptance, after-sales, and other work of the products you need, which is convenient for your equipment maintenance and management.

A one-stop procurement approach can reduce a company's overall cost of investment (COI). For example, replacing 9 individual SKUs with one SKU at a simple price can simplify the procurement, inventory, and operational issues of optical modules. This reduces the time spent on multiple 400G optical module suppliers, and a high-quality supplier like FS can spend valuable time in other more important places, you can save up to 70% of the cost.

FS 400G product family

Explore FS 400G Optics Solutions

Facing the diverse general optic product supplier market, you should choose a supplier you trust, which will have a huge influence on your business. FS can be one of your best options as a general optical product supplier. With a professional technical team, global warehousing capabilities, remote demo services, and 400G transceivers with the same OEM performance, FS can ensure your high-performance network, optimize your operational efficiency, and minimize waste of time, effort, and budget.

You might be interested in

Knowledge
See profile for Rameez Arif.
Rameez Arif
How 400G Ethernet Influences Enterprise Networks?
Jun 23, 2022
7.8k
Blog
See profile for George.
George
FAQs About FS 400G Transceivers
Jul 16, 2022
7.5k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge