English

XFP vs SFP+: What Are the Differences?

Updated on Jan 5, 2022 by
51.5k

In fiber optic networking, optical module is the indispensable building block and the enabler of seamless data transmission. 10G fiber optic transceivers are still popular in the market such as 10G XFP and 10G SFP+, then XFP vs SFP+, what are the differences? How about their inter-compatibility? Can we connect XFP with SFP+ module? Find all the answers in the following.

XFP vs SFP+: Definition

The XFP (10 Gigabit Small Form Factor Pluggable) is a standard for modules for high-speed network and telecommunication links that use optical fiber. XFP modules are hot-swappable, protocol-independent and they typically operate at near-infrared wavelengths (colors) of 850nm, 1310nm or 1550nm. Also, XFP transceivers can operate over a single wavelength or use dense wavelength-division multiplexing techniques. Principal applications of XFP modules include SONET OC-192, SDH STM-64, 10 Gbit/s Optical Transport Network (OTN) OTU-2, and parallel optics links.

The SFP+ (Enhanced Small Form-factor Pluggable) is an enhanced version of the SFP that supports data rates up to 16 Gbit/s. 10G SFP+ modules can be applied for SONET OC-192, SDH STM-64, OTN G.709, CPRI wireless, 16G Fibre Channel, and the emerging 32G Fibre Channel application.

Figure 1: XFP vs SFP+

XFP vs SFP+: Specifications

XFP vs SFP+, what are the differences? Although both of these modules are mainly used in 10G fiber optic networking, 10G XFP transceivers differs from 10G SFP+ optics in some specifications. Let's look at the details from the following figures.

Optical Type XFP SFP+
Standard IEE802.3ae; XFP MSA IEE802.3ae; SFF-8431; SFF-8432
Publish Time 2002 2006
Size Bigger Smaller
Data Rate 6Gbps; 8.5Gbps; 10Gbps 6Gbps; 8.5Gbps; 10Gbps
Wavelength 850nm; 1310nm; 1550nm; CWDM; DWDM; BIDI; Tunable; Copper 850nm; 1310nm; 1550nm; CWDM; DWDM; BIDI; Tunable; Copper
Fiber Type OM3; OM4; OS1; OS2 OM3; OM4; OS1; OS2
Typical Connector LC LC
Max Distance 120km 120km
Cost Higher Lower

Through comparing XFP vs SFP+, it is clear that SFP+ shares some advantages over XFP:

10G SFP+ optics has a smaller footprint than the XFP modules, which can also enable greater port density. That is because SFP+ transceivers leave more circuitry to be implemented on the motherboard instead of its inside — it moves some functions to the motherboard, including signal modulation function, MAC, CDR and EDC. Moreover, XFP technology is relatively older but more expensive, that's also the reason 10G SFP+ modules have been gaining more market share.

XFP vs SFP+: Application Scenarios

XFP optics are connectivity options for data center, enterprise wiring closet, and service provider transport applications.

10G SFP+ Transceivers are widely used on 10G switches, routers, servers, NICs and other transmission equipment. Featuring low power consumption and high speed, SFP+ is suitable for data center, enterprise wiring closet and other environments. You can click the link to see the details.

Additionally, 10G XFP and SFP+ transceivers can be inter-compatible in one Ethernet network on condition that their protocols are consistent and they conform to the same wavelength and signaling rate (as the figure presented below).

Figure 2: XFP vs SFP+: Interconnection Application

XFP vs SFP+: FAQs

Q: Can XFP module connect with SFP+ transceiver?

A: XFP connector and SFP+ connector are both LC duplex. For example, the XFP 10G 1310nm transceivers can talk to the SFP+ 10G 1310nm modules via LC duplex fiber optic cable. The following figure shows a typical interconnection application with XFP and SFP+ modules.

Q: Can I plug SFP+ module into the XFP slot?

A: No. Since the size of two formats are totally different from each other, it is not feasible to use SFP+ module in XFP slot and vice versa. Please make clear which port type the switch is equipped with and remember that XFP and SFP+ optical transceivers are not interchangeable.

Figure 3: SFP+ Module Can't be Plugged in XFP Slot

Q: What are the differences between XFP vs SFP+ vs SFP?

A: SFP and SFP+ are the same size with different speed and compatibility. Unlike XFP and SFP+ modules which are used in 10GbE applications, SFP is for 100BASE or 1000BASE applications. And SFP+ ports can accept SFP optics at a reduced speed of 1 Gbit/s, but a SFP+ transceiver can not be plugged into a SFP port. Excerpt from SFP vs SFP+ vs SFP28 vs QSFP+ vs QSFP28, What Are the Differences?

Q: How's the prospect of 10G XFP and SFP+ modules?

A: Though the pursuit for higher bandwidth is unstoppable, 10GbE won't step out of the market in many cases. SFP+ transceivers are still a mainstream option offering a smaller size, lower consumption and lower cost. Not as popular as SFP+ transceivers, 10G XFP modules still play an irreplaceable role in some 10G network applications.

Conclusion:

To summarize, XFP vs SFP+, there are many differences. While SFP+ transceivers have a smaller size than 10G XFP modules, considering cost, port density and applications, 10G SFP+ transceivers are favored in the market as a cost-effective solution.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k