English

How to Choose the Best 10gb Switch for Home?

Updated on Jan 18, 2023 by
28.7k

As the popularity of 10 Gigabit Ethernet grows and the price of 10 Gigabit devices drops, more and more individual home users, such as technology enthusiasts, gamers, and professional video editors, have deployed 10gb switches on their home networks. This article focuses on why 10gb switches are needed for home networks, and how to choose the best 10gb switch for home.

Why is 10gb Switch Needed for Home?

A 10gb switch is necessary for home users to meet a specific network requirement. For example, when multiple family members are simultaneously streaming HD videos, a 10 Gigabit Ethernet switch is needed to provide sufficient bandwidth to ensure network stability and smoothness. Alternatively, if there are numerous devices connected to the home network, such as smart home devices, surveillance cameras, media servers, etc., a stronger network capacity is required to support the connectivity of all devices. In addition, the security of data and the convenience of external network access is also improved.

 

     " Also check - FS 10G Switches

 

10G switch

Common Types of 10gb Switch for Home

10gb PoE Switch

10gb PoE Switches have multiple Ethernet ports that can be used to connect other devices, such as VoIP phones, wireless access points, and IP cameras. The switch is responsible for providing power to the connected devices, eliminating the need for separate power cables.

 

     " Also check - Unlocking the Secrets of PoE Switches — A Complete Guide

 

10gb SFP+ Switch

10gb SFP+ Switch offers superior performance in network latency and throughput, supporting high speeds of up to 10Gbps per SFP+ port. 10gb SFP+ switches are becoming very popular choices for latency-sensitive applications. It can be connected using fiber optic cables or DAC/AOC cables, etc. For LAN networks that require ultra-low latency and large bandwidth, a 10gb SFP+ switch can be a suitable choice.

10gb BASE-T Switch

10gb BASE-T switches are compatible with existing copper infrastructure. They can seamlessly integrate into networks that already have Cat 5e or Cat 6 copper cabling installed, eliminating the need for costly cable upgrades. This makes them a cost-effective solution for home looking to upgrade their network speeds without completely overhauling their cabling infrastructure.

Six Considerations When Choosing a 10gb Switch for Home

To make sure the 10gb switch that you choose is suitable for your home network, you need to consider the following aspects of 10 Gigabit switches.

Switch Ports

There are two main port types of 10gb switches, copper ports and optical ports. The copper ports on a 10 gigabit switch support Ethernet cables like Cat6 for data transmission, but the distance is limited to 100m (330ft). If your legacy network uses Cat5e or Cat6 Ethernet cables to transmit data, as mentioned above, it's a good choice to buy a 10gb Base-T network switch. You can continue to use the existing cables to achieve a 10G transmission.

 

     " Also check - Get Further Understanding of Ethernet Switch Port Types

 

But if you decide to upgrade to 10G fiber networks, buying a 10gb SFP+ network switch is better. The optical ports on the 10 Gigabit switch can be inserted with SFP+ transceivers and fiber optic cables, which helps lower latency and power consumption.

In addition, you should figure out how many of your home devices need to be connected to the 10gb switch. Usually, a 24-port 10Gb Ethernet switch can satisfy the needs of most home users.

 

     " Also check - FS S5850-24S2Q, 24-Port Ethernet Layer 3 10G Switch

 

Network Deployment Cost

The network deployment cost depends on whether you use the 10gb BASE-T switch or the 10gb SFP+ switch. For the home network, if you choose a 10gb BASE-T switch, the conventional Cat6 Ethernet cable will make it with ease. If you choose a 10Gb Ethernet SFP+ switch, you need to prepare dedicated SFP+ modules and optical fibers. Note that one optical fiber requires two SFP+ modules. If you buy a home-use 10 gigabit SFP+ switch, you also need to pay for SFP+ transceivers, which will further increase the cost of 10G network deployment.

 

     " Also check - FS S5860-20SQ, 24-Port Ethernet Layer 3 10Gb Switch, support AC/DC power supply

 

Managed or Unmanaged

An unmanaged 10gb switch switch is a plug-and-play device that comes with a fixed configuration that cannot be changed. It is easy to use and suitable for home users who just want to set up a 10G network and don’t want to worry about its management.

In contrast, a managed 10gb switch is more complex and allows users to change settings. It also requires skills to set up and maintain. Users can disable unused ports, limit access to their network, limit speed, prioritize traffic, adjust parameters, etc.

 

     " Also check - FS S5800-48T4S, 48-Port Ethernet Layer 3 10G Switch

 

Even if all your home devices are active simultaneously, clogged traffic will not be a problem. And the 10 gigabit switches with features such as IPv6 ACL(Access Control List) can help increase your home network security, making it possible for controlling switch port access for each network user individually.

PoE or Non-PoE

PoE technology is different from non-poe in that it can support power and data transmission on the same network cable. Therefore, if you're planning to install IP Phones, security cameras, and more in your home, then 10gb PoE switch will be a great option. Besides, the 10gb PoE switch delivers great flexibility, allowing you to easily place endpoints anywhere in your home without considering the power outlet.

 

     " Also check - S5850-48S6Q, 48-Port Ethernet Layer 3 10G Switch

 

Figure2: 10G PoE Switch for Home Network

Smart Fans

To select a 10gb switch for home use, you also need to consider the smart fan design. This functional design not only guarantees superior cooling performance, and power reduction, but also creates a quiet environment for you and your family without having to worry about noise from a 10 gigabit switch with a smart fan.

Conclusion

Nowadays, there are so many data and applications running on our home networks, and traffic will continue to grow definitely. Using a 10gb switch to build a 10G home network is becoming more and more popular. You need to consider your current needs and the above-mentioned points if you want to select the best 10gb switch for your home network.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k