English

What's the Difference? Hub vs Switch vs Router

Updated on Dec 17, 2021 by
367.0k


In an Ethernet network, there are some networking devices that play their roles at various levels such as hubs, switches and routers. The functions of the three devices are all quite different from one another, even if sometimes they are all integrated into a single device. due to that, many people feel confused about the differences between the hub, switch, and router. The following part will focus on the topic—hub vs switch vs router, aiming to clarify differences among them.

What Are Hub, Switch and Router?

Hub

Hub is commonly used to connect segments of a LAN (Local Area Network). A hub contains multiple ports. When a packet arrives at one port, it is copied to the other ports so that all segments of the LAN can see all packets. Hub acts as a common connection point for devices in a network.

Switch

A switch operates at the data link layer (layer 2) and sometimes the network layer (layer 3) of the OSI (Open Systems Interconnection) Reference Model and therefore support any packet protocol. LANs that use switches to join segments are called switched LANs or, in the case of Ethernet networks, switched Ethernet LANs. In networks, the switch is the device that filters and forwards packets between LAN segments. See more information on Network Switch and Selection Suggestions.

Router

A router is connected to at least two networks, commonly two LANs or WANs (Wide Area Networks) or a LAN and its ISP.s (Internet Service Provider.s) network. The router is generally located at gateways, the places where two or more networks connect. Using headers and forwarding tables, router determines the best path to forward the packets. In addition, router uses protocols such as ICMP (Internet Control Message Protocol) to communicate with each other and configures the best route between any two hosts. In a word, router forwards data packets along with networks.

Hub vs Switch vs Router

In network equipment and devices, data is usually transmitted in the form of a frame. When a frame is received, it is amplified and then transmitted to the port of the destination PC (Personal Computer). The big difference between hub and switch is in the method in which frames are being delivered.

hub.gif

In a hub, a frame is passed along or "broadcast" to every one of its ports. It doesn't matter that the frame is only destined for one port. The hub has no way of distinguishing which port a frame should be sent to. Additionally, a 10/100Mbps hub must share its bandwidth with each and every one of its ports. In comparison, a switch keeps a record of the MAC (Media Access Control) addresses of all the devices connected to it. With this information, a network switch can identify which system is sitting on which port. So when a frame is received, it knows exactly which port to send it to, without significantly increasing network response times. In addition, unlike a hub, a 10/100Mbps switch will allocate a full 10/100Mbps to each of its ports. So regardless of the number of PCs transmitting, users will always have access to the maximum amount of bandwidth.

ethernet-switch.gif

Unlike an Ethernet hub or switch that is concerned with transmitting frames, a router is to route packets to other networks until that packet ultimately reaches its destination. One of the key features of a packet is that it not only contains data but the destination address of where it's going. What's more, router is the only one of these three devices that will allow you to share a single IP (Internet Protocol) address among multiple network clients.

You can have a clear view of the comparison among hub vs switch vs router here:

template Hub Switch Router
Layer Physical layer Data link layer Network layer
Function To connect a network of personal computers together, they can be joined through a central hub Allow connections to multiple devices, manage ports, manage VLAN security settings Direct data in a network
Data Transmission form electrical signal or bits frame & packet packet
Port 4/12 ports multi-port, usually between 4 and 48 2/4/5/8 ports
Transmission type Frame flooding, unicast, multicast or broadcast First broadcast, then unicast and/or multicast depends on the need At Initial Level Broadcast then Uni-cast and multicast
Device type Non-intelligent device Intelligent device Intelligent device
Used in(LAN, MAN, WAN) LAN LAN LAN, MAN, WAN
Transmission mode Half duplex Half/Full duplex Full duplex
Speed 10Mbps 10/100Mbps, 1Gbps 1-100Mbps(wireless); 100Mbps-1Gbps(wired)
Address used for data transmission MAC address MAC address IP address

Conclusion

The differences between hub, switch and router is a confusing term for users. Understanding these distinctions among them can be helpful to find the most appropriate device for your network. I hope this article will help you get clear about the knowledge of hub vs switch vs router and get able to choose the devices you need after reading this.

Related Articles:

Layer 2 vs Layer 3 Switch: Which One Do You Need?
Network Switch vs Network Router vs Network Firewall
What Is VPN Router and Why You Need It?

You might be interested in

Knowledge
See profile for Howard.
Howard
Essential Facts About Bare Metal Switch
Jun 1, 2022
4.2k
Knowledge
Knowledge
Knowledge
See profile for Howard.
Howard
VXLAN: the Future for Data Center Networks
May 20, 2023
7.8k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
384.7k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.0k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
334.2k
Knowledge