中文

飞速(FS) S3900系列交换机如何配置STP?

发布于 2020年06月05日 by
421

STP(生成树协议)是由IEEE 802.1D定义的一种在网桥和以太网交换机上运行的第二层协议,其主要作用是通过阻塞冗余链路上的一些端口来避免网络环路的形成,有效避免广播风暴以及MAC地址表不稳定等问题的出现,从而确保用户通信质量;与此同时,当活动路径发生故障时,可激活冗余备份链路,恢复网络连通性,确保网络正常运行。飞速(FS) S3900系列千兆管理型交换机适用于SMB、企业和校园网络,可支持STP,提供冗余链路,有效避免环路的产生,从而提高网络的可靠性和稳定性。

S3900交换机更多配置操作说明请参阅:飞速(FS) S3900系列交换机基于IP子网划分VLAN配置指南

飞速(FS) S3900系列交换机的STP应用

以飞速(FS)S3900系列交换机的STP典型应用组网方案为例。如下图,用户在交换机A、B、C上部署STP协议后,三台交换机可通过彼此交互信息发现网络中的环路,并有选择的对某个端口进行阻塞,从而防止报文在环路网络中不断增生和无线循环。

在以下STP典型方案中,STP将交换机B作为根桥,STP协议通过计算路径开销选择较为“强壮”的链路1(PC1-交换机B-交换机C-PC2)作为活动路径,同时,使用STA(生成树算法)阻塞了交换机C上的非指定端口,将链路2(PC1-交换机B-交换机A-交换机C-PC2)作为冗余备份链路(正常情况下不可用)。当链路1发生故障时,STP将开启交换机C上被阻塞的非指定端口,让数据包从链路2进行传输,最后成功的达到PC2。

注意事项:

1)由于STP协议存在较大局限性,因此IEEE又制定了RSTP和MSTP协议。RSTP在STP基础上实现了快速收敛,并增加边缘端口的概念和保护功能,可快速响应网络变化或网络故障。MSTP则是弥补了STP和RSTP的缺陷,它把一个交换网络划分成多个域,每个域内形成多棵生成树,生成树之间彼此独立。也就是说MSTP通过生成多棵无环路生成树,解决广播风暴,实现冗余备份,并在VLAN间实现负载均衡,不同VLAN的流量按照不同的路径转发。

2)飞速(FS) S3900系列交换机包含了S3900-24F4S、S3900-24T4S和S3900-48T4S三种型号,这三种交换机均支持STP/RSTP/MSTP,可与思科、瞻博等品牌交换机搭配使用,实现STP/RSTP/MSTP功能。但需要注意的是,对于小型企业来说,考虑到网络收敛速度,建议用户优先选择RSTP,MSTP更适用于大型企业网络。

 

飞速(FS) S3900系列交换机的STP配置思路P

飞速(FS) S3900系列交换机适用于小型企业网,通常情况下,配置STP/RSTP即可,而MSTP适用于大型企业网络,在飞速(FS) S3900系列交换机不常用,这里不做多说明。飞速(FS) S3900系列交换机可通过CLI命令配置STP/RSTP,配置主要分为以下四个步骤:

1. 启动STP;

2. 配置STP模式;

3. 配置根桥;

4. 验证配置。

 

飞速(FS) S3900系列交换机通过CLI配置STP/RSTP

图2为飞速(FS) S3900系列交换机STP/RSTP应用方案图。

STP配置步骤和命令

1. 配置S3900-24F4S-A交换机,在全局开启生成树并更改生成树模式和优先级,使其成为根桥;

S3900-24F4S-A-2(config)#spanning-tree
S3900-24F4S-A-2(config)#spanning-tree mode stp
S3900-24F4S-A-2(config)#spanning-tree priority 0

2. 配置S3900-24F4S-B交换机,全局开启生成树并更改生成树模式;

S3900-24F4S-B(config)#spanning-tree
S3900-24F4S(config)#interface vlan 1

3. 配置S3900-48T4S交换机,全局开启生成树并更改生成树模式;

S3900-48T4S-3(config)#spanning-tree
S3900-48T4S-3(config)#spanning-tree mode stp

4. 查看三台交换机的生成树状态。

#检查S3900-24F4S-A交换机的状态

S3900-24F4S-A-2#show spanning-tree brief
Spanning Tree Mode: STP
Spanning Tree Enabled/Disabled: Enabled
Designated Root: 0.ECD68A369C78
Current Root Port: 0
Current Root Cost: 0

stp 1.png

#检查S3900-24F4S-B交换机的状态

S3900-24F4S-B#show spanning-tree brief
Spanning Tree Mode: STP
Spanning Tree Enabled/Disabled: Enabled
Designated Root: 0.ECD68A369C78
Current Root Port (Eth): 1/21
Current Root Cost: 20000

stp 2.png

#检查S3900-48T4S交换机的状态

S3900-48T4S-A-3#show spanning-tree brief
Spanning Tree Mode: STP
Spanning Tree Enabled/Disabled: Enabled
Designated Root: 0.ECD68A369C78
Current Root Port (Eth): 1/1
Current Root Cost: 20000

stp 3.png

配置结果:

1)交换机S3900-24F4S-A因优先级最高,因此成为了根桥;
2)交换机S3900-24F4S-A因优先级最高,因此成为了根桥;
结论:交换机S3900-24F4S支持STP功能,并可正常运行。

RSTP配置步骤和命令

1. 配置S3900-24F4S-A交换机,在全局开启生成树并更改生成树模式和优先级,使其成为根桥;

S3900-24F4S-A-2(config)#spanning-tree
S3900-24F4S-A-2(config)#spanning-tree priority 0
S3900-24F4S-A-2(config)#spanning-tree mode rstp

2. 配置S3900-24F4S-B交换机,全局开启生成树并更改生成树模式;

S3900-24F4S-B(config)#spanning-tree
S3900-24F4S-B(config)#spanning-tree mode rstp

3. 配置S3900-48T4S交换机,全局开启生成树并更改生成树模式;

S3900-48T4S-1(config)#spanning-tree
S3900-48T4S-1(config)#spanning-tree mode rstp

4. 查看三台交换机的生成树状态。 .

#检查S3900-24F4S-A交换机的状态

S3900-24F4S-A-2#show spanning-tree brief
Spanning Tree Mode: RSTP
Spanning Tree Enabled/Disabled: Enabled
Designated Root: 0.ECD68A369C78
Current Root Port: 0
Current Root Cost: 0

rstp 1.png

#检查S3900-24F4S-B交换机的状态

S3900-24F4S-B#show spanning-tree brief
Spanning Tree Mode: RSTP
Spanning Tree Enabled/Disabled: Enabled
Designated Root: 0.ECD68A369C78
Current Root Port (Eth): 1/21
Current Root Cost: 20000

rstp 2.png

#检查S3900-48T4S交换机的状态

S3900-48T4S-1#show spanning-tree brief
Spanning Tree Mode: RSTP
Spanning Tree Enabled/Disabled: Enabled
Designated Root: 0.ECD68A369C78
Current Root Port (Eth): 1/1
Current Root Cost: 20000

rstp 3.png

 

配置结果:

1)三台交换机均开启RSTP;
2)交换机S3900-24F4S-A因优先级最高成为了根桥,其端口eth1/21-22成为指定端口;
3)交换机S3900-24F4S-B端口eth1/22被阻塞,使其存在于一个逻辑无环的链路中。
结论:交换机S3900-24F4S支持RSTP功能,并可正常运行。
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
44
技术博文
See profile for Audrey.
Audrey
数据中心预端接主干铜缆解决方案
2021年12月31日
1.8k