- English
- German
- French
- Spanish
- Japanese
- Italian
- Chinese
- Chinese (traditional)
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
- Blog Type
- Product
- Topic
- Region
Hot Search
- Product Updates
- Share FS
- PoE Switch
- Networking
- Networking Devices
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
-
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
- Blog Type
- Product
- Topic
- Region
- Home
- Blog
- Case Study
- Knowledge Center
- Glossary
- Story
- Video
- English
Hot Search
- Product Updates
- Share FS
- PoE Switch
- Networking
- Networking Devices
Optimizing Data Center High-density Cabling with Uniboot Fiber Cables
A data center is a critical infrastructure for storing and processing large amounts of data. To meet the increasing demand for high-speed transmission, high-density fiber optic cabling has become an important aspect of data center construction. Uniboot fiber optic cables, with their unique advantages, have become a powerful aid for high-density cabling in data centers.
Characteristics of Uniboot Fiber Patch Cables
Both in terms of cable structure and connectors, uniboot fiber optic cables differ from ordinary fiber optic cables because they are specifically designed for high-density cabling. The following are the specific features of uniboot patch cables.
One Cable Carries Two Fibers
Uniboot fiber patch cables allow one cable to carry two fibers, meaning one patch cord and one connector can transmit signals for two fibers. Therefore, uniboot fiber patch cords occupy less space and require fewer cable resources than ordinary optical fiber cables. In addition, the fiber cores of uniboot patch cables are Corning bend-insensitive fibers, with a minimum bending radius as low as 7.5mm, allowing for tighter bending of patch cords, and making cable management and storage more relaxed and flexible. Read the introduction "Uniboot vs Standard Fiber Cables: Which One to Choose?" to get more information about the difference between uniboot fiber cables and standard fiber cables.
A Wide Variety of Connector Types
Uniboot optical fiber cables come with various specialized connector designs, including standard clip, flat clip, flat clip with push-pull boot, secure keyed, and more. Among them, the flat clip uniboot fibers allow for polarity reversal without exposing the fibers and or needing any tools. The flat clip uniboot fiber with push-pull boot facilitates easy insertion and removal of uniboot patch cables. The very small form factor (VSFF) of SN & CS & MDC connectors can significantly increase cabling density. We can choose the most suitable connector type based on our specific needs.
Application of Uniboot Fiber Cables in High-Density Cabling
So why is uniboot fiber the ideal choice for high-density cabling in data centers? It's not difficult to see that this must be closely related to the features of the uniboot fiber mentioned earlier. The unique uniboot fiber optic cables optimize high-density cabling in the following aspects.
Saving Fiber Optic Cabling Space
The uniboot fiber achieves bidirectional signal transmission with a single cable, and the unique SN & CS & MDC connectors of these types of uniboot fiber cables are super small-sized connectors with a fiber density three times that of LC connectors. Compared to conventional fiber connectors, it not only saves fiber cable resources but also allows for more fiber connections in a smaller space. Therefore, uniboot fiber cables improve the space utilization and cabling density of data center. Additionally, the bend-insensitive fibers of uniboot patch cables enable tighter and more relaxed cable layouts. High-density cabling requires reducing cable space and increasing cabling density, making uniboot an authentic high-density fiber optic cable.
Simplifying Cabling Management
Reducing Cable Congestion
Uniboot fiber cables streamline cabling management by reducing complexity. With a single cable carrying two fibers, uniboot fibers have fewer cable counts than conventional optical fiber cables in the same high-density cabling space, which helps reduce cable congestion caused by excessive cable quantities and simplifies the operation and maintenance of high-density cabling in data centers.
Improving Cabling Efficiency
The flat clip Uniboot fiber cables meet your polarity reversal needs without tools or exposing the fibers. The operation is simple and convenient as the figure shows. Therefore, this connector design eliminates many troubles in cabling management and enhances cabling efficiency. In addition, uniboot fiber optic patch cable with push-pull boot enables easy and fast insertion and removal in high-density cabling spaces, further enhancing the convenience and efficiency of cabling management. It is clear that uniboot optical fiber cables play a vital role in simplifying cabling.
Supporting High-speed Data Transmission
Uniboot fiber cables with SN & CS & MDC connectors support 100/400/800G Ethernet data transmission. For example, the distinctive SN connector, a very small form factor (VSFF) duplex fiber connector manufactured with 1.25mm ceramic ferrule technology, has been adopted in the specifications of QSFP-DD and OSFP transceivers. These connectors are the new standard for next-generation pluggable transceivers used in 200Gbps, 400Gbps, and 800Gbps data center interconnects (DCI). They provide excellent optical performance and perfectly meet the application requirements of high-speed data transmission in data centers. The types of uniboot fiber patch cables that support high-speed transmission are organized in the following figure.
Connector Type |
CS™-CS™ |
CS™-LC |
MDC-MDC |
MDC-LC |
SN-SN |
SN-LC |
Transceivers | OSFP/QSFP-DD | OSFP/QSFP-DD |
OSFP/QSFP-DD/SFP-DD |
OSFP/QSFP-DD/SFP-DD |
OSFP/QSFP-DD/SFP-DD |
OSFP/QSFP-DD/SFP-DD |
Transmission Speed |
2x100/2x200/ 4x200G |
2x100/2x200/ 4x200G |
2x50/4x100/ 4x200G |
2x50/4x100/ 4x200G |
2x50/4x100/ 4x200G |
2x50/4x100/ 4x200G |
Improving Airflow in Cabling Space
Multimode flat clip uniboot fiber patch cables use Suncall LC connectors, which provide additional space between connectors, improving airflow and cooling efficiency. In high-density cabling spaces, where fiber optic cable density is high and connectors are in close proximity, data centers can easily experience temperature issues. The flat clip connectors of uniboot fiber cables create more space between connectors, relieving the high-temperature issue effectively.
Conclusion
In conclusion, as analyzed in the previous text, the exclusive cable structure and connector features of uniboot fiber patch cables make them well-suited for application needs in data center high-density cabling, including space-saving, simplified cabling management, high-speed data transmission, and improved cooling efficiency. Without doubt, uniboot fiber patch cable has become the savior of popularized high-density cabling systems. If you want to learn more about uniboot fiber optic cables, please read the article "Introducing the Uniboot Fiber Patch Cable Series". With the increasing demand for higher data transmission rates and throughput in data centers, it is expected that uniboot fiber optic cables will continue to evolve and effectively support high-density cabling in the future.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023